Training ... // WiSeConnect 3//Version 3.3.3 //API Reference Guide ... You are viewing documentation for version: 3.3.3 ... The WiSeConnect™ SDK v3.x uses Silicon Labs standard status codes.
Bits 0 - 2 : Highest 3 bits of the data payload length field Bits 3 - 5 : Device type Bit value 100 : Bluetooth LE ... 0x01 2 Events ... 0x12 3 cmd_gatt_server_send_user_prepare_write_response
Support ... // WiSeConnect 3//Version 3.4.0 //Developing with WiSeConnect 3 SDK You are viewing documentation for ... To learn more about the WiSeConnect SDK v3.x, see the About the SDK pages.
The value in milliseconds must be larger than (1 + latency) * max_interval * 2, where max_interval is given in milliseconds ... sl_bt_gap_phy_coding_500k_coded (0x8): 500k Coded PHY (S=2)
You are viewing documentation for version: 2.6 | Version History ... See Stack Tokens for documentation. ... The following convenience macros are used to simplify the definition process for ...
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/4.1/emlib/api/efr32xg23/machine-learning/api/group-ml-audio-feature-generation