Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ... ls
ProductWirelessResource TypeSoftware API documentation
BGX13-1.x Command Reference This page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. ... > gge 5 1 gges
ProductWirelessResource TypeSoftware API documentation
1 - an update is available, the contains the new bundle version string ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ... ipd 1 Input, high-impedance
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... Note
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/4.2/emlib/api/efm32g/service/api/group-policy