// Gecko Platform//Version 4.4.1 //Services ... All API functions can be called from within interrupt handlers. ... sl_sleeptimer_is_power_manager_early_restore_timer_latest_to_expire(void)
Example ... Also define the CTS and RTS locations by setting portLocationCts and portLocationRts in the init struct. ... [in] type Abort type – whether to abort only Tx, only Rx, or both.
ProductMicrocontrollersResource TypeSoftware API documentation
// Platform//Version 5.0.1 //Security ... is the recommended device independent crypto API and should be used whenever possible ... sl_se_otp_init_t otp_settings_init = SL_SE_OTP_INIT_DEFAULT;
Results 1-5 of 5 for gecko-platform/4.2/emlib/api/efm32gg/driver/api/group-uartdrv-error-codes