2 - no update available (i.e. the device's current firmware is up-to-date) <message> - bundle version or ... Gecko OS writes the file to extended flash or bulk flash, depending on the location ...
Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Issue Gecko OS command, store string result in buffer. ... Issue Gecko OS command, return result data in buffer. ... Issue Gecko OS command asynchronously and invoke callback on completion.
ProductWirelessResource TypeSoftware API documentation
BGX modules create a serial interface replacement using the custom Xpress streaming ... Evaluation board ... See the following for additional example demos for using the BGX13:
ProductWirelessResource TypeSoftware API documentation
Example Example usage. Alphabetical List of Commands ... Note 2 : Using this command will also cause the BGX to clear its internal bonding ... os pins can only use the strong drive strength.
ProductWirelessResource TypeSoftware API documentation
Results 1-5 of 5 for gecko-platform/4.2/emlib/api/efm32gg11/machine-learning/api/group-ml-audio-feature-generation