Silicon Labs
gecko-platform/4.2/emlib/api/efm32gg12/common/api/group-atomic
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
    Results 1-5 of 5 for gecko-platform/4.2/emlib/api/efm32gg12/common/api/group-atomic in 0.18 seconds
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
    ProductWireless Resource TypeSoftware API documentation
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Modules ... Issue Gecko OS command asynchronously and invoke callback on completion. ... [out] buffer Buffer to hold returned data [in] ... [out] buffer Buffer to hold string result [in]
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren ) ... Returns the RSSI value from the latest received packet of the current active ...
    ProductWireless Resource TypeSoftware API documentation
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    Gecko OS writes the file to extended flash or bulk flash, depending on the location ... , file version defaults to 1.0.0 . -t <type> t ype: specify file type as integer or hex string 2 .
      Results 1-5 of 5 for gecko-platform/4.2/emlib/api/efm32gg12/common/api/group-atomic