Silicon Labs
gecko-platform/4.2/emlib/api/efm32hg/service/api/group-cpc-security-secondary
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
    Results 1-5 of 5 for gecko-platform/4.2/emlib/api/efm32hg/service/api/group-cpc-security-secondary in 0.09 seconds
    Gecko OS Commands Silicon Labs
    https://docs.silabs.com/.../comma...
    tls_server UART uart_update UDP ... 0 - the request failed, the contains the error message ... Gecko OS writes the file to extended flash or bulk flash, depending on the location option: -l ...
    Gecko OS 4.2 Command API Silicon Labs
    https://docs.silabs.com/.../...
    Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as lots of Command API examples covering a wide range of uses.
    Update and Recovery - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../update-and-recov...
    Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... 0 = no, 1 = yes <- Print a list of faults (8 faults should print) <- Reset faults ...
    ProductWireless Resource TypeSoftware API documentation
    Commands - v4.1 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../group-api-core-comm...
    Modules Types Command data types. Functions ... Issue Gecko OS command, store string result in buffer. ... ) Issue Gecko OS Command. For available commands, see Gecko OS Command API . ... Note
    ProductWireless Resource TypeSoftware API documentation
    BGX13-1.x Command Reference - v1.0 - Gecko OS API Documentation Silicon Labs
    https://docs.silabs.com/.../comma...
    ... page provides a list of Bluetooth Xpress API commands with a full description of how ... os pins can only use the strong drive strength. May be one of the following types: drvst : Strong drive ...
    ProductWireless Resource TypeSoftware API documentation
      Results 1-5 of 5 for gecko-platform/4.2/emlib/api/efm32hg/service/api/group-cpc-security-secondary