You are viewing documentation for version: 4.2 | Version History ... Configuration Options The API Flow Control Support Example ... Flow Control method. enum UARTDRV_FlowControlState_t {
ProductMicrocontrollersResource TypeSoftware API documentation
You are viewing documentation for version: 4.2 | Version History ... The control block references a ring buffer for each configured channel. ... You should avoid using it in production.
ProductMicrocontrollersResource TypeSoftware API documentation
5.1.2 (latest) Platform# Platform (formerly known as Gecko Platform) is the foundation for Silicon Labs ... Gecko SDK will continue to be available providing long-term support for our Series 0 ...
// Gecko Platform//Version 4.4.1 //Services ... SL_SLEEPTIMER_FREQ_DIVIDER must be a power of 2 within the range 1 to 32. ... All API functions can be called from within interrupt handlers.
... that PSA Crypto is the recommended device independent crypto API and should be used whenever possible. ... , secure boot and secure debug implementation, is available on all series 2 devices.
Results 1-6 of 6 for gecko-platform/4.2/emlib/api/efm32wg/common/api/group-enum