Gecko OS 4.2 Command API The Command API documentation provides details of commands and variables as well as ... Overview for a description of the general structure and features of Gecko OS 4.
Gecko OS is part of a larger sophisticated application framework installed on all Gecko OS devices. ... The Gecko OS Device Firmware Update (DFU) feature allows device firmware to be updated ...
ProductWirelessResource TypeSoftware API documentation
Command data types. ... Issue Gecko OS command, store string result in buffer. ... More. gos_result_t gos_cmd_issue_with_config ( gos_cmd_operation_config_t *config, const char *fmt,.)
ProductWirelessResource TypeSoftware API documentation
os pins can only use the strong drive strength. ... Output, open-source with pull-up (see gdi os pren ) ... Returns the RSSI value from the latest received packet of the current active ...
ProductWirelessResource TypeSoftware API documentation
Gecko OS writes the file to extended flash or bulk flash, depending on the location ... , file version defaults to 1.0.0 . -t <type> t ype: specify file type as integer or hex string 2 .
Results 1-5 of 5 for gecko-platform/4.2/emlib/api/efm32zg/hardware-driver/api/group-joystick