You are viewing documentation for version:4.3PWM driver instance. Public Attributes#TIMER_TypeDef *timerTIMER instance. uint8_tchannelTIMER channel. uint8_tportGPIO port. uint8_tpinGPIO pin. uint8_tlocationGPIO location. Public Attribute Documentation#timer#TIMER_TypeDef* sl_pwm_instance_t::timerTIMER instance. channel#uint8_t sl_pwm_instance_t::channelTIMER channel. port#uint8_t sl_pwm_instance_t::portGPIO port. pin#uint8_t sl_pwm_instance_t::pinGPIO pin. location#uint8_t sl_pwm_instance_t::locationGPIO location.