Synchronous mode initialization structure.

Public Attributes#

Specifies whether TX and/or RX shall be enabled when initialization is completed.

uint32_t

USART/UART reference clock assumed when configuring baud rate setup.

uint32_t

Desired baud rate.

Number of data bits in frame.

bool

Select if to operate in master or slave mode.

bool

Select if to send most or least significant bit first.

Clock polarity/phase mode.

bool

Auto CS enabling.

bool

Enable CS invert.

Public Attribute Documentation#

enable#

USART_Enable_TypeDef USART_InitSync_TypeDef::enable

Specifies whether TX and/or RX shall be enabled when initialization is completed.


refFreq#

uint32_t USART_InitSync_TypeDef::refFreq

USART/UART reference clock assumed when configuring baud rate setup.

Set to 0 to use the currently configured reference clock.


baudrate#

uint32_t USART_InitSync_TypeDef::baudrate

Desired baud rate.


databits#

USART_Databits_TypeDef USART_InitSync_TypeDef::databits

Number of data bits in frame.


master#

bool USART_InitSync_TypeDef::master

Select if to operate in master or slave mode.


msbf#

bool USART_InitSync_TypeDef::msbf

Select if to send most or least significant bit first.


clockMode#

USART_ClockMode_TypeDef USART_InitSync_TypeDef::clockMode

Clock polarity/phase mode.


autoCsEnable#

bool USART_InitSync_TypeDef::autoCsEnable

Auto CS enabling.


csInv#

bool USART_InitSync_TypeDef::csInv

Enable CS invert.

By default, chip select is active low. Set to true to make chip select active high.