LESENSE decoder control descriptor structure.

Public Attributes#

Select input to the LESENSE decoder.

uint32_t

Initial state of the LESENSE decoder.

bool

Set to enable decoder to check the present state in addition to the states defined in TCONF.

bool

When set, a transition from state x in decoder will set the interrupt flag CHx.

bool

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.

bool

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.

bool

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.

bool

Set to enable hysteresis in decoder for suppressing the interrupt requests.

bool

Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.

Select PRS channel input for bit 0 of LESENSE decoder.

Select PRS channel input for bit 1 of LESENSE decoder.

Select PRS channel input for bit 2 of LESENSE decoder.

Select PRS channel input for bit 3 of LESENSE decoder.

Public Attribute Documentation#

decInput#

LESENSE_DecInput_TypeDef LESENSE_DecCtrlDesc_TypeDef::decInput

Select input to the LESENSE decoder.


initState#

uint32_t LESENSE_DecCtrlDesc_TypeDef::initState

Initial state of the LESENSE decoder.


chkState#

bool LESENSE_DecCtrlDesc_TypeDef::chkState

Set to enable decoder to check the present state in addition to the states defined in TCONF.


intMap#

bool LESENSE_DecCtrlDesc_TypeDef::intMap

When set, a transition from state x in decoder will set the interrupt flag CHx.


hystPRS0#

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.


hystPRS1#

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.


hystPRS2#

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.


hystIRQ#

bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ

Set to enable hysteresis in decoder for suppressing the interrupt requests.


prsCount#

bool LESENSE_DecCtrlDesc_TypeDef::prsCount

Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.


prsChSel0#

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel0

Select PRS channel input for bit 0 of LESENSE decoder.


prsChSel1#

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel1

Select PRS channel input for bit 1 of LESENSE decoder.


prsChSel2#

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel2

Select PRS channel input for bit 2 of LESENSE decoder.


prsChSel3#

LESENSE_PRSSel_TypeDef LESENSE_DecCtrlDesc_TypeDef::prsChSel3

Select PRS channel input for bit 3 of LESENSE decoder.