QSPI initialization structure.

Public Attributes#

bool

Enable/disable Quad SPI when initialization is completed.

uint8_t

Master mode baud rate divisor.

Public Attribute Documentation#

enable#

bool QSPI_Init_TypeDef::enable

Enable/disable Quad SPI when initialization is completed.


divisor#

uint8_t QSPI_Init_TypeDef::divisor

Master mode baud rate divisor.

Values can be even numbers in the range [2-32] inclusive.