ECC configuration.

Public Attributes#

bool

Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.

uint32_t

Array of 2 DMA channel numbers to use for ECC initialization.

Public Attribute Documentation#

enableEccBank#

bool MSC_EccConfig_TypeDef::enableEccBank[MSC_ECC_BANKS]

Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.


Definition at line 293 of file platform/emlib/inc/em_msc.h

dmaChannels#

uint32_t MSC_EccConfig_TypeDef::dmaChannels[2]

Array of 2 DMA channel numbers to use for ECC initialization.


Definition at line 297 of file platform/emlib/inc/em_msc.h