ACMP initialization structure.

Public Attributes#

bool

Full-bias current.

uint32_t

Bias current.

bool

Enable setting the interrupt flag on the falling edge.

bool

Enable setting the interrupt flag on the rising edge.

ACMP accuracy mode.

Select the power source for the ACMP.

Hysteresis when ACMP output is 0.

Hysteresis when ACMP output is 1.

bool

Inactive value emitted by ACMP during warmup.

bool

If true, ACMP is enabled after configuration.

Public Attribute Documentation#

fullBias#

bool ACMP_Init_TypeDef::fullBias

Full-bias current.

See the ACMP chapter about bias and response time in the reference manual for details.


Definition at line 743 of file platform/emlib/inc/em_acmp.h

biasProg#

uint32_t ACMP_Init_TypeDef::biasProg

Bias current.

See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.


Definition at line 754 of file platform/emlib/inc/em_acmp.h

interruptOnFallingEdge#

bool ACMP_Init_TypeDef::interruptOnFallingEdge

Enable setting the interrupt flag on the falling edge.


Definition at line 758 of file platform/emlib/inc/em_acmp.h

interruptOnRisingEdge#

bool ACMP_Init_TypeDef::interruptOnRisingEdge

Enable setting the interrupt flag on the rising edge.


Definition at line 762 of file platform/emlib/inc/em_acmp.h

inputRange#

ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange

Input range.

Adjust this setting to optimize the performance for a given input voltage range.


Definition at line 769 of file platform/emlib/inc/em_acmp.h

accuracy#

ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy

ACMP accuracy mode.

Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.


Definition at line 777 of file platform/emlib/inc/em_acmp.h

powerSource#

ACMP_PowerSource_TypeDef ACMP_Init_TypeDef::powerSource

Select the power source for the ACMP.


Definition at line 782 of file platform/emlib/inc/em_acmp.h

hysteresisLevel_0#

ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_0

Hysteresis when ACMP output is 0.


Definition at line 797 of file platform/emlib/inc/em_acmp.h

hysteresisLevel_1#

ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_1

Hysteresis when ACMP output is 1.


Definition at line 800 of file platform/emlib/inc/em_acmp.h

vlpInput#

ACMP_VLPInput_Typedef ACMP_Init_TypeDef::vlpInput

VLP Input source.

Select between using VADIV or VBDIV as the VLP source.


Definition at line 806 of file platform/emlib/inc/em_acmp.h

inactiveValue#

bool ACMP_Init_TypeDef::inactiveValue

Inactive value emitted by ACMP during warmup.


Definition at line 810 of file platform/emlib/inc/em_acmp.h

enable#

bool ACMP_Init_TypeDef::enable

If true, ACMP is enabled after configuration.


Definition at line 829 of file platform/emlib/inc/em_acmp.h