ACMP initialization structure.

Public Attributes#

bool

Full-bias current.

uint32_t

Bias current.

bool

Enable setting the interrupt flag on the falling edge.

bool

Enable setting the interrupt flag on the rising edge.

ACMP accuracy mode.

Select the power source for the ACMP.

Hysteresis when ACMP output is 0.

Hysteresis when ACMP output is 1.

bool

Inactive value emitted by ACMP during warmup.

bool

If true, ACMP is enabled after configuration.

Public Attribute Documentation#

fullBias#

bool ACMP_Init_TypeDef::fullBias

Full-bias current.

See the ACMP chapter about bias and response time in the reference manual for details.


biasProg#

uint32_t ACMP_Init_TypeDef::biasProg

Bias current.

See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.


interruptOnFallingEdge#

bool ACMP_Init_TypeDef::interruptOnFallingEdge

Enable setting the interrupt flag on the falling edge.


interruptOnRisingEdge#

bool ACMP_Init_TypeDef::interruptOnRisingEdge

Enable setting the interrupt flag on the rising edge.


inputRange#

ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange

Input range.

Adjust this setting to optimize the performance for a given input voltage range.


accuracy#

ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy

ACMP accuracy mode.

Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.


powerSource#

ACMP_PowerSource_TypeDef ACMP_Init_TypeDef::powerSource

Select the power source for the ACMP.


hysteresisLevel_0#

ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_0

Hysteresis when ACMP output is 0.


hysteresisLevel_1#

ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel_1

Hysteresis when ACMP output is 1.


vlpInput#

ACMP_VLPInput_Typedef ACMP_Init_TypeDef::vlpInput

VLP Input source.

Select between using VADIV or VBDIV as the VLP source.


inactiveValue#

bool ACMP_Init_TypeDef::inactiveValue

Inactive value emitted by ACMP during warmup.


enable#

bool ACMP_Init_TypeDef::enable

If true, ACMP is enabled after configuration.