Channel descriptor structure.
Public Attributes#
Set to enable scan channel CHx.
Set to enable CHx pin.
Enable/disable channel interrupts after configuring all the sensor channel parameters.
Configure channel pin mode for the excitation phase of the scan sequence.
Configure channel pin idle setup in LESENSE idle phase.
Set to use alternate excite pin for excitation.
Set to enable result from this channel being shifted into the decoder register.
Set to invert result bit stored in the SCANRES register.
Set to store counter value in the RAM (accessible via RESDATA) and make the comparison result available in the SCANRES register.
Select clock used for the excitation timing.
Select clock used for the sample delay timing.
Configure the excitation time.
Configure the sample delay.
Configure the measure delay.
Configure the ACMP threshold or the DAC data.
Select if the ACMP output, the ADC output or the counter output should be used in comparison.
Configure the interrupt generation mode for the CHx interrupt flag.
Configure the decision threshold for the sensor data comparison.
Select the mode for counter comparison.
Select the sensor evaluation mode.
Public Attribute Documentation#
enaInt#
bool LESENSE_ChDesc_TypeDef::enaInt
Enable/disable channel interrupts after configuring all the sensor channel parameters.
chPinExMode#
LESENSE_ChPinExMode_TypeDef LESENSE_ChDesc_TypeDef::chPinExMode
Configure channel pin mode for the excitation phase of the scan sequence.
Note: OPAOUT is only available on channels 2, 3, 4, and 5.
chPinIdleMode#
LESENSE_ChPinIdleMode_TypeDef LESENSE_ChDesc_TypeDef::chPinIdleMode
Configure channel pin idle setup in LESENSE idle phase.
shiftRes#
bool LESENSE_ChDesc_TypeDef::shiftRes
Set to enable result from this channel being shifted into the decoder register.
storeCntRes#
bool LESENSE_ChDesc_TypeDef::storeCntRes
Set to store counter value in the RAM (accessible via RESDATA) and make the comparison result available in the SCANRES register.
exClk#
LESENSE_ChClk_TypeDef LESENSE_ChDesc_TypeDef::exClk
Select clock used for the excitation timing.
sampleClk#
LESENSE_ChClk_TypeDef LESENSE_ChDesc_TypeDef::sampleClk
Select clock used for the sample delay timing.
exTime#
uint8_t LESENSE_ChDesc_TypeDef::exTime
Configure the excitation time.
Excitation will last exTime+1 excitation clock cycles. Valid range: 0-63 (6 bits).
sampleDelay#
uint8_t LESENSE_ChDesc_TypeDef::sampleDelay
Configure the sample delay.
Sampling will occur after sampleDelay+1 sample clock cycles. Valid range: 0-127 (7 bits) or 0-255 (8 bits) depending on device.
measDelay#
uint16_t LESENSE_ChDesc_TypeDef::measDelay
Configure the measure delay.
Sensor measuring is delayed for measDelay excitation clock cycles. Valid range: 0-127 (7 bits) or 0-1023 (10 bits) depending on device.
acmpThres#
uint16_t LESENSE_ChDesc_TypeDef::acmpThres
Configure the ACMP threshold or the DAC data.
If perCtrl.dacCh0Data or perCtrl.dacCh1Data is set to lesenseDACIfData, acmpThres defines the 12-bit DAC data in the corresponding data register of DAC interface (DACn_CH0DATA and DACn_CH1DATA). In this case, the valid range is: 0-4095 (12 bits). If perCtrl.dacCh0Data or perCtrl.dacCh1Data is set to lesenseACMPThres, acmpThres defines the 6-bit Vdd scaling factor of ACMP negative input (VDDLEVEL in ACMP_INPUTSEL register). In this case, the valid range is: 0-63 (6 bits).
sampleMode#
LESENSE_ChSampleMode_TypeDef LESENSE_ChDesc_TypeDef::sampleMode
Select if the ACMP output, the ADC output or the counter output should be used in comparison.
intMode#
LESENSE_ChIntMode_TypeDef LESENSE_ChDesc_TypeDef::intMode
Configure the interrupt generation mode for the CHx interrupt flag.
cntThres#
uint16_t LESENSE_ChDesc_TypeDef::cntThres
Configure the decision threshold for the sensor data comparison.
Valid range: 0-65535 (16 bits).
compMode#
LESENSE_ChCompMode_TypeDef LESENSE_ChDesc_TypeDef::compMode
Select the mode for counter comparison.
evalMode#
LESENSE_ChEvalMode_TypeDef LESENSE_ChDesc_TypeDef::evalMode
Select the sensor evaluation mode.