Initialization structure.

Public Attributes#

Specifies whether TX and/or RX will be enabled when initialization completes.

uint32_t

EUSART reference clock assumed when configuring baud rate setup.

uint32_t

Desired baud rate.

Number of data bits in frame.

Parity mode to use.

Number of stop bits to use.

Majority Vote can be disabled for 16x, 8x and 6x oversampling modes.

Enable Loop Back configuration.

Advanced initialization structure pointer. It can be NULL.

Public Attribute Documentation#

enable#

EUSART_Enable_TypeDef EUSART_UartInit_TypeDef::enable

Specifies whether TX and/or RX will be enabled when initialization completes.


Definition at line 467 of file platform/emlib/inc/em_eusart.h

refFreq#

uint32_t EUSART_UartInit_TypeDef::refFreq

EUSART reference clock assumed when configuring baud rate setup.

Set to 0 if using currently configured reference clock.


Definition at line 471 of file platform/emlib/inc/em_eusart.h

baudrate#

uint32_t EUSART_UartInit_TypeDef::baudrate

Desired baud rate.

If set to 0, Auto Baud feature is enabled and the EUSART will wait for (0x55) frame to detect the Baudrate.


Definition at line 475 of file platform/emlib/inc/em_eusart.h

oversampling#

EUSART_OVS_TypeDef EUSART_UartInit_TypeDef::oversampling

Oversampling used.


Definition at line 478 of file platform/emlib/inc/em_eusart.h

databits#

EUSART_Databits_TypeDef EUSART_UartInit_TypeDef::databits

Number of data bits in frame.


Definition at line 481 of file platform/emlib/inc/em_eusart.h

parity#

EUSART_Parity_TypeDef EUSART_UartInit_TypeDef::parity

Parity mode to use.


Definition at line 484 of file platform/emlib/inc/em_eusart.h

stopbits#

EUSART_Stopbits_TypeDef EUSART_UartInit_TypeDef::stopbits

Number of stop bits to use.


Definition at line 487 of file platform/emlib/inc/em_eusart.h

majorityVote#

EUSART_MajorityVote_TypeDef EUSART_UartInit_TypeDef::majorityVote

Majority Vote can be disabled for 16x, 8x and 6x oversampling modes.


Definition at line 490 of file platform/emlib/inc/em_eusart.h

loopbackEnable#

EUSART_LoopbackEnable_TypeDef EUSART_UartInit_TypeDef::loopbackEnable

Enable Loop Back configuration.


Definition at line 493 of file platform/emlib/inc/em_eusart.h

advancedSettings#

EUSART_AdvancedInit_TypeDef* EUSART_UartInit_TypeDef::advancedSettings

Advanced initialization structure pointer. It can be NULL.


Definition at line 496 of file platform/emlib/inc/em_eusart.h