SE Command structure to which all commands to the SE must adhere.

Public Attributes#

uint32_t

SE Command.

uint32_t

Parameters.

size_t

Number of parameters.

Public Attribute Documentation#

command#

uint32_t SE_Command_t::command

SE Command.


data_in#

SE_DataTransfer_t* SE_Command_t::data_in

Input data.


data_out#

SE_DataTransfer_t* SE_Command_t::data_out

Output data.


parameters#

uint32_t SE_Command_t::parameters[SE_MAX_PARAMETERS]

Parameters.


num_parameters#

size_t SE_Command_t::num_parameters

Number of parameters.