RTCC - Real Timer Counter/Calendar#

Real Time Counter and Calendar (RTCC) Peripheral API.

This module contains functions to control the RTCC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTCC ensures timekeeping in low energy modes. The RTCC also includes a BCD calendar mode for easy time and date keeping.

Modules#

RTCC_Init_TypeDef

RTCC_CCChConf_TypeDef

Enumerations#

enum
rtccCntPresc_1 = _RTCC_CFG_CNTPRESC_DIV1
rtccCntPresc_2 = _RTCC_CFG_CNTPRESC_DIV2
rtccCntPresc_4 = _RTCC_CFG_CNTPRESC_DIV4
rtccCntPresc_8 = _RTCC_CFG_CNTPRESC_DIV8
rtccCntPresc_16 = _RTCC_CFG_CNTPRESC_DIV16
rtccCntPresc_32 = _RTCC_CFG_CNTPRESC_DIV32
rtccCntPresc_64 = _RTCC_CFG_CNTPRESC_DIV64
rtccCntPresc_128 = _RTCC_CFG_CNTPRESC_DIV128
rtccCntPresc_256 = _RTCC_CFG_CNTPRESC_DIV256
rtccCntPresc_512 = _RTCC_CFG_CNTPRESC_DIV512
rtccCntPresc_1024 = _RTCC_CFG_CNTPRESC_DIV1024
rtccCntPresc_2048 = _RTCC_CFG_CNTPRESC_DIV2048
rtccCntPresc_4096 = _RTCC_CFG_CNTPRESC_DIV4096
rtccCntPresc_8192 = _RTCC_CFG_CNTPRESC_DIV8192
rtccCntPresc_16384 = _RTCC_CFG_CNTPRESC_DIV16384
rtccCntPresc_32768 = _RTCC_CFG_CNTPRESC_DIV32768
}

Counter prescaler selection.

enum
rtccCntTickPresc = _RTCC_CFG_CNTTICK_PRESC
rtccCntTickCCV0Match = _RTCC_CFG_CNTTICK_CCV0MATCH
}

Prescaler mode of the RTCC counter.

enum
rtccCapComChModeOff = _RTCC_CC_CTRL_MODE_OFF
rtccCapComChModeCapture = _RTCC_CC_CTRL_MODE_INPUTCAPTURE
rtccCapComChModeCompare = _RTCC_CC_CTRL_MODE_OUTPUTCOMPARE
}

Capture/Compare channel mode.

enum
rtccCompMatchOutActionPulse = _RTCC_CC_CTRL_CMOA_PULSE
rtccCompMatchOutActionToggle = _RTCC_CC_CTRL_CMOA_TOGGLE
rtccCompMatchOutActionClear = _RTCC_CC_CTRL_CMOA_CLEAR
rtccCompMatchOutActionSet = _RTCC_CC_CTRL_CMOA_SET
}

Compare match output action mode.

enum
rtccInEdgeRising = _RTCC_CC_CTRL_ICEDGE_RISING
rtccInEdgeFalling = _RTCC_CC_CTRL_ICEDGE_FALLING
rtccInEdgeBoth = _RTCC_CC_CTRL_ICEDGE_BOTH
rtccInEdgeNone = _RTCC_CC_CTRL_ICEDGE_NONE
}

Input edge select.

enum
rtccCompBaseCnt = _RTCC_CC_CTRL_COMPBASE_CNT
rtccCompBasePreCnt = _RTCC_CC_CTRL_COMPBASE_PRECNT
}

Capture/Compare channel compare mode.

Typedefs#

typedef uint8_t

PRS channel number.

Functions#

void
RTCC_ChannelInit(int ch, RTCC_CCChConf_TypeDef const *confPtr)

Configure the selected capture/compare channel of the RTCC.

void
RTCC_Enable(bool enable)

Enable/disable RTCC counting.

void
RTCC_Init(const RTCC_Init_TypeDef *init)

Initialize RTCC.

void

Restore RTCC to its reset state.

void

Clear the STATUS register.

uint32_t

Get the RTCC compare register value for a selected channel.

void
RTCC_ChannelCompareValueSet(int ch, uint32_t value)

Set the RTCC compare register value for a selected channel.

uint32_t

Get the RTCC input capture register value for a selected channel.

uint32_t

Get the RTCC capture/compare register value for a selected channel.

void
RTCC_ChannelCCVSet(int ch, uint32_t value)

Set RTCC capture/compare register value for a selected channel.

uint32_t

Get the combined CNT/PRECNT register content.

uint32_t

Get the RTCC counter value.

void
RTCC_CounterSet(uint32_t value)

Set the RTCC CNT counter.

void
RTCC_IntClear(uint32_t flags)

Clear one or more pending RTCC interrupts.

void
RTCC_IntDisable(uint32_t flags)

Disable one or more RTCC interrupts.

void
RTCC_IntEnable(uint32_t flags)

Enable one or more RTCC interrupts.

uint32_t

Get pending RTCC interrupt flags.

uint32_t

Get enabled and pending RTCC interrupt flags.

void
RTCC_IntSet(uint32_t flags)

Set one or more pending RTCC interrupts from SW.

void
RTCC_Lock(void)

Lock RTCC registers.

uint32_t

Get the RTCC pre-counter value.

void
RTCC_PreCounterSet(uint32_t preCntVal)

Set the RTCC pre-counter value.

uint32_t

Get the STATUS register value.

void

Wait for the RTCC to complete all synchronization of register changes and commands.

void

Start the RTCC counter.

void
RTCC_Stop(void)

Stop the RTCC counter.

void

Unlock RTCC registers.

Macros#

#define
RTCC_INIT_DEFAULT undefined

Default RTCC initialization structure.

#define
RTCC_CH_INIT_COMPARE_DEFAULT undefined

Default RTCC channel output compare initialization structure.

#define
RTCC_CH_INIT_CAPTURE_DEFAULT undefined

Default RTCC channel input capture initialization structure.

#define
RTCC_CH_VALID (ch)

Number of RTCC capture/compare channels.

Enumeration Documentation#

RTCC_CntPresc_TypeDef#

RTCC_CntPresc_TypeDef

Counter prescaler selection.

Enumerator
rtccCntPresc_1

Divide clock by 1.

rtccCntPresc_2

Divide clock by 2.

rtccCntPresc_4

Divide clock by 4.

rtccCntPresc_8

Divide clock by 8.

rtccCntPresc_16

Divide clock by 16.

rtccCntPresc_32

Divide clock by 32.

rtccCntPresc_64

Divide clock by 64.

rtccCntPresc_128

Divide clock by 128.

rtccCntPresc_256

Divide clock by 256.

rtccCntPresc_512

Divide clock by 512.

rtccCntPresc_1024

Divide clock by 1024.

rtccCntPresc_2048

Divide clock by 2048.

rtccCntPresc_4096

Divide clock by 4096.

rtccCntPresc_8192

Divide clock by 8192.

rtccCntPresc_16384

Divide clock by 16384.

rtccCntPresc_32768

Divide clock by 32768.


RTCC_PrescMode_TypeDef#

RTCC_PrescMode_TypeDef

Prescaler mode of the RTCC counter.

Enumerator
rtccCntTickPresc

CNT register ticks according to the prescaler value.

rtccCntTickCCV0Match

CNT register ticks when PRECNT matches the 15 least significant bits of ch.


RTCC_CapComChMode_TypeDef#

RTCC_CapComChMode_TypeDef

Capture/Compare channel mode.

Enumerator
rtccCapComChModeOff

Capture/Compare channel turned off.

rtccCapComChModeCapture

Capture mode.

rtccCapComChModeCompare

Compare mode.


RTCC_CompMatchOutAction_TypeDef#

RTCC_CompMatchOutAction_TypeDef

Compare match output action mode.

Enumerator
rtccCompMatchOutActionPulse

Generate a pulse.

rtccCompMatchOutActionToggle

Toggle output.

rtccCompMatchOutActionClear

Clear output.

rtccCompMatchOutActionSet

Set output.


RTCC_InEdgeSel_TypeDef#

RTCC_InEdgeSel_TypeDef

Input edge select.

Enumerator
rtccInEdgeRising

Rising edges detected.

rtccInEdgeFalling

Falling edges detected.

rtccInEdgeBoth

Both edges detected.

rtccInEdgeNone

No edge detection, signal is left as is.


RTCC_CompBase_TypeDef#

RTCC_CompBase_TypeDef

Capture/Compare channel compare mode.

Enumerator
rtccCompBaseCnt

CCVx is compared with the CNT register.

rtccCompBasePreCnt

CCVx is compared with a CNT[16:0] and PRECNT[14:0].


Typedef Documentation#

RTCC_PRSSel_TypeDef#

typedef uint8_t RTCC_PRSSel_TypeDef

PRS channel number.

This type is used when configuring input capture mode on a RTCC channel.


Function Documentation#

RTCC_ChannelInit#

void RTCC_ChannelInit (int ch, RTCC_CCChConf_TypeDef const * confPtr)

Configure the selected capture/compare channel of the RTCC.

Parameters
TypeDirectionArgument NameDescription
int[in]ch

A channel selector.

RTCC_CCChConf_TypeDef const *[in]confPtr

A pointer to the configuration structure.

Use this function to configure an RTCC channel. Select capture/compare mode, match output action, overflow output action, and PRS input configuration. See the configuration structure RTCC_CCChConf_TypeDef for more details.


RTCC_Enable#

void RTCC_Enable (bool enable)

Enable/disable RTCC counting.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

True to enable RTCC counting, false to disable counting.


RTCC_Init#

void RTCC_Init (const RTCC_Init_TypeDef * init)

Initialize RTCC.

Parameters
TypeDirectionArgument NameDescription
const RTCC_Init_TypeDef *[in]init

A pointer to the RTCC initialization structure.

Note that the compare values must be set separately with RTCC_CompareSet(), which should probably be done prior to the use of this function if configuring the RTCC to start when initialization is completed.


RTCC_Reset#

void RTCC_Reset (void )

Restore RTCC to its reset state.

Parameters
TypeDirectionArgument NameDescription
voidN/A

RTCC_StatusClear#

void RTCC_StatusClear (void )

Clear the STATUS register.

Parameters
TypeDirectionArgument NameDescription
voidN/A

RTCC_ChannelCompareValueGet#

uint32_t RTCC_ChannelCompareValueGet (int ch)

Get the RTCC compare register value for a selected channel.

Parameters
TypeDirectionArgument NameDescription
int[in]ch

Channel selector.

Returns

  • Compare register value.


RTCC_ChannelCompareValueSet#

void RTCC_ChannelCompareValueSet (int ch, uint32_t value)

Set the RTCC compare register value for a selected channel.

Parameters
TypeDirectionArgument NameDescription
int[in]ch

Channel selector.

uint32_t[in]value

Compare register value


RTCC_ChannelCaptureValueGet#

uint32_t RTCC_ChannelCaptureValueGet (int ch)

Get the RTCC input capture register value for a selected channel.

Parameters
TypeDirectionArgument NameDescription
int[in]ch

Channel selector.

Returns

  • Capture register value.


RTCC_ChannelCCVGet#

uint32_t RTCC_ChannelCCVGet (int ch)

Get the RTCC capture/compare register value for a selected channel.

Parameters
TypeDirectionArgument NameDescription
int[in]ch

Channel selector.

For parts with separate capture compare value registers, this function returns the compare value.

Returns

  • Capture/compare register value.


RTCC_ChannelCCVSet#

void RTCC_ChannelCCVSet (int ch, uint32_t value)

Set RTCC capture/compare register value for a selected channel.

Parameters
TypeDirectionArgument NameDescription
int[in]ch

Channel selector.

uint32_t[in]value

Capture/compare register value

For parts with separate capture compare value registers, this function sets the compare value.


RTCC_CombinedCounterGet#

uint32_t RTCC_CombinedCounterGet (void )

Get the combined CNT/PRECNT register content.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • CNT/PRECNT register value.


RTCC_CounterGet#

uint32_t RTCC_CounterGet (void )

Get the RTCC counter value.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Current RTCC counter value.


RTCC_CounterSet#

void RTCC_CounterSet (uint32_t value)

Set the RTCC CNT counter.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]value

CNT value.


RTCC_IntClear#

void RTCC_IntClear (uint32_t flags)

Clear one or more pending RTCC interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

RTCC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources.


RTCC_IntDisable#

void RTCC_IntDisable (uint32_t flags)

Disable one or more RTCC interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

RTCC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt.


RTCC_IntEnable#

void RTCC_IntEnable (uint32_t flags)

Enable one or more RTCC interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

RTCC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using RTCC_IntClear() prior to enabling the interrupt.


RTCC_IntGet#

uint32_t RTCC_IntGet (void )

Get pending RTCC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Event bits are not cleared by using this function.

Returns

  • Pending RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.


RTCC_IntGetEnabled#

uint32_t RTCC_IntGetEnabled (void )

Get enabled and pending RTCC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Useful for handling more interrupt sources in the same interrupt handler.

Returns

  • Pending and enabled RTCC interrupt sources. Returns a set of interrupt flags OR-ed together for the interrupt sources set.


RTCC_IntSet#

void RTCC_IntSet (uint32_t flags)

Set one or more pending RTCC interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

RTCC interrupt sources to set to pending. Use a set of interrupt flags (RTCC_IFS_nnn).


RTCC_Lock#

void RTCC_Lock (void )

Lock RTCC registers.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.


RTCC_PreCounterGet#

uint32_t RTCC_PreCounterGet (void )

Get the RTCC pre-counter value.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Current RTCC pre-counter value.


RTCC_PreCounterSet#

void RTCC_PreCounterSet (uint32_t preCntVal)

Set the RTCC pre-counter value.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]preCntVal

RTCC pre-counter value to be set.


RTCC_StatusGet#

uint32_t RTCC_StatusGet (void )

Get the STATUS register value.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Current STATUS register value.


RTCC_SyncWait#

void RTCC_SyncWait (void )

Wait for the RTCC to complete all synchronization of register changes and commands.

Parameters
TypeDirectionArgument NameDescription
voidN/A

RTCC_Start#

void RTCC_Start (void )

Start the RTCC counter.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will send a start command to the RTCC peripheral. The RTCC peripheral will use some LF clock ticks before the command is executed. The RTCC_SyncWait() function can be used to wait for the start command to be executed.

Note

  • This function requires the RTCC to be enabled.


RTCC_Stop#

void RTCC_Stop (void )

Stop the RTCC counter.

Parameters
TypeDirectionArgument NameDescription
voidN/A

This function will send a stop command to the RTCC peripheral. The RTCC peripheral will use some LF clock ticks before the command is executed. The RTCC_SyncWait() function can be used to wait for the stop command to be executed.

Note

  • This function requires the RTCC to be enabled.


RTCC_Unlock#

void RTCC_Unlock (void )

Unlock RTCC registers.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • When RTCC registers are locked, RTCC_CTRL, RTCC_PRECNT, RTCC_CNT, RTCC_TIME, RTCC_DATE, RTCC_IEN, RTCC_POWERDOWN and RTCC_CCx_XXX registers cannot be written to.