LESENSE decoder control descriptor structure.

Public Attributes#

bool

Set to enable decoder to check the present state in addition to the states defined in TCONF.

bool

When set, a transition from state x in decoder will set the interrupt flag CHx.

bool

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.

bool

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.

bool

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.

bool

Set to enable hysteresis in decoder for suppressing the interrupt requests.

bool

Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.

Public Attribute Documentation#

chkState#

bool LESENSE_DecCtrlDesc_TypeDef::chkState

Set to enable decoder to check the present state in addition to the states defined in TCONF.


intMap#

bool LESENSE_DecCtrlDesc_TypeDef::intMap

When set, a transition from state x in decoder will set the interrupt flag CHx.


hystPRS0#

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS0

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 0.


hystPRS1#

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS1

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 1.


hystPRS2#

bool LESENSE_DecCtrlDesc_TypeDef::hystPRS2

Set to enable hysteresis in decoder for suppressing the changes on PRS channel 2.


hystIRQ#

bool LESENSE_DecCtrlDesc_TypeDef::hystIRQ

Set to enable hysteresis in decoder for suppressing the interrupt requests.


prsCount#

bool LESENSE_DecCtrlDesc_TypeDef::prsCount

Set to enable count mode on decoder PRS channels 0 and 1 to produce outputs which can be used by a PCNT to count up or down.