Standalone Bootloader#

Definition of the standalone bootloader interface.

Some functions in this file return an ::EmberStatus value. See error-def.h for definitions of all ::EmberStatus return values.

See bootloader-interface-standalone.h for source code.

Functions#

uint16_t

Detects if the standalone bootloader is installed, and if so returns the installed version.

EmberStatus

Quits the current application and launches the standalone bootloader (if installed).

Macros#

#define
NO_BOOTLOADER_MODE 0xFF

Define a numerical value for NO BOOTLOADER mode.

#define
STANDALONE_BOOTLOADER_NORMAL_MODE 1

Define a numerical value for the normal bootloader mode.

#define
STANDALONE_BOOTLOADER_RECOVERY_MODE 0

Define a numerical value for the recovery bootloader mode.

Function Documentation#

halGetStandaloneBootloaderVersion#

uint16_t halGetStandaloneBootloaderVersion (void )

Detects if the standalone bootloader is installed, and if so returns the installed version.

Parameters
N/A

A returned version of 0x1234 would indicate version 1.2 build 34

Returns


Definition at line 44 of file platform/service/legacy_hal/inc/bootloader-interface-standalone.h

halLaunchStandaloneBootloader#

EmberStatus halLaunchStandaloneBootloader (uint8_t mode)

Quits the current application and launches the standalone bootloader (if installed).

Parameters
N/Amode

Controls the mode in which the standalone bootloader will run. See the bootloader Application Note for full details. Options are:

Both modes also allow an image transfer to begin via serial xmodem.

The function returns an error if the standalone bootloader is not present.

Returns

  • An ::EmberStatus error if the standalone bootloader is not present, or ::EMBER_SUCCESS.


Definition at line 77 of file platform/service/legacy_hal/inc/bootloader-interface-standalone.h