Status Codes#
Status Codes contains error and status code definitions used by GSDK software components and stacks. This module also provides routines to read the string linked with the error and status codes.
Typedefs#
define global status variable.
Functions#
Macros#
sl status space mask.
sl status generic space.
sl status platform 1 space.
sl status platform 2 space.
sl status hardware space.
sl status bluetooth space.
sl status bluetooth mesh space.
sl status can canopen space.
sl status connect space.
sl status net suite space.
sl status thread space.
sl status usb space.
sl status wifi space.
sl status zigbee space.
sl status z wave space.
sl status gecko os 1 space.
sl status gecko os 2 space.
sl status bluetooth ctrl space.
sl status bluetooth att space.
sl status bluetooth mesh foundation space.
sl status bluetooth mesh foundation space.
sl status wisun space.
sl status compute space.
No error.
Generic error.
Generic invalid state error.
Module is not ready for requested operation.
Module is busy and cannot carry out requested operation.
Operation is in progress and not yet complete (pass or fail).
Operation aborted.
Operation timed out.
Operation not allowed per permissions.
Non-blocking operation would block.
Operation/module is Idle, cannot carry requested operation.
Operation cannot be done while construct is waiting.
No task/construct waiting/pending for that action/event.
Operation cannot be done while construct is suspended.
Feature not available due to software configuration.
Feature not supported.
Initialization failed.
Module has not been initialized.
Module has already been initialized.
Object/construct has been deleted.
Illegal call from ISR.
Illegal call because network is up.
Illegal call because network is down.
Failure due to not being joined in a network.
Invalid operation as there are no beacons.
Generic allocation error.
No more resource available to perform the operation.
Item/list/queue is empty.
Item/list/queue is full.
Item would overflow.
Item/list/queue has been overflowed.
Generic ownership error.
Already/still owning resource.
Generic invalid argument or consequence of invalid argument.
Invalid null pointer received as argument.
Invalid configuration provided.
Invalid mode.
Invalid handle.
Invalid type for operation.
Invalid index.
Invalid range.
Invalid key.
Invalid credentials.
Invalid count.
Invalid signature / verification failed.
Item could not be found.
Item already exists.
Generic I/O failure.
I/O failure due to timeout.
Generic transmission error.
Transmit underflowed.
Transmit is incomplete.
Transmit is busy.
Generic reception error.
Failed to read on/via given object.
Failed to write on/via given object.
Message is too long.
EEPROM MFG version mismatch.
EEPROM Stack version mismatch.
Flash write is inhibited.
Flash verification failed.
Flash programming failed.
Flash erase failed.
MAC no data.
MAC no ACK received.
MAC indirect timeout.
MAC unknown header type.
MAC ACK unknown header type.
MAC command transmit failure.
Error in open NVM.
Image checksum is not valid.
Decryption failed.
Command was not recognized.
Command or parameter maximum length exceeded.
Data received does not form a complete command.
Bus error, e.g. invalid DMA address.
CCA failure.
MAC scanning.
MAC incorrect scan type.
Invalid channel mask.
Bad scan duration.
Bonding procedure can't be started because device has no space left for bond.
Unspecified error.
Hardware failure.
The bonding does not exist.
Error using crypto functions.
Data was corrupted.
Invalid periodic advertising sync handle.
Bluetooth cannot be used on this hardware.
Error received from radio.
Returned when remote disconnects the connection-oriented channel by sending disconnection request.
Returned when local host disconnect the connection-oriented channel by sending disconnection request.
Returned when local host did not find a connection-oriented channel with given destination CID.
Returned when connection-oriented channel disconnected due to LE connection is dropped.
Returned when connection-oriented channel disconnected due to remote end send data even without credit.
Returned when connection-oriented channel disconnected due to remote end send flow control credits exceed 65535.
Returned when connection-oriented channel has run out of flow control credit and local application still trying to send data.
Returned when connection-oriented channel has not received connection response message within maximum timeout.
Returned when local host received a connection-oriented channel connection response with an invalid destination CID.
Returned when local host application tries to send a command which is not suitable for L2CAP channel's current state.
Flash reserved for PS store is full.
PS key not found.
Mismatched or insufficient security level.
Encryption/decryption operation failed.
Connection does not exist, or connection open request was cancelled.
Pairing or authentication failed due to incorrect results in the pairing or authentication procedure. This could be due to an incorrect PIN or Link Key.
Pairing failed because of missing PIN, or authentication failed because of missing Key.
Controller is out of memory.
Link supervision timeout has expired.
Controller is at limit of connections it can support.
The Synchronous Connection Limit to a Device Exceeded error code indicates that the Controller has reached the limit to the number of synchronous connections that can be achieved to a device.
The ACL Connection Already Exists error code indicates that an attempt to create a new ACL Connection to a device when there is already a connection to this device.
Command requested cannot be executed because the Controller is in a state where it cannot process this command at this time.
The Connection Rejected Due To Limited Resources error code indicates that an incoming connection was rejected due to limited resources.
The Connection Rejected Due To Security Reasons error code indicates that a connection was rejected due to security requirements not being fulfilled, like authentication or pairing.
The Connection was rejected because this device does not accept the BD_ADDR. This may be because the device will only accept connections from specific BD_ADDRs.
The Connection Accept Timeout has been exceeded for this connection attempt.
A feature or parameter value in the HCI command is not supported.
Command contained invalid parameters.
User on the remote device terminated the connection.
The remote device terminated the connection because of low resources.
Remote Device Terminated Connection due to Power Off.
Local device terminated the connection.
The Controller is disallowing an authentication or pairing procedure because too little time has elapsed since the last authentication or pairing attempt failed.
The device does not allow pairing. This can be for example, when a device only allows pairing during a certain time window after some user input allows pairing.
The remote device does not support the feature associated with the issued command.
No other error code specified is appropriate to use.
Connection terminated due to link-layer procedure timeout.
LL procedure has collided with the same transaction or procedure that is already in progress.
The requested encryption mode is not acceptable at this time.
Link key cannot be changed because a fixed unit key is being used.
LMP PDU or LL PDU that includes an instant cannot be performed because the instant when this would have occurred has passed.
It was not possible to pair as a unit key was requested and it is not supported.
LMP transaction was started that collides with an ongoing transaction.
The Controller cannot perform channel assessment because it is not supported.
The HCI command or LMP PDU sent is only possible on an encrypted link.
A parameter value requested is outside the mandatory range of parameters for the given HCI command or LMP PDU.
The IO capabilities request or response was rejected because the sending Host does not support Secure Simple Pairing even though the receiving Link Manager does.
The Host is busy with another pairing operation and unable to support the requested pairing. The receiving device should retry pairing again later.
The Controller could not calculate an appropriate value for the Channel selection operation.
Operation was rejected because the controller is busy and unable to process the request.
Remote device terminated the connection because of an unacceptable connection interval.
Advertising for a fixed duration completed or, for directed advertising, that advertising completed without a connection being created.
Connection was terminated because the Message Integrity Check (MIC) failed on a received packet.
LL initiated a connection but the connection has failed to be established. Controller did not receive any packets from remote end.
The MAC of the 802.11 AMP was requested to connect to a peer, but the connection failed.
The master, at this time, is unable to make a coarse adjustment to the piconet clock, using the supplied parameters. Instead the master will attempt to move the clock using clock dragging.
A command was sent from the Host that should identify an Advertising or Sync handle, but the Advertising or Sync handle does not exist.
Number of operations requested has been reached and has indicated the completion of the activity (e.g., advertising or scanning).
A request to the Controller issued by the Host and still pending was successfully canceled.
An attempt was made to send or receive a packet that exceeds the maximum allowed packet l.
The attribute handle given was not valid on this server.
The attribute cannot be read.
The attribute cannot be written.
The attribute PDU was invalid.
The attribute requires authentication before it can be read or written.
Attribute Server does not support the request received from the client.
Offset specified was past the end of the attribute.
The attribute requires authorization before it can be read or written.
Too many prepare writes have been queued.
No attribute found within the given attribute handle range.
The attribute cannot be read or written using the Read Blob Request.
The Encryption Key Size used for encrypting this link is insufficient.
The attribute value length is invalid for the operation.
The attribute request that was requested has encountered an error that was unlikely, and therefore could not be completed as requested.
The attribute requires encryption before it can be read or written.
The attribute type is not a supported grouping attribute as defined by a higher layer specification.
Insufficient Resources to complete the request.
The server requests the client to rediscover the database.
The attribute parameter value was not allowed.
When this is returned in a BGAPI response, the application tried to read or write the value of a user attribute from the GATT database.
The requested write operation cannot be fulfilled for reasons other than permissions.
The Client Characteristic Configuration descriptor is not configured according to the requirements of the profile or service.
The profile or service request cannot be serviced because an operation that has been previously triggered is still in progress.
The attribute value is out of range as defined by a profile or service specification.
The user input of passkey failed, for example, the user cancelled the operation.
Out of Band data is not available for authentication.
The pairing procedure cannot be performed as authentication requirements cannot be met due to IO capabilities of one or both devices.
The confirm value does not match the calculated compare value.
Pairing is not supported by the device.
The resultant encryption key size is insufficient for the security requirements of this device.
The SMP command received is not supported on this device.
Pairing failed due to an unspecified reason.
Pairing or authentication procedure is disallowed because too little time has elapsed since last pairing request or security request.
The Invalid Parameters error code indicates: the command length is invalid or a parameter is outside of the specified range.
Indicates to the remote device that the DHKey Check value received doesn't match the one calculated by the local device.
Indicates that the confirm values in the numeric comparison protocol do not match.
Indicates that the pairing over the LE transport failed due to a Pairing Request sent over the BR/EDR transport in process.
Indicates that the BR/EDR Link Key generated on the BR/EDR transport cannot be used to derive and distribute keys for the LE transport.
Indicates that the device chose not to accept a distributed key.
Returned when trying to add a key or some other unique resource with an ID which already exists.
Returned when trying to manipulate a key or some other resource with an ID which does not exist.
Returned when an operation cannot be executed because a pre-configured limit for keys, key bindings, elements, models, virtual addresses, provisioned devices, or provisioning sessions is reached.
Returned when trying to use a reserved address or add a "pre-provisioned" device using an address already used by some other device.
In a BGAPI response, the user supplied malformed data; in a BGAPI event, the remote end responded with malformed or unrecognized data.
An attempt was made to initialize a subsystem that was already initialized.
An attempt was made to use a subsystem that wasn't initialized yet. Call the subsystem's init function first.
Returned when trying to establish a friendship as a Low Power Node, but no acceptable friend offer message was received.
Provisioning link was unexpectedly closed before provisioning was complete.
An unrecognized provisioning PDU was received.
A provisioning PDU with wrong length or containing field values that are out of bounds was received.
An unexpected (out of sequence) provisioning PDU was received.
The computed confirmation value did not match the expected value.
Provisioning could not be continued due to insufficient resources.
The provisioning data block could not be decrypted.
An unexpected error happened during provisioning.
Device could not assign unicast addresses to all of its elements.
Returned when trying to reuse an address of a previously deleted device before an IV Index Update has been executed.
Returned when trying to assign an address that is used by one of the devices in the Device Database, or by the Provisioner itself.
Application key or publish address are not set.
Application key is not bound to a model.
Returned when address in request was not valid.
Returned when model identified is not found for a given element.
Returned when the key identified by AppKeyIndex is not stored in the node.
Returned when the key identified by NetKeyIndex is not stored in the node.
Returned when The node cannot serve the request due to insufficient resources.
Returned when the key identified is already stored in the node and the new NetKey value is different.
Returned when the model does not support the publish mechanism.
Returned when the model does not support the subscribe mechanism.
Returned when storing of the requested parameters failed.
Returned when requested setting is not supported.
Returned when the requested update operation cannot be performed due to general constraints.
Returned when the requested delete operation cannot be performed due to general constraints.
Returned when the requested bind operation cannot be performed due to general constraints.
Returned when The node cannot start advertising with Node Identity or Proxy since the maximum number of parallel advertising is reached.
Returned when the requested state cannot be set.
Returned when an unspecified error took place.
Returned when the NetKeyIndex and AppKeyIndex combination is not valid for a Config AppKey Update.
Invalid firmware keyset.
The firmware download took too long.
Unknown request ID or wrong interface ID used.
The request is successful but some parameters have been ignored.
No Packets waiting to be received.
The sleep mode is granted.
The WFx does not go back to sleep.
The SecureLink MAC key was not found.
The SecureLink MAC key is already installed in OTP.
The SecureLink MAC key cannot be installed in RAM.
The SecureLink MAC key installation failed.
SecureLink key (re)negotiation failed.
The device is in an inappropriate state to perform the request.
The request failed due to regulatory limitations.
The connection request failed because no suitable AP was found.
The connection request was aborted by host.
The connection request failed because of a timeout.
The connection request failed because the AP rejected the device.
The connection request failed because the WPA handshake did not complete successfully.
The request failed because the retry limit was exceeded.
The request failed because the MSDU life time was exceeded.
Critical fault.
ALU operation output NaN.
ALU numeric overflow.
ALU numeric underflow.
Overflow during array store.
Underflow during array store conversion.
Infinity encountered during array store conversion.
NaN encountered during array store conversion.
MATH NaN encountered.
MATH Infinity encountered.
MATH numeric overflow.
MATH numeric underflow.
Function Documentation#
sl_status_get_string_n#
int32_t sl_status_get_string_n (sl_status_t status, char * buffer, uint32_t buffer_length)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_status_t | N/A | status | The status code from which to obtain the status string. |
| char * | N/A | buffer | Pointer to a buffer in which the status string will be copied. A terminating null-character will be appended after the copied status string. |
| uint32_t | N/A | buffer_length | Maximum number of characters that can be written in the buffer, including the terminating null-character. If the status string would be longer than the available length, it will be truncated and a null-terminating character will be the last character contained in the buffer. |
Get a copy of the status string associated to the status code passed, up to 'buffer_length' length, if the string associated to the status code is enabled. If not, the error code number, in hex, prefixed by "SL_STATUS_" will be copied in the buffer instead. For example, the buffer would either contain "SL_STATUS_FAIL" if that status string is enabled, or "SL_STATUS_0x0001" if the string is disabled, as SL_STATUS_FAIL's value is 0x0001.
Returns
The number of characters that would have been written if the buffer_length had been sufficiently large, not counting the terminating null character. If the status code is invalid, 0 or a negative number is returned. Notice that only when this returned value is strictly positive and less than buffer_length, the status string has been completely written in the buffer.
sl_status_print#
void sl_status_print (sl_status_t status)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_status_t | N/A | status | The status code of which to print the status string. |
Print, through printf, the string associated to the passed status code. If the string associated to the status code is enabled, the status string will be printed, for example "SL_STATUS_OK". If the string associated to the status code is disabled, the status number, in hex, prefixed by "SL_STATUS_" will be printed instead, for example "SL_STATUS_0x0000", as SL_STATUS_OK's value is 0x0000.
Macro Definition Documentation#
SL_STATUS_GENERIC_SPACE#
#define SL_STATUS_GENERIC_SPACEValue:
((sl_status_t)0x0000)
sl status generic space.
SL_STATUS_PLATFORM_1_SPACE#
#define SL_STATUS_PLATFORM_1_SPACEValue:
((sl_status_t)0x0100)
sl status platform 1 space.
SL_STATUS_PLATFORM_2_SPACE#
#define SL_STATUS_PLATFORM_2_SPACEValue:
((sl_status_t)0x0200)
sl status platform 2 space.
SL_STATUS_HARDWARE_SPACE#
#define SL_STATUS_HARDWARE_SPACEValue:
((sl_status_t)0x0300)
sl status hardware space.
SL_STATUS_BLUETOOTH_SPACE#
#define SL_STATUS_BLUETOOTH_SPACEValue:
((sl_status_t)0x0400)
sl status bluetooth space.
SL_STATUS_BLUETOOTH_MESH_SPACE#
#define SL_STATUS_BLUETOOTH_MESH_SPACEValue:
((sl_status_t)0x0500)
sl status bluetooth mesh space.
SL_STATUS_CAN_CANOPEN_SPACE#
#define SL_STATUS_CAN_CANOPEN_SPACEValue:
((sl_status_t)0x0600)
sl status can canopen space.
SL_STATUS_CONNECT_SPACE#
#define SL_STATUS_CONNECT_SPACEValue:
((sl_status_t)0x0700)
sl status connect space.
SL_STATUS_NET_SUITE_SPACE#
#define SL_STATUS_NET_SUITE_SPACEValue:
((sl_status_t)0x0800)
sl status net suite space.
SL_STATUS_THREAD_SPACE#
#define SL_STATUS_THREAD_SPACEValue:
((sl_status_t)0x0900)
sl status thread space.
SL_STATUS_ZIGBEE_SPACE#
#define SL_STATUS_ZIGBEE_SPACEValue:
((sl_status_t)0x0C00)
sl status zigbee space.
SL_STATUS_Z_WAVE_SPACE#
#define SL_STATUS_Z_WAVE_SPACEValue:
((sl_status_t)0x0D00)
sl status z wave space.
SL_STATUS_GECKO_OS_1_SPACE#
#define SL_STATUS_GECKO_OS_1_SPACEValue:
((sl_status_t)0x0E00)
sl status gecko os 1 space.
SL_STATUS_GECKO_OS_2_SPACE#
#define SL_STATUS_GECKO_OS_2_SPACEValue:
((sl_status_t)0x0F00)
sl status gecko os 2 space.
SL_STATUS_BLUETOOTH_CTRL_SPACE#
#define SL_STATUS_BLUETOOTH_CTRL_SPACEValue:
((sl_status_t)0x1000)
sl status bluetooth ctrl space.
SL_STATUS_BLUETOOTH_ATT_SPACE#
#define SL_STATUS_BLUETOOTH_ATT_SPACEValue:
((sl_status_t)0x1100)
sl status bluetooth att space.
SL_STATUS_BLUETOOTH_SMP_SPACE#
#define SL_STATUS_BLUETOOTH_SMP_SPACEValue:
((sl_status_t)0x1200)
sl status bluetooth mesh foundation space.
SL_STATUS_BLUETOOTH_MESH_FOUNDATION_SPACE#
#define SL_STATUS_BLUETOOTH_MESH_FOUNDATION_SPACEValue:
((sl_status_t)0x1300)
sl status bluetooth mesh foundation space.
SL_STATUS_WISUN_SPACE#
#define SL_STATUS_WISUN_SPACEValue:
((sl_status_t)0x1400)
sl status wisun space.
SL_STATUS_COMPUTE_SPACE#
#define SL_STATUS_COMPUTE_SPACEValue:
((sl_status_t)0x1500)
sl status compute space.
SL_STATUS_INVALID_STATE#
#define SL_STATUS_INVALID_STATEValue:
((sl_status_t)0x0002)
Generic invalid state error.
SL_STATUS_NOT_READY#
#define SL_STATUS_NOT_READYValue:
((sl_status_t)0x0003)
Module is not ready for requested operation.
SL_STATUS_BUSY#
#define SL_STATUS_BUSYValue:
((sl_status_t)0x0004)
Module is busy and cannot carry out requested operation.
SL_STATUS_IN_PROGRESS#
#define SL_STATUS_IN_PROGRESSValue:
((sl_status_t)0x0005)
Operation is in progress and not yet complete (pass or fail).
SL_STATUS_PERMISSION#
#define SL_STATUS_PERMISSIONValue:
((sl_status_t)0x0008)
Operation not allowed per permissions.
SL_STATUS_WOULD_BLOCK#
#define SL_STATUS_WOULD_BLOCKValue:
((sl_status_t)0x0009)
Non-blocking operation would block.
SL_STATUS_IDLE#
#define SL_STATUS_IDLEValue:
((sl_status_t)0x000A)
Operation/module is Idle, cannot carry requested operation.
SL_STATUS_IS_WAITING#
#define SL_STATUS_IS_WAITINGValue:
((sl_status_t)0x000B)
Operation cannot be done while construct is waiting.
SL_STATUS_NONE_WAITING#
#define SL_STATUS_NONE_WAITINGValue:
((sl_status_t)0x000C)
No task/construct waiting/pending for that action/event.
SL_STATUS_SUSPENDED#
#define SL_STATUS_SUSPENDEDValue:
((sl_status_t)0x000D)
Operation cannot be done while construct is suspended.
SL_STATUS_NOT_AVAILABLE#
#define SL_STATUS_NOT_AVAILABLEValue:
((sl_status_t)0x000E)
Feature not available due to software configuration.
SL_STATUS_NOT_SUPPORTED#
#define SL_STATUS_NOT_SUPPORTEDValue:
((sl_status_t)0x000F)
Feature not supported.
SL_STATUS_INITIALIZATION#
#define SL_STATUS_INITIALIZATIONValue:
((sl_status_t)0x0010)
Initialization failed.
SL_STATUS_NOT_INITIALIZED#
#define SL_STATUS_NOT_INITIALIZEDValue:
((sl_status_t)0x0011)
Module has not been initialized.
SL_STATUS_ALREADY_INITIALIZED#
#define SL_STATUS_ALREADY_INITIALIZEDValue:
((sl_status_t)0x0012)
Module has already been initialized.
SL_STATUS_DELETED#
#define SL_STATUS_DELETEDValue:
((sl_status_t)0x0013)
Object/construct has been deleted.
SL_STATUS_NETWORK_UP#
#define SL_STATUS_NETWORK_UPValue:
((sl_status_t)0x0015)
Illegal call because network is up.
SL_STATUS_NETWORK_DOWN#
#define SL_STATUS_NETWORK_DOWNValue:
((sl_status_t)0x0016)
Illegal call because network is down.
SL_STATUS_NOT_JOINED#
#define SL_STATUS_NOT_JOINEDValue:
((sl_status_t)0x0017)
Failure due to not being joined in a network.
SL_STATUS_NO_BEACONS#
#define SL_STATUS_NO_BEACONSValue:
((sl_status_t)0x0018)
Invalid operation as there are no beacons.
SL_STATUS_ALLOCATION_FAILED#
#define SL_STATUS_ALLOCATION_FAILEDValue:
((sl_status_t)0x0019)
Generic allocation error.
SL_STATUS_NO_MORE_RESOURCE#
#define SL_STATUS_NO_MORE_RESOURCEValue:
((sl_status_t)0x001A)
No more resource available to perform the operation.
SL_STATUS_WOULD_OVERFLOW#
#define SL_STATUS_WOULD_OVERFLOWValue:
((sl_status_t)0x001D)
Item would overflow.
SL_STATUS_HAS_OVERFLOWED#
#define SL_STATUS_HAS_OVERFLOWEDValue:
((sl_status_t)0x001E)
Item/list/queue has been overflowed.
SL_STATUS_IS_OWNER#
#define SL_STATUS_IS_OWNERValue:
((sl_status_t)0x0020)
Already/still owning resource.
SL_STATUS_INVALID_PARAMETER#
#define SL_STATUS_INVALID_PARAMETERValue:
((sl_status_t)0x0021)
Generic invalid argument or consequence of invalid argument.
SL_STATUS_NULL_POINTER#
#define SL_STATUS_NULL_POINTERValue:
((sl_status_t)0x0022)
Invalid null pointer received as argument.
SL_STATUS_INVALID_CONFIGURATION#
#define SL_STATUS_INVALID_CONFIGURATIONValue:
((sl_status_t)0x0023)
Invalid configuration provided.
SL_STATUS_INVALID_TYPE#
#define SL_STATUS_INVALID_TYPEValue:
((sl_status_t)0x0026)
Invalid type for operation.
SL_STATUS_INVALID_CREDENTIALS#
#define SL_STATUS_INVALID_CREDENTIALSValue:
((sl_status_t)0x002A)
Invalid credentials.
SL_STATUS_INVALID_SIGNATURE#
#define SL_STATUS_INVALID_SIGNATUREValue:
((sl_status_t)0x002C)
Invalid signature / verification failed.
SL_STATUS_ALREADY_EXISTS#
#define SL_STATUS_ALREADY_EXISTSValue:
((sl_status_t)0x002E)
Item already exists.
SL_STATUS_IO_TIMEOUT#
#define SL_STATUS_IO_TIMEOUTValue:
((sl_status_t)0x0030)
I/O failure due to timeout.
SL_STATUS_TRANSMIT_UNDERFLOW#
#define SL_STATUS_TRANSMIT_UNDERFLOWValue:
((sl_status_t)0x0032)
Transmit underflowed.
SL_STATUS_TRANSMIT_INCOMPLETE#
#define SL_STATUS_TRANSMIT_INCOMPLETEValue:
((sl_status_t)0x0033)
Transmit is incomplete.
SL_STATUS_OBJECT_READ#
#define SL_STATUS_OBJECT_READValue:
((sl_status_t)0x0036)
Failed to read on/via given object.
SL_STATUS_OBJECT_WRITE#
#define SL_STATUS_OBJECT_WRITEValue:
((sl_status_t)0x0037)
Failed to write on/via given object.
SL_STATUS_MESSAGE_TOO_LONG#
#define SL_STATUS_MESSAGE_TOO_LONGValue:
((sl_status_t)0x0038)
Message is too long.
SL_STATUS_EEPROM_MFG_VERSION_MISMATCH#
#define SL_STATUS_EEPROM_MFG_VERSION_MISMATCHValue:
((sl_status_t)0x0039)
EEPROM MFG version mismatch.
SL_STATUS_EEPROM_STACK_VERSION_MISMATCH#
#define SL_STATUS_EEPROM_STACK_VERSION_MISMATCHValue:
((sl_status_t)0x003A)
EEPROM Stack version mismatch.
SL_STATUS_FLASH_WRITE_INHIBITED#
#define SL_STATUS_FLASH_WRITE_INHIBITEDValue:
((sl_status_t)0x003B)
Flash write is inhibited.
SL_STATUS_FLASH_VERIFY_FAILED#
#define SL_STATUS_FLASH_VERIFY_FAILEDValue:
((sl_status_t)0x003C)
Flash verification failed.
SL_STATUS_FLASH_PROGRAM_FAILED#
#define SL_STATUS_FLASH_PROGRAM_FAILEDValue:
((sl_status_t)0x003D)
Flash programming failed.
SL_STATUS_FLASH_ERASE_FAILED#
#define SL_STATUS_FLASH_ERASE_FAILEDValue:
((sl_status_t)0x003E)
Flash erase failed.
SL_STATUS_MAC_NO_ACK_RECEIVED#
#define SL_STATUS_MAC_NO_ACK_RECEIVEDValue:
((sl_status_t)0x0040)
MAC no ACK received.
SL_STATUS_MAC_INDIRECT_TIMEOUT#
#define SL_STATUS_MAC_INDIRECT_TIMEOUTValue:
((sl_status_t)0x0041)
MAC indirect timeout.
SL_STATUS_MAC_UNKNOWN_HEADER_TYPE#
#define SL_STATUS_MAC_UNKNOWN_HEADER_TYPEValue:
((sl_status_t)0x0042)
MAC unknown header type.
SL_STATUS_MAC_ACK_HEADER_TYPE#
#define SL_STATUS_MAC_ACK_HEADER_TYPEValue:
((sl_status_t)0x0043)
MAC ACK unknown header type.
SL_STATUS_MAC_COMMAND_TRANSMIT_FAILURE#
#define SL_STATUS_MAC_COMMAND_TRANSMIT_FAILUREValue:
((sl_status_t)0x0044)
MAC command transmit failure.
SL_STATUS_CLI_STORAGE_NVM_OPEN_ERROR#
#define SL_STATUS_CLI_STORAGE_NVM_OPEN_ERRORValue:
((sl_status_t)0x0045)
Error in open NVM.
SL_STATUS_SECURITY_IMAGE_CHECKSUM_ERROR#
#define SL_STATUS_SECURITY_IMAGE_CHECKSUM_ERRORValue:
((sl_status_t)0x0046)
Image checksum is not valid.
SL_STATUS_SECURITY_DECRYPT_ERROR#
#define SL_STATUS_SECURITY_DECRYPT_ERRORValue:
((sl_status_t)0x0047)
Decryption failed.
SL_STATUS_COMMAND_IS_INVALID#
#define SL_STATUS_COMMAND_IS_INVALIDValue:
((sl_status_t)0x0048)
Command was not recognized.
SL_STATUS_COMMAND_TOO_LONG#
#define SL_STATUS_COMMAND_TOO_LONGValue:
((sl_status_t)0x0049)
Command or parameter maximum length exceeded.
SL_STATUS_COMMAND_INCOMPLETE#
#define SL_STATUS_COMMAND_INCOMPLETEValue:
((sl_status_t)0x004A)
Data received does not form a complete command.
SL_STATUS_BUS_ERROR#
#define SL_STATUS_BUS_ERRORValue:
((sl_status_t)0x004B)
Bus error, e.g. invalid DMA address.
SL_STATUS_MAC_INCORRECT_SCAN_TYPE#
#define SL_STATUS_MAC_INCORRECT_SCAN_TYPEValue:
((sl_status_t)0x004E)
MAC incorrect scan type.
SL_STATUS_INVALID_CHANNEL_MASK#
#define SL_STATUS_INVALID_CHANNEL_MASKValue:
((sl_status_t)0x004F)
Invalid channel mask.
SL_STATUS_BAD_SCAN_DURATION#
#define SL_STATUS_BAD_SCAN_DURATIONValue:
((sl_status_t)0x0050)
Bad scan duration.
SL_STATUS_BT_OUT_OF_BONDS#
#define SL_STATUS_BT_OUT_OF_BONDSValue:
((sl_status_t)0x0402)
Bonding procedure can't be started because device has no space left for bond.
SL_STATUS_BT_UNSPECIFIED#
#define SL_STATUS_BT_UNSPECIFIEDValue:
((sl_status_t)0x0403)
Unspecified error.
SL_STATUS_BT_NO_BONDING#
#define SL_STATUS_BT_NO_BONDINGValue:
((sl_status_t)0x0406)
The bonding does not exist.
SL_STATUS_BT_CRYPTO#
#define SL_STATUS_BT_CRYPTOValue:
((sl_status_t)0x0407)
Error using crypto functions.
SL_STATUS_BT_DATA_CORRUPTED#
#define SL_STATUS_BT_DATA_CORRUPTEDValue:
((sl_status_t)0x0408)
Data was corrupted.
SL_STATUS_BT_INVALID_SYNC_HANDLE#
#define SL_STATUS_BT_INVALID_SYNC_HANDLEValue:
((sl_status_t)0x040A)
Invalid periodic advertising sync handle.
SL_STATUS_BT_INVALID_MODULE_ACTION#
#define SL_STATUS_BT_INVALID_MODULE_ACTIONValue:
((sl_status_t)0x040B)
Bluetooth cannot be used on this hardware.
SL_STATUS_BT_L2CAP_REMOTE_DISCONNECTED#
#define SL_STATUS_BT_L2CAP_REMOTE_DISCONNECTEDValue:
((sl_status_t)0x040D)
Returned when remote disconnects the connection-oriented channel by sending disconnection request.
SL_STATUS_BT_L2CAP_LOCAL_DISCONNECTED#
#define SL_STATUS_BT_L2CAP_LOCAL_DISCONNECTEDValue:
((sl_status_t)0x040E)
Returned when local host disconnect the connection-oriented channel by sending disconnection request.
SL_STATUS_BT_L2CAP_CID_NOT_EXIST#
#define SL_STATUS_BT_L2CAP_CID_NOT_EXISTValue:
((sl_status_t)0x040F)
Returned when local host did not find a connection-oriented channel with given destination CID.
SL_STATUS_BT_L2CAP_LE_DISCONNECTED#
#define SL_STATUS_BT_L2CAP_LE_DISCONNECTEDValue:
((sl_status_t)0x0410)
Returned when connection-oriented channel disconnected due to LE connection is dropped.
SL_STATUS_BT_L2CAP_FLOW_CONTROL_VIOLATED#
#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_VIOLATEDValue:
((sl_status_t)0x0412)
Returned when connection-oriented channel disconnected due to remote end send data even without credit.
SL_STATUS_BT_L2CAP_FLOW_CONTROL_CREDIT_OVERFLOWED#
#define SL_STATUS_BT_L2CAP_FLOW_CONTROL_CREDIT_OVERFLOWEDValue:
((sl_status_t)0x0413)
Returned when connection-oriented channel disconnected due to remote end send flow control credits exceed 65535.
SL_STATUS_BT_L2CAP_NO_FLOW_CONTROL_CREDIT#
#define SL_STATUS_BT_L2CAP_NO_FLOW_CONTROL_CREDITValue:
((sl_status_t)0x0414)
Returned when connection-oriented channel has run out of flow control credit and local application still trying to send data.
SL_STATUS_BT_L2CAP_CONNECTION_REQUEST_TIMEOUT#
#define SL_STATUS_BT_L2CAP_CONNECTION_REQUEST_TIMEOUTValue:
((sl_status_t)0x0415)
Returned when connection-oriented channel has not received connection response message within maximum timeout.
SL_STATUS_BT_L2CAP_INVALID_CID#
#define SL_STATUS_BT_L2CAP_INVALID_CIDValue:
((sl_status_t)0x0416)
Returned when local host received a connection-oriented channel connection response with an invalid destination CID.
SL_STATUS_BT_L2CAP_WRONG_STATE#
#define SL_STATUS_BT_L2CAP_WRONG_STATEValue:
((sl_status_t)0x0417)
Returned when local host application tries to send a command which is not suitable for L2CAP channel's current state.
SL_STATUS_BT_PS_STORE_FULL#
#define SL_STATUS_BT_PS_STORE_FULLValue:
((sl_status_t)0x041B)
Flash reserved for PS store is full.
SL_STATUS_BT_PS_KEY_NOT_FOUND#
#define SL_STATUS_BT_PS_KEY_NOT_FOUNDValue:
((sl_status_t)0x041C)
PS key not found.
SL_STATUS_BT_APPLICATION_MISMATCHED_OR_INSUFFICIENT_SECURITY#
#define SL_STATUS_BT_APPLICATION_MISMATCHED_OR_INSUFFICIENT_SECURITYValue:
((sl_status_t)0x041D)
Mismatched or insufficient security level.
SL_STATUS_BT_APPLICATION_ENCRYPTION_DECRYPTION_ERROR#
#define SL_STATUS_BT_APPLICATION_ENCRYPTION_DECRYPTION_ERRORValue:
((sl_status_t)0x041E)
Encryption/decryption operation failed.
SL_STATUS_BT_CTRL_UNKNOWN_CONNECTION_IDENTIFIER#
#define SL_STATUS_BT_CTRL_UNKNOWN_CONNECTION_IDENTIFIERValue:
((sl_status_t)0x1002)
Connection does not exist, or connection open request was cancelled.
SL_STATUS_BT_CTRL_AUTHENTICATION_FAILURE#
#define SL_STATUS_BT_CTRL_AUTHENTICATION_FAILUREValue:
((sl_status_t)0x1005)
Pairing or authentication failed due to incorrect results in the pairing or authentication procedure. This could be due to an incorrect PIN or Link Key.
SL_STATUS_BT_CTRL_PIN_OR_KEY_MISSING#
#define SL_STATUS_BT_CTRL_PIN_OR_KEY_MISSINGValue:
((sl_status_t)0x1006)
Pairing failed because of missing PIN, or authentication failed because of missing Key.
SL_STATUS_BT_CTRL_MEMORY_CAPACITY_EXCEEDED#
#define SL_STATUS_BT_CTRL_MEMORY_CAPACITY_EXCEEDEDValue:
((sl_status_t)0x1007)
Controller is out of memory.
SL_STATUS_BT_CTRL_CONNECTION_TIMEOUT#
#define SL_STATUS_BT_CTRL_CONNECTION_TIMEOUTValue:
((sl_status_t)0x1008)
Link supervision timeout has expired.
SL_STATUS_BT_CTRL_CONNECTION_LIMIT_EXCEEDED#
#define SL_STATUS_BT_CTRL_CONNECTION_LIMIT_EXCEEDEDValue:
((sl_status_t)0x1009)
Controller is at limit of connections it can support.
SL_STATUS_BT_CTRL_SYNCHRONOUS_CONNECTION_LIMIT_EXCEEDED#
#define SL_STATUS_BT_CTRL_SYNCHRONOUS_CONNECTION_LIMIT_EXCEEDEDValue:
((sl_status_t)0x100A)
The Synchronous Connection Limit to a Device Exceeded error code indicates that the Controller has reached the limit to the number of synchronous connections that can be achieved to a device.
SL_STATUS_BT_CTRL_ACL_CONNECTION_ALREADY_EXISTS#
#define SL_STATUS_BT_CTRL_ACL_CONNECTION_ALREADY_EXISTSValue:
((sl_status_t)0x100B)
The ACL Connection Already Exists error code indicates that an attempt to create a new ACL Connection to a device when there is already a connection to this device.
SL_STATUS_BT_CTRL_COMMAND_DISALLOWED#
#define SL_STATUS_BT_CTRL_COMMAND_DISALLOWEDValue:
((sl_status_t)0x100C)
Command requested cannot be executed because the Controller is in a state where it cannot process this command at this time.
SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_LIMITED_RESOURCES#
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_LIMITED_RESOURCESValue:
((sl_status_t)0x100D)
The Connection Rejected Due To Limited Resources error code indicates that an incoming connection was rejected due to limited resources.
SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_SECURITY_REASONS#
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_SECURITY_REASONSValue:
((sl_status_t)0x100E)
The Connection Rejected Due To Security Reasons error code indicates that a connection was rejected due to security requirements not being fulfilled, like authentication or pairing.
SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_UNACCEPTABLE_BD_ADDR#
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_UNACCEPTABLE_BD_ADDRValue:
((sl_status_t)0x100F)
The Connection was rejected because this device does not accept the BD_ADDR. This may be because the device will only accept connections from specific BD_ADDRs.
SL_STATUS_BT_CTRL_CONNECTION_ACCEPT_TIMEOUT_EXCEEDED#
#define SL_STATUS_BT_CTRL_CONNECTION_ACCEPT_TIMEOUT_EXCEEDEDValue:
((sl_status_t)0x1010)
The Connection Accept Timeout has been exceeded for this connection attempt.
SL_STATUS_BT_CTRL_UNSUPPORTED_FEATURE_OR_PARAMETER_VALUE#
#define SL_STATUS_BT_CTRL_UNSUPPORTED_FEATURE_OR_PARAMETER_VALUEValue:
((sl_status_t)0x1011)
A feature or parameter value in the HCI command is not supported.
SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERS#
#define SL_STATUS_BT_CTRL_INVALID_COMMAND_PARAMETERSValue:
((sl_status_t)0x1012)
Command contained invalid parameters.
SL_STATUS_BT_CTRL_REMOTE_USER_TERMINATED#
#define SL_STATUS_BT_CTRL_REMOTE_USER_TERMINATEDValue:
((sl_status_t)0x1013)
User on the remote device terminated the connection.
SL_STATUS_BT_CTRL_REMOTE_DEVICE_TERMINATED_CONNECTION_DUE_TO_LOW_RESOURCES#
#define SL_STATUS_BT_CTRL_REMOTE_DEVICE_TERMINATED_CONNECTION_DUE_TO_LOW_RESOURCESValue:
((sl_status_t)0x1014)
The remote device terminated the connection because of low resources.
SL_STATUS_BT_CTRL_REMOTE_POWERING_OFF#
#define SL_STATUS_BT_CTRL_REMOTE_POWERING_OFFValue:
((sl_status_t)0x1015)
Remote Device Terminated Connection due to Power Off.
SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_BY_LOCAL_HOST#
#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_BY_LOCAL_HOSTValue:
((sl_status_t)0x1016)
Local device terminated the connection.
SL_STATUS_BT_CTRL_REPEATED_ATTEMPTS#
#define SL_STATUS_BT_CTRL_REPEATED_ATTEMPTSValue:
((sl_status_t)0x1017)
The Controller is disallowing an authentication or pairing procedure because too little time has elapsed since the last authentication or pairing attempt failed.
SL_STATUS_BT_CTRL_PAIRING_NOT_ALLOWED#
#define SL_STATUS_BT_CTRL_PAIRING_NOT_ALLOWEDValue:
((sl_status_t)0x1018)
The device does not allow pairing. This can be for example, when a device only allows pairing during a certain time window after some user input allows pairing.
SL_STATUS_BT_CTRL_UNSUPPORTED_REMOTE_FEATURE#
#define SL_STATUS_BT_CTRL_UNSUPPORTED_REMOTE_FEATUREValue:
((sl_status_t)0x101A)
The remote device does not support the feature associated with the issued command.
SL_STATUS_BT_CTRL_UNSPECIFIED_ERROR#
#define SL_STATUS_BT_CTRL_UNSPECIFIED_ERRORValue:
((sl_status_t)0x101F)
No other error code specified is appropriate to use.
SL_STATUS_BT_CTRL_LL_RESPONSE_TIMEOUT#
#define SL_STATUS_BT_CTRL_LL_RESPONSE_TIMEOUTValue:
((sl_status_t)0x1022)
Connection terminated due to link-layer procedure timeout.
SL_STATUS_BT_CTRL_LL_PROCEDURE_COLLISION#
#define SL_STATUS_BT_CTRL_LL_PROCEDURE_COLLISIONValue:
((sl_status_t)0x1023)
LL procedure has collided with the same transaction or procedure that is already in progress.
SL_STATUS_BT_CTRL_ENCRYPTION_MODE_NOT_ACCEPTABLE#
#define SL_STATUS_BT_CTRL_ENCRYPTION_MODE_NOT_ACCEPTABLEValue:
((sl_status_t)0x1025)
The requested encryption mode is not acceptable at this time.
SL_STATUS_BT_CTRL_LINK_KEY_CANNOT_BE_CHANGED#
#define SL_STATUS_BT_CTRL_LINK_KEY_CANNOT_BE_CHANGEDValue:
((sl_status_t)0x1026)
Link key cannot be changed because a fixed unit key is being used.
SL_STATUS_BT_CTRL_INSTANT_PASSED#
#define SL_STATUS_BT_CTRL_INSTANT_PASSEDValue:
((sl_status_t)0x1028)
LMP PDU or LL PDU that includes an instant cannot be performed because the instant when this would have occurred has passed.
SL_STATUS_BT_CTRL_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED#
#define SL_STATUS_BT_CTRL_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTEDValue:
((sl_status_t)0x1029)
It was not possible to pair as a unit key was requested and it is not supported.
SL_STATUS_BT_CTRL_DIFFERENT_TRANSACTION_COLLISION#
#define SL_STATUS_BT_CTRL_DIFFERENT_TRANSACTION_COLLISIONValue:
((sl_status_t)0x102A)
LMP transaction was started that collides with an ongoing transaction.
SL_STATUS_BT_CTRL_CHANNEL_ASSESSMENT_NOT_SUPPORTED#
#define SL_STATUS_BT_CTRL_CHANNEL_ASSESSMENT_NOT_SUPPORTEDValue:
((sl_status_t)0x102E)
The Controller cannot perform channel assessment because it is not supported.
SL_STATUS_BT_CTRL_INSUFFICIENT_SECURITY#
#define SL_STATUS_BT_CTRL_INSUFFICIENT_SECURITYValue:
((sl_status_t)0x102F)
The HCI command or LMP PDU sent is only possible on an encrypted link.
SL_STATUS_BT_CTRL_PARAMETER_OUT_OF_MANDATORY_RANGE#
#define SL_STATUS_BT_CTRL_PARAMETER_OUT_OF_MANDATORY_RANGEValue:
((sl_status_t)0x1030)
A parameter value requested is outside the mandatory range of parameters for the given HCI command or LMP PDU.
SL_STATUS_BT_CTRL_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST#
#define SL_STATUS_BT_CTRL_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOSTValue:
((sl_status_t)0x1037)
The IO capabilities request or response was rejected because the sending Host does not support Secure Simple Pairing even though the receiving Link Manager does.
SL_STATUS_BT_CTRL_HOST_BUSY_PAIRING#
#define SL_STATUS_BT_CTRL_HOST_BUSY_PAIRINGValue:
((sl_status_t)0x1038)
The Host is busy with another pairing operation and unable to support the requested pairing. The receiving device should retry pairing again later.
SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_NO_SUITABLE_CHANNEL_FOUND#
#define SL_STATUS_BT_CTRL_CONNECTION_REJECTED_DUE_TO_NO_SUITABLE_CHANNEL_FOUNDValue:
((sl_status_t)0x1039)
The Controller could not calculate an appropriate value for the Channel selection operation.
SL_STATUS_BT_CTRL_CONTROLLER_BUSY#
#define SL_STATUS_BT_CTRL_CONTROLLER_BUSYValue:
((sl_status_t)0x103A)
Operation was rejected because the controller is busy and unable to process the request.
SL_STATUS_BT_CTRL_UNACCEPTABLE_CONNECTION_INTERVAL#
#define SL_STATUS_BT_CTRL_UNACCEPTABLE_CONNECTION_INTERVALValue:
((sl_status_t)0x103B)
Remote device terminated the connection because of an unacceptable connection interval.
SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUT#
#define SL_STATUS_BT_CTRL_ADVERTISING_TIMEOUTValue:
((sl_status_t)0x103C)
Advertising for a fixed duration completed or, for directed advertising, that advertising completed without a connection being created.
SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_DUE_TO_MIC_FAILURE#
#define SL_STATUS_BT_CTRL_CONNECTION_TERMINATED_DUE_TO_MIC_FAILUREValue:
((sl_status_t)0x103D)
Connection was terminated because the Message Integrity Check (MIC) failed on a received packet.
SL_STATUS_BT_CTRL_CONNECTION_FAILED_TO_BE_ESTABLISHED#
#define SL_STATUS_BT_CTRL_CONNECTION_FAILED_TO_BE_ESTABLISHEDValue:
((sl_status_t)0x103E)
LL initiated a connection but the connection has failed to be established. Controller did not receive any packets from remote end.
SL_STATUS_BT_CTRL_MAC_CONNECTION_FAILED#
#define SL_STATUS_BT_CTRL_MAC_CONNECTION_FAILEDValue:
((sl_status_t)0x103F)
The MAC of the 802.11 AMP was requested to connect to a peer, but the connection failed.
SL_STATUS_BT_CTRL_COARSE_CLOCK_ADJUSTMENT_REJECTED_BUT_WILL_TRY_TO_ADJUST_USING_CLOCK_DRAGGING#
#define SL_STATUS_BT_CTRL_COARSE_CLOCK_ADJUSTMENT_REJECTED_BUT_WILL_TRY_TO_ADJUST_USING_CLOCK_DRAGGINGValue:
((sl_status_t)0x1040)
The master, at this time, is unable to make a coarse adjustment to the piconet clock, using the supplied parameters. Instead the master will attempt to move the clock using clock dragging.
SL_STATUS_BT_CTRL_UNKNOWN_ADVERTISING_IDENTIFIER#
#define SL_STATUS_BT_CTRL_UNKNOWN_ADVERTISING_IDENTIFIERValue:
((sl_status_t)0x1042)
A command was sent from the Host that should identify an Advertising or Sync handle, but the Advertising or Sync handle does not exist.
SL_STATUS_BT_CTRL_LIMIT_REACHED#
#define SL_STATUS_BT_CTRL_LIMIT_REACHEDValue:
((sl_status_t)0x1043)
Number of operations requested has been reached and has indicated the completion of the activity (e.g., advertising or scanning).
SL_STATUS_BT_CTRL_OPERATION_CANCELLED_BY_HOST#
#define SL_STATUS_BT_CTRL_OPERATION_CANCELLED_BY_HOSTValue:
((sl_status_t)0x1044)
A request to the Controller issued by the Host and still pending was successfully canceled.
SL_STATUS_BT_CTRL_PACKET_TOO_LONG#
#define SL_STATUS_BT_CTRL_PACKET_TOO_LONGValue:
((sl_status_t)0x1045)
An attempt was made to send or receive a packet that exceeds the maximum allowed packet l.
SL_STATUS_BT_ATT_INVALID_HANDLE#
#define SL_STATUS_BT_ATT_INVALID_HANDLEValue:
((sl_status_t)0x1101)
The attribute handle given was not valid on this server.
SL_STATUS_BT_ATT_READ_NOT_PERMITTED#
#define SL_STATUS_BT_ATT_READ_NOT_PERMITTEDValue:
((sl_status_t)0x1102)
The attribute cannot be read.
SL_STATUS_BT_ATT_WRITE_NOT_PERMITTED#
#define SL_STATUS_BT_ATT_WRITE_NOT_PERMITTEDValue:
((sl_status_t)0x1103)
The attribute cannot be written.
SL_STATUS_BT_ATT_INVALID_PDU#
#define SL_STATUS_BT_ATT_INVALID_PDUValue:
((sl_status_t)0x1104)
The attribute PDU was invalid.
SL_STATUS_BT_ATT_INSUFFICIENT_AUTHENTICATION#
#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHENTICATIONValue:
((sl_status_t)0x1105)
The attribute requires authentication before it can be read or written.
SL_STATUS_BT_ATT_REQUEST_NOT_SUPPORTED#
#define SL_STATUS_BT_ATT_REQUEST_NOT_SUPPORTEDValue:
((sl_status_t)0x1106)
Attribute Server does not support the request received from the client.
SL_STATUS_BT_ATT_INVALID_OFFSET#
#define SL_STATUS_BT_ATT_INVALID_OFFSETValue:
((sl_status_t)0x1107)
Offset specified was past the end of the attribute.
SL_STATUS_BT_ATT_INSUFFICIENT_AUTHORIZATION
#define SL_STATUS_BT_ATT_INSUFFICIENT_AUTHORIZATIONValue:
((sl_status_t)0x1108)
The attribute requires authorization before it can be read or written.
SL_STATUS_BT_ATT_PREPARE_QUEUE_FULL#
#define SL_STATUS_BT_ATT_PREPARE_QUEUE_FULLValue:
((sl_status_t)0x1109)
Too many prepare writes have been queued.
SL_STATUS_BT_ATT_ATT_NOT_FOUND#
#define SL_STATUS_BT_ATT_ATT_NOT_FOUNDValue:
((sl_status_t)0x110A)
No attribute found within the given attribute handle range.
SL_STATUS_BT_ATT_ATT_NOT_LONG#
#define SL_STATUS_BT_ATT_ATT_NOT_LONGValue:
((sl_status_t)0x110B)
The attribute cannot be read or written using the Read Blob Request.
SL_STATUS_BT_ATT_INSUFFICIENT_ENC_KEY_SIZE#
#define SL_STATUS_BT_ATT_INSUFFICIENT_ENC_KEY_SIZEValue:
((sl_status_t)0x110C)
The Encryption Key Size used for encrypting this link is insufficient.
SL_STATUS_BT_ATT_INVALID_ATT_LENGTH#
#define SL_STATUS_BT_ATT_INVALID_ATT_LENGTHValue:
((sl_status_t)0x110D)
The attribute value length is invalid for the operation.
SL_STATUS_BT_ATT_UNLIKELY_ERROR#
#define SL_STATUS_BT_ATT_UNLIKELY_ERRORValue:
((sl_status_t)0x110E)
The attribute request that was requested has encountered an error that was unlikely, and therefore could not be completed as requested.
SL_STATUS_BT_ATT_INSUFFICIENT_ENCRYPTION#
#define SL_STATUS_BT_ATT_INSUFFICIENT_ENCRYPTIONValue:
((sl_status_t)0x110F)
The attribute requires encryption before it can be read or written.
SL_STATUS_BT_ATT_UNSUPPORTED_GROUP_TYPE#
#define SL_STATUS_BT_ATT_UNSUPPORTED_GROUP_TYPEValue:
((sl_status_t)0x1110)
The attribute type is not a supported grouping attribute as defined by a higher layer specification.
SL_STATUS_BT_ATT_INSUFFICIENT_RESOURCES#
#define SL_STATUS_BT_ATT_INSUFFICIENT_RESOURCESValue:
((sl_status_t)0x1111)
Insufficient Resources to complete the request.
SL_STATUS_BT_ATT_OUT_OF_SYNC#
#define SL_STATUS_BT_ATT_OUT_OF_SYNCValue:
((sl_status_t)0x1112)
The server requests the client to rediscover the database.
SL_STATUS_BT_ATT_VALUE_NOT_ALLOWED#
#define SL_STATUS_BT_ATT_VALUE_NOT_ALLOWEDValue:
((sl_status_t)0x1113)
The attribute parameter value was not allowed.
SL_STATUS_BT_ATT_APPLICATION#
#define SL_STATUS_BT_ATT_APPLICATIONValue:
((sl_status_t)0x1180)
When this is returned in a BGAPI response, the application tried to read or write the value of a user attribute from the GATT database.
SL_STATUS_BT_ATT_WRITE_REQUEST_REJECTED#
#define SL_STATUS_BT_ATT_WRITE_REQUEST_REJECTEDValue:
((sl_status_t)0x11FC)
The requested write operation cannot be fulfilled for reasons other than permissions.
SL_STATUS_BT_ATT_CLIENT_CHARACTERISTIC_CONFIGURATION_DESCRIPTOR_IMPROPERLY_CONFIGURED#
#define SL_STATUS_BT_ATT_CLIENT_CHARACTERISTIC_CONFIGURATION_DESCRIPTOR_IMPROPERLY_CONFIGUREDValue:
((sl_status_t)0x11FD)
The Client Characteristic Configuration descriptor is not configured according to the requirements of the profile or service.
SL_STATUS_BT_ATT_PROCEDURE_ALREADY_IN_PROGRESS#
#define SL_STATUS_BT_ATT_PROCEDURE_ALREADY_IN_PROGRESSValue:
((sl_status_t)0x11FE)
The profile or service request cannot be serviced because an operation that has been previously triggered is still in progress.
SL_STATUS_BT_ATT_OUT_OF_RANGE#
#define SL_STATUS_BT_ATT_OUT_OF_RANGEValue:
((sl_status_t)0x11FF)
The attribute value is out of range as defined by a profile or service specification.
SL_STATUS_BT_SMP_PASSKEY_ENTRY_FAILED#
#define SL_STATUS_BT_SMP_PASSKEY_ENTRY_FAILEDValue:
((sl_status_t)0x1201)
The user input of passkey failed, for example, the user cancelled the operation.
SL_STATUS_BT_SMP_OOB_NOT_AVAILABLE#
#define SL_STATUS_BT_SMP_OOB_NOT_AVAILABLEValue:
((sl_status_t)0x1202)
Out of Band data is not available for authentication.
SL_STATUS_BT_SMP_AUTHENTICATION_REQUIREMENTS#
#define SL_STATUS_BT_SMP_AUTHENTICATION_REQUIREMENTSValue:
((sl_status_t)0x1203)
The pairing procedure cannot be performed as authentication requirements cannot be met due to IO capabilities of one or both devices.
SL_STATUS_BT_SMP_CONFIRM_VALUE_FAILED#
#define SL_STATUS_BT_SMP_CONFIRM_VALUE_FAILEDValue:
((sl_status_t)0x1204)
The confirm value does not match the calculated compare value.
SL_STATUS_BT_SMP_PAIRING_NOT_SUPPORTED#
#define SL_STATUS_BT_SMP_PAIRING_NOT_SUPPORTEDValue:
((sl_status_t)0x1205)
Pairing is not supported by the device.
SL_STATUS_BT_SMP_ENCRYPTION_KEY_SIZE#
#define SL_STATUS_BT_SMP_ENCRYPTION_KEY_SIZEValue:
((sl_status_t)0x1206)
The resultant encryption key size is insufficient for the security requirements of this device.
SL_STATUS_BT_SMP_COMMAND_NOT_SUPPORTED#
#define SL_STATUS_BT_SMP_COMMAND_NOT_SUPPORTEDValue:
((sl_status_t)0x1207)
The SMP command received is not supported on this device.
SL_STATUS_BT_SMP_UNSPECIFIED_REASON#
#define SL_STATUS_BT_SMP_UNSPECIFIED_REASONValue:
((sl_status_t)0x1208)
Pairing failed due to an unspecified reason.
SL_STATUS_BT_SMP_REPEATED_ATTEMPTS#
#define SL_STATUS_BT_SMP_REPEATED_ATTEMPTSValue:
((sl_status_t)0x1209)
Pairing or authentication procedure is disallowed because too little time has elapsed since last pairing request or security request.
SL_STATUS_BT_SMP_INVALID_PARAMETERS#
#define SL_STATUS_BT_SMP_INVALID_PARAMETERSValue:
((sl_status_t)0x120A)
The Invalid Parameters error code indicates: the command length is invalid or a parameter is outside of the specified range.
SL_STATUS_BT_SMP_DHKEY_CHECK_FAILED#
#define SL_STATUS_BT_SMP_DHKEY_CHECK_FAILEDValue:
((sl_status_t)0x120B)
Indicates to the remote device that the DHKey Check value received doesn't match the one calculated by the local device.
SL_STATUS_BT_SMP_NUMERIC_COMPARISON_FAILED#
#define SL_STATUS_BT_SMP_NUMERIC_COMPARISON_FAILEDValue:
((sl_status_t)0x120C)
Indicates that the confirm values in the numeric comparison protocol do not match.
SL_STATUS_BT_SMP_BREDR_PAIRING_IN_PROGRESS#
#define SL_STATUS_BT_SMP_BREDR_PAIRING_IN_PROGRESSValue:
((sl_status_t)0x120D)
Indicates that the pairing over the LE transport failed due to a Pairing Request sent over the BR/EDR transport in process.
SL_STATUS_BT_SMP_CROSS_TRANSPORT_KEY_DERIVATION_GENERATION_NOT_ALLOWED#
#define SL_STATUS_BT_SMP_CROSS_TRANSPORT_KEY_DERIVATION_GENERATION_NOT_ALLOWEDValue:
((sl_status_t)0x120E)
Indicates that the BR/EDR Link Key generated on the BR/EDR transport cannot be used to derive and distribute keys for the LE transport.
SL_STATUS_BT_SMP_KEY_REJECTED#
#define SL_STATUS_BT_SMP_KEY_REJECTEDValue:
((sl_status_t)0x120F)
Indicates that the device chose not to accept a distributed key.
SL_STATUS_BT_MESH_ALREADY_EXISTS#
#define SL_STATUS_BT_MESH_ALREADY_EXISTSValue:
((sl_status_t)0x0501)
Returned when trying to add a key or some other unique resource with an ID which already exists.
SL_STATUS_BT_MESH_DOES_NOT_EXIST#
#define SL_STATUS_BT_MESH_DOES_NOT_EXISTValue:
((sl_status_t)0x0502)
Returned when trying to manipulate a key or some other resource with an ID which does not exist.
SL_STATUS_BT_MESH_LIMIT_REACHED#
#define SL_STATUS_BT_MESH_LIMIT_REACHEDValue:
((sl_status_t)0x0503)
Returned when an operation cannot be executed because a pre-configured limit for keys, key bindings, elements, models, virtual addresses, provisioned devices, or provisioning sessions is reached.
SL_STATUS_BT_MESH_INVALID_ADDRESS#
#define SL_STATUS_BT_MESH_INVALID_ADDRESSValue:
((sl_status_t)0x0504)
Returned when trying to use a reserved address or add a "pre-provisioned" device using an address already used by some other device.
SL_STATUS_BT_MESH_MALFORMED_DATA#
#define SL_STATUS_BT_MESH_MALFORMED_DATAValue:
((sl_status_t)0x0505)
In a BGAPI response, the user supplied malformed data; in a BGAPI event, the remote end responded with malformed or unrecognized data.
SL_STATUS_BT_MESH_ALREADY_INITIALIZED#
#define SL_STATUS_BT_MESH_ALREADY_INITIALIZEDValue:
((sl_status_t)0x0506)
An attempt was made to initialize a subsystem that was already initialized.
SL_STATUS_BT_MESH_NOT_INITIALIZED#
#define SL_STATUS_BT_MESH_NOT_INITIALIZEDValue:
((sl_status_t)0x0507)
An attempt was made to use a subsystem that wasn't initialized yet. Call the subsystem's init function first.
SL_STATUS_BT_MESH_NO_FRIEND_OFFER#
#define SL_STATUS_BT_MESH_NO_FRIEND_OFFERValue:
((sl_status_t)0x0508)
Returned when trying to establish a friendship as a Low Power Node, but no acceptable friend offer message was received.
SL_STATUS_BT_MESH_PROV_LINK_CLOSED#
#define SL_STATUS_BT_MESH_PROV_LINK_CLOSEDValue:
((sl_status_t)0x0509)
Provisioning link was unexpectedly closed before provisioning was complete.
SL_STATUS_BT_MESH_PROV_INVALID_PDU#
#define SL_STATUS_BT_MESH_PROV_INVALID_PDUValue:
((sl_status_t)0x050A)
An unrecognized provisioning PDU was received.
SL_STATUS_BT_MESH_PROV_INVALID_PDU_FORMAT#
#define SL_STATUS_BT_MESH_PROV_INVALID_PDU_FORMATValue:
((sl_status_t)0x050B)
A provisioning PDU with wrong length or containing field values that are out of bounds was received.
SL_STATUS_BT_MESH_PROV_UNEXPECTED_PDU#
#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_PDUValue:
((sl_status_t)0x050C)
An unexpected (out of sequence) provisioning PDU was received.
SL_STATUS_BT_MESH_PROV_CONFIRMATION_FAILED#
#define SL_STATUS_BT_MESH_PROV_CONFIRMATION_FAILEDValue:
((sl_status_t)0x050D)
The computed confirmation value did not match the expected value.
SL_STATUS_BT_MESH_PROV_OUT_OF_RESOURCES#
#define SL_STATUS_BT_MESH_PROV_OUT_OF_RESOURCESValue:
((sl_status_t)0x050E)
Provisioning could not be continued due to insufficient resources.
SL_STATUS_BT_MESH_PROV_DECRYPTION_FAILED#
#define SL_STATUS_BT_MESH_PROV_DECRYPTION_FAILEDValue:
((sl_status_t)0x050F)
The provisioning data block could not be decrypted.
SL_STATUS_BT_MESH_PROV_UNEXPECTED_ERROR#
#define SL_STATUS_BT_MESH_PROV_UNEXPECTED_ERRORValue:
((sl_status_t)0x0510)
An unexpected error happened during provisioning.
SL_STATUS_BT_MESH_PROV_CANNOT_ASSIGN_ADDR#
#define SL_STATUS_BT_MESH_PROV_CANNOT_ASSIGN_ADDRValue:
((sl_status_t)0x0511)
Device could not assign unicast addresses to all of its elements.
SL_STATUS_BT_MESH_ADDRESS_TEMPORARILY_UNAVAILABLE
#define SL_STATUS_BT_MESH_ADDRESS_TEMPORARILY_UNAVAILABLEValue:
((sl_status_t)0x0512)
Returned when trying to reuse an address of a previously deleted device before an IV Index Update has been executed.
SL_STATUS_BT_MESH_ADDRESS_ALREADY_USED#
#define SL_STATUS_BT_MESH_ADDRESS_ALREADY_USEDValue:
((sl_status_t)0x0513)
Returned when trying to assign an address that is used by one of the devices in the Device Database, or by the Provisioner itself.
SL_STATUS_BT_MESH_PUBLISH_NOT_CONFIGURED#
#define SL_STATUS_BT_MESH_PUBLISH_NOT_CONFIGUREDValue:
((sl_status_t)0x0514)
Application key or publish address are not set.
SL_STATUS_BT_MESH_APP_KEY_NOT_BOUND#
#define SL_STATUS_BT_MESH_APP_KEY_NOT_BOUNDValue:
((sl_status_t)0x0515)
Application key is not bound to a model.
SL_STATUS_BT_MESH_FOUNDATION_INVALID_ADDRESS#
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_ADDRESSValue:
((sl_status_t)0x1301)
Returned when address in request was not valid.
SL_STATUS_BT_MESH_FOUNDATION_INVALID_MODEL#
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_MODELValue:
((sl_status_t)0x1302)
Returned when model identified is not found for a given element.
SL_STATUS_BT_MESH_FOUNDATION_INVALID_APP_KEY#
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_APP_KEYValue:
((sl_status_t)0x1303)
Returned when the key identified by AppKeyIndex is not stored in the node.
SL_STATUS_BT_MESH_FOUNDATION_INVALID_NET_KEY#
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_NET_KEYValue:
((sl_status_t)0x1304)
Returned when the key identified by NetKeyIndex is not stored in the node.
SL_STATUS_BT_MESH_FOUNDATION_INSUFFICIENT_RESOURCES#
#define SL_STATUS_BT_MESH_FOUNDATION_INSUFFICIENT_RESOURCESValue:
((sl_status_t)0x1305)
Returned when The node cannot serve the request due to insufficient resources.
SL_STATUS_BT_MESH_FOUNDATION_KEY_INDEX_EXISTS#
#define SL_STATUS_BT_MESH_FOUNDATION_KEY_INDEX_EXISTSValue:
((sl_status_t)0x1306)
Returned when the key identified is already stored in the node and the new NetKey value is different.
SL_STATUS_BT_MESH_FOUNDATION_INVALID_PUBLISH_PARAMS#
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_PUBLISH_PARAMSValue:
((sl_status_t)0x1307)
Returned when the model does not support the publish mechanism.
SL_STATUS_BT_MESH_FOUNDATION_NOT_SUBSCRIBE_MODEL#
#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUBSCRIBE_MODELValue:
((sl_status_t)0x1308)
Returned when the model does not support the subscribe mechanism.
SL_STATUS_BT_MESH_FOUNDATION_STORAGE_FAILURE#
#define SL_STATUS_BT_MESH_FOUNDATION_STORAGE_FAILUREValue:
((sl_status_t)0x1309)
Returned when storing of the requested parameters failed.
SL_STATUS_BT_MESH_FOUNDATION_NOT_SUPPORTED#
#define SL_STATUS_BT_MESH_FOUNDATION_NOT_SUPPORTEDValue:
((sl_status_t)0x130A)
Returned when requested setting is not supported.
SL_STATUS_BT_MESH_FOUNDATION_CANNOT_UPDATE#
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_UPDATEValue:
((sl_status_t)0x130B)
Returned when the requested update operation cannot be performed due to general constraints.
SL_STATUS_BT_MESH_FOUNDATION_CANNOT_REMOVE#
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_REMOVEValue:
((sl_status_t)0x130C)
Returned when the requested delete operation cannot be performed due to general constraints.
SL_STATUS_BT_MESH_FOUNDATION_CANNOT_BIND#
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_BINDValue:
((sl_status_t)0x130D)
Returned when the requested bind operation cannot be performed due to general constraints.
SL_STATUS_BT_MESH_FOUNDATION_TEMPORARILY_UNABLE#
#define SL_STATUS_BT_MESH_FOUNDATION_TEMPORARILY_UNABLEValue:
((sl_status_t)0x130E)
Returned when The node cannot start advertising with Node Identity or Proxy since the maximum number of parallel advertising is reached.
SL_STATUS_BT_MESH_FOUNDATION_CANNOT_SET#
#define SL_STATUS_BT_MESH_FOUNDATION_CANNOT_SETValue:
((sl_status_t)0x130F)
Returned when the requested state cannot be set.
SL_STATUS_BT_MESH_FOUNDATION_UNSPECIFIED#
#define SL_STATUS_BT_MESH_FOUNDATION_UNSPECIFIEDValue:
((sl_status_t)0x1310)
Returned when an unspecified error took place.
SL_STATUS_BT_MESH_FOUNDATION_INVALID_BINDING#
#define SL_STATUS_BT_MESH_FOUNDATION_INVALID_BINDINGValue:
((sl_status_t)0x1311)
Returned when the NetKeyIndex and AppKeyIndex combination is not valid for a Config AppKey Update.
SL_STATUS_WIFI_INVALID_KEY#
#define SL_STATUS_WIFI_INVALID_KEYValue:
((sl_status_t)0x0B01)
Invalid firmware keyset.
SL_STATUS_WIFI_FIRMWARE_DOWNLOAD_TIMEOUT#
#define SL_STATUS_WIFI_FIRMWARE_DOWNLOAD_TIMEOUTValue:
((sl_status_t)0x0B02)
The firmware download took too long.
SL_STATUS_WIFI_UNSUPPORTED_MESSAGE_ID#
#define SL_STATUS_WIFI_UNSUPPORTED_MESSAGE_IDValue:
((sl_status_t)0x0B03)
Unknown request ID or wrong interface ID used.
SL_STATUS_WIFI_WARNING#
#define SL_STATUS_WIFI_WARNINGValue:
((sl_status_t)0x0B04)
The request is successful but some parameters have been ignored.
SL_STATUS_WIFI_NO_PACKET_TO_RECEIVE#
#define SL_STATUS_WIFI_NO_PACKET_TO_RECEIVEValue:
((sl_status_t)0x0B05)
No Packets waiting to be received.
SL_STATUS_WIFI_SLEEP_GRANTED#
#define SL_STATUS_WIFI_SLEEP_GRANTEDValue:
((sl_status_t)0x0B08)
The sleep mode is granted.
SL_STATUS_WIFI_SLEEP_NOT_GRANTED#
#define SL_STATUS_WIFI_SLEEP_NOT_GRANTEDValue:
((sl_status_t)0x0B09)
The WFx does not go back to sleep.
SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ERROR#
#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ERRORValue:
((sl_status_t)0x0B10)
The SecureLink MAC key was not found.
SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ALREADY_BURNED#
#define SL_STATUS_WIFI_SECURE_LINK_MAC_KEY_ALREADY_BURNEDValue:
((sl_status_t)0x0B11)
The SecureLink MAC key is already installed in OTP.
SL_STATUS_WIFI_SECURE_LINK_RAM_MODE_NOT_ALLOWED#
#define SL_STATUS_WIFI_SECURE_LINK_RAM_MODE_NOT_ALLOWEDValue:
((sl_status_t)0x0B12)
The SecureLink MAC key cannot be installed in RAM.
SL_STATUS_WIFI_SECURE_LINK_FAILED_UNKNOWN_MODE#
#define SL_STATUS_WIFI_SECURE_LINK_FAILED_UNKNOWN_MODEValue:
((sl_status_t)0x0B13)
The SecureLink MAC key installation failed.
SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILED#
#define SL_STATUS_WIFI_SECURE_LINK_EXCHANGE_FAILEDValue:
((sl_status_t)0x0B14)
SecureLink key (re)negotiation failed.
SL_STATUS_WIFI_WRONG_STATE#
#define SL_STATUS_WIFI_WRONG_STATEValue:
((sl_status_t)0x0B18)
The device is in an inappropriate state to perform the request.
SL_STATUS_WIFI_CHANNEL_NOT_ALLOWED#
#define SL_STATUS_WIFI_CHANNEL_NOT_ALLOWEDValue:
((sl_status_t)0x0B19)
The request failed due to regulatory limitations.
SL_STATUS_WIFI_NO_MATCHING_AP#
#define SL_STATUS_WIFI_NO_MATCHING_APValue:
((sl_status_t)0x0B1A)
The connection request failed because no suitable AP was found.
SL_STATUS_WIFI_CONNECTION_ABORTED#
#define SL_STATUS_WIFI_CONNECTION_ABORTEDValue:
((sl_status_t)0x0B1B)
The connection request was aborted by host.
SL_STATUS_WIFI_CONNECTION_TIMEOUT#
#define SL_STATUS_WIFI_CONNECTION_TIMEOUTValue:
((sl_status_t)0x0B1C)
The connection request failed because of a timeout.
SL_STATUS_WIFI_CONNECTION_REJECTED_BY_AP#
#define SL_STATUS_WIFI_CONNECTION_REJECTED_BY_APValue:
((sl_status_t)0x0B1D)
The connection request failed because the AP rejected the device.
SL_STATUS_WIFI_CONNECTION_AUTH_FAILURE#
#define SL_STATUS_WIFI_CONNECTION_AUTH_FAILUREValue:
((sl_status_t)0x0B1E)
The connection request failed because the WPA handshake did not complete successfully.
SL_STATUS_WIFI_RETRY_EXCEEDED#
#define SL_STATUS_WIFI_RETRY_EXCEEDEDValue:
((sl_status_t)0x0B1F)
The request failed because the retry limit was exceeded.
SL_STATUS_WIFI_TX_LIFETIME_EXCEEDED#
#define SL_STATUS_WIFI_TX_LIFETIME_EXCEEDEDValue:
((sl_status_t)0x0B20)
The request failed because the MSDU life time was exceeded.
SL_STATUS_COMPUTE_DRIVER_FAULT#
#define SL_STATUS_COMPUTE_DRIVER_FAULTValue:
((sl_status_t)0x1501)
Critical fault.
SL_STATUS_COMPUTE_DRIVER_ALU_NAN#
#define SL_STATUS_COMPUTE_DRIVER_ALU_NANValue:
((sl_status_t)0x1502)
ALU operation output NaN.
SL_STATUS_COMPUTE_DRIVER_ALU_OVERFLOW#
#define SL_STATUS_COMPUTE_DRIVER_ALU_OVERFLOWValue:
((sl_status_t)0x1503)
ALU numeric overflow.
SL_STATUS_COMPUTE_DRIVER_ALU_UNDERFLOW#
#define SL_STATUS_COMPUTE_DRIVER_ALU_UNDERFLOWValue:
((sl_status_t)0x1504)
ALU numeric underflow.
SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_OVERFLOW#
#define SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_OVERFLOWValue:
((sl_status_t)0x1505)
Overflow during array store.
SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_UNDERFLOW#
#define SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_UNDERFLOWValue:
((sl_status_t)0x1506)
Underflow during array store conversion.
SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_INFINITY#
#define SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_INFINITYValue:
((sl_status_t)0x1507)
Infinity encountered during array store conversion.
SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_NAN#
#define SL_STATUS_COMPUTE_DRIVER_STORE_CONVERSION_NANValue:
((sl_status_t)0x1508)
NaN encountered during array store conversion.
SL_STATUS_COMPUTE_MATH_NAN#
#define SL_STATUS_COMPUTE_MATH_NANValue:
((sl_status_t)0x1512)
MATH NaN encountered.
SL_STATUS_COMPUTE_MATH_INFINITY#
#define SL_STATUS_COMPUTE_MATH_INFINITYValue:
((sl_status_t)0x1513)
MATH Infinity encountered.
SL_STATUS_COMPUTE_MATH_OVERFLOW#
#define SL_STATUS_COMPUTE_MATH_OVERFLOWValue:
((sl_status_t)0x1514)
MATH numeric overflow.
SL_STATUS_COMPUTE_MATH_UNDERFLOW#
#define SL_STATUS_COMPUTE_MATH_UNDERFLOWValue:
((sl_status_t)0x1515)
MATH numeric underflow.