LCD - Liquid Crystal Display#
Liquid Crystal Display (LCD) Peripheral API.
This module contains functions to control the LDC peripheral of Silicon Labs 32-bit MCUs and SoCs. The LCD driver can drive up to 8x36 segmented LCD directly. The animation feature makes it possible to have active animations without the CPU intervention.
Modules#
Enumerations#
MUX setting.
Wave type.
Bias setting.
VLCD Voltage Source.
Contrast Configuration.
Voltage Boost Level - Data sheets document setting for each part number.
Frame Counter Clock Prescaler, FC-CLK = FrameRate (Hz) / this factor.
Segment selection.
Update Data Control.
Animation Shift operation; none, left or right.
Animation Logic Control, how AReg and BReg should be combined.
Functions#
Initialize the Liquid Crystal Display (LCD) controller.
Select a source for VLCD.
Configure Update Control.
Initialize the LCD Frame Counter.
Configure the LCD controller Animation feature.
Enables updating this range of LCD segment lines.
Turn on or clear a segment.
Update 0-31 lowest segments on a given COM-line in one operation according to the bit mask.
Update the high (32-39) segments on a given COM-line in one operation.
Configure the contrast level on the LCD panel.
Configure the bias level on the LCD panel.
Configure voltage booster.
Enable or disable LCD controller.
Enable or disable LCD Animation feature.
Enable or disable the LCD blink.
Disable all segments while keeping segment state.
Enable or disable LCD Frame counter.
Return the current animation state.
Return the current blink state.
When set, LCD registers will not be updated until cleared.
Return SYNCBUSY bits, indicating which registers have pending updates.
Poll LCD SYNCBUSY flags until the flag has been cleared.
Get pending LCD interrupt flags.
Get enabled and pending LCD interrupt flags.
Set one or more pending LCD interrupts from SW.
Enable LCD interrupts.
Disable LCD interrupts.
Clear one or more interrupt flags.
Macros#
Default Clock Prescaler.
Default LCD Frame Rate Divisor.
Default LCD Contrast.
Default configuration for LCD initialization structure, enables 160 segments.
Frame counter uses a maximum of 5 bits (FCTOP[5:0]).
Enumeration Documentation#
LCD_Mux_TypeDef#
LCD_Mux_TypeDef
MUX setting.
| Enumerator | |
|---|---|
| lcdMuxStatic | Static (segments can be multiplexed with LCD_COM[0]). |
| lcdMuxDuplex | Duplex / 1/2 Duty cycle (segments can be multiplexed with LCD_COM[0:1]). |
| lcdMuxTriplex | Triplex / 1/3 Duty cycle (segments can be multiplexed with LCD_COM[0:2]). |
| lcdMuxQuadruplex | Quadruplex / 1/4 Duty cycle (segments can be multiplexed with LCD_COM[0:3]). |
LCD_Wave_TypeDef#
LCD_Wave_TypeDef
Wave type.
| Enumerator | |
|---|---|
| lcdWaveLowPower | Low power optimized waveform output. |
| lcdWaveNormal | Regular waveform output. |
LCD_Bias_TypeDef#
LCD_Bias_TypeDef
Bias setting.
| Enumerator | |
|---|---|
| lcdBiasStatic | Static (2 levels). |
| lcdBiasOneHalf | 1/2 Bias (3 levels). |
| lcdBiasOneThird | 1/3 Bias (4 levels). |
LCD_VLCDSel_TypeDef#
LCD_VLCDSel_TypeDef
VLCD Voltage Source.
| Enumerator | |
|---|---|
| lcdVLCDSelVDD | VLCD Powered by VDD. |
| lcdVLCDSelVExtBoost | VLCD Powered by external VDD / Voltage Boost. |
LCD_ConConf_TypeDef#
LCD_ConConf_TypeDef
Contrast Configuration.
| Enumerator | |
|---|---|
| lcdConConfVLCD | Contrast is adjusted relative to VDD (VLCD). |
| lcdConConfGND | Contrast is adjusted relative to Ground. |
LCD_VBoostLevel_TypeDef#
LCD_VBoostLevel_TypeDef
Voltage Boost Level - Data sheets document setting for each part number.
| Enumerator | |
|---|---|
| lcdVBoostLevel0 | Voltage boost LEVEL0. |
| lcdVBoostLevel1 | Voltage boost LEVEL1. |
| lcdVBoostLevel2 | Voltage boost LEVEL2. |
| lcdVBoostLevel3 | Voltage boost LEVEL3. |
| lcdVBoostLevel4 | Voltage boost LEVEL4. |
| lcdVBoostLevel5 | Voltage boost LEVEL5. |
| lcdVBoostLevel6 | Voltage boost LEVEL6. |
| lcdVBoostLevel7 | Voltage boost LEVEL7. |
LCD_FCPreScale_TypeDef#
LCD_FCPreScale_TypeDef
Frame Counter Clock Prescaler, FC-CLK = FrameRate (Hz) / this factor.
| Enumerator | |
|---|---|
| lcdFCPrescDiv1 | Prescale Div 1. |
| lcdFCPrescDiv2 | Prescale Div 2. |
| lcdFCPrescDiv4 | Prescale Div 4. |
| lcdFCPrescDiv8 | Prescale Div 8. |
LCD_SegmentRange_TypeDef#
LCD_SegmentRange_TypeDef
Segment selection.
| Enumerator | |
|---|---|
| lcdSegment0_3 | Select segment lines 0 to 3. |
| lcdSegment4_7 | Select segment lines 4 to 7. |
| lcdSegment8_11 | Select segment lines 8 to 11. |
| lcdSegment12_15 | Select segment lines 12 to 15. |
| lcdSegment16_19 | Select segment lines 16 to 19. |
| lcdSegment20_23 | Select segment lines 20 to 23. |
| lcdSegment24_27 | Select segment lines 24 to 27. |
| lcdSegment28_31 | Select segment lines 28 to 31. |
| lcdSegment32_35 | Select segment lines 32 to 35. |
| lcdSegment36_39 | Select segment lines 36 to 39. |
| lcdSegmentAll | Select all segment lines. |
LCD_UpdateCtrl_TypeDef#
LCD_UpdateCtrl_TypeDef
Update Data Control.
| Enumerator | |
|---|---|
| lcdUpdateCtrlRegular | Regular update, data transfer done immediately. |
| lcdUpdateCtrlFCEvent | Data transfer done at Frame Counter event. |
| lcdUpdateCtrlFrameStart | Data transfer done at Frame Start. |
LCD_AnimShift_TypeDef#
LCD_AnimShift_TypeDef
Animation Shift operation; none, left or right.
| Enumerator | |
|---|---|
| lcdAnimShiftNone | No shift. |
| lcdAnimShiftLeft | Shift segment bits left. |
| lcdAnimShiftRight | Shift segment bits right. |
LCD_AnimLogic_TypeDef#
LCD_AnimLogic_TypeDef
Animation Logic Control, how AReg and BReg should be combined.
| Enumerator | |
|---|---|
| lcdAnimLogicAnd | Use bitwise logic AND to mix animation register A (AREGA) and B (AREGB). |
| lcdAnimLogicOr | Use bitwise logic OR to mix animation register A (AREGA) and B (AREGB). |
Function Documentation#
LCD_Init#
void LCD_Init (const LCD_Init_TypeDef * lcdInit)
Initialize the Liquid Crystal Display (LCD) controller.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const LCD_Init_TypeDef * | [in] | lcdInit | A pointer to the initialization structure which configures the LCD controller. |
Configures the LCD controller. You must enable it afterwards, potentially configuring Frame Control and interrupts first according to requirements.
LCD_VLCDSelect#
void LCD_VLCDSelect (LCD_VLCDSel_TypeDef vlcd)
Select a source for VLCD.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LCD_VLCDSel_TypeDef | [in] | vlcd | Select a source for the VLCD voltage. |
LCD_UpdateCtrl#
void LCD_UpdateCtrl (LCD_UpdateCtrl_TypeDef ud)
Configure Update Control.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LCD_UpdateCtrl_TypeDef | [in] | ud | Configures the LCD update method. |
LCD_FrameCountInit#
void LCD_FrameCountInit (const LCD_FrameCountInit_TypeDef * fcInit)
Initialize the LCD Frame Counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const LCD_FrameCountInit_TypeDef * | [in] | fcInit | A pointer to the Frame Counter initialization structure. |
LCD_AnimInit#
void LCD_AnimInit (const LCD_AnimInit_TypeDef * animInit)
Configure the LCD controller Animation feature.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const LCD_AnimInit_TypeDef * | [in] | animInit | A pointer to the LCD Animation initialization structure. |
LCD_SegmentRangeEnable#
void LCD_SegmentRangeEnable (LCD_SegmentRange_TypeDef segmentRange, bool enable)
Enables updating this range of LCD segment lines.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LCD_SegmentRange_TypeDef | [in] | segmentRange | A range of 4 LCD segment lines to enable or disable for all enabled COM lines. |
| bool | [in] | enable | Boolean true to enable segment updates, false to disable updates. |
LCD_SegmentSet#
void LCD_SegmentSet (int com, int bit, bool enable)
Turn on or clear a segment.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int | [in] | com | A COM line to change. |
| int | [in] | bit | A bit index indicating which field to change. |
| bool | [in] | enable | True will set segment, false will clear segment. |
Note
For the Gecko Family, the maximum configuration is (COM-lines x Segment-Lines) 4x40. For the Tiny Gecko Family, the maximum configuration is 8x20 or 4x24. For the Giant Gecko Family, the maximum configuration is 8x36 or 4x40. For the Series 2 Family, the maximum configuration is 4x20. For the Series 2 xG28, the maximum configuration is 8x24 or 4x28.
LCD_SegmentSetLow#
void LCD_SegmentSetLow (int com, uint32_t mask, uint32_t bits)
Update 0-31 lowest segments on a given COM-line in one operation according to the bit mask.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int | [in] | com | Indicates a COM line to update. |
| uint32_t | [in] | mask | A bit mask for segments 0-31. |
| uint32_t | [in] | bits | A bit pattern for segments 0-31. |
LCD_SegmentSetHigh#
void LCD_SegmentSetHigh (int com, uint32_t mask, uint32_t bits)
Update the high (32-39) segments on a given COM-line in one operation.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int | [in] | com | Indicates a COM line to update. |
| uint32_t | [in] | mask | A bit mask for segments 32-39. |
| uint32_t | [in] | bits | A bit pattern for segments 32-39. |
LCD_ContrastSet#
void LCD_ContrastSet (int level)
Configure the contrast level on the LCD panel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| int | [in] | level | The contrast level in range 0-63. |
LCD_BiasSet#
void LCD_BiasSet (LCD_Bias_TypeDef bias)
Configure the bias level on the LCD panel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LCD_Bias_TypeDef | [in] | bias | The bias level. |
LCD_VBoostSet#
void LCD_VBoostSet (LCD_VBoostLevel_TypeDef vboost)
Configure voltage booster.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| LCD_VBoostLevel_TypeDef | [in] | vboost | Voltage boost level |
The resulting voltage level is described in each part number's data sheet
LCD_Enable#
void LCD_Enable (bool enable)
Enable or disable LCD controller.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | If true, enables LCD controller with current configuration. If false, disables LCD controller. Enable CMU clock for LCD for correct operation. |
LCD_AnimEnable#
void LCD_AnimEnable (bool enable)
Enable or disable LCD Animation feature.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | Boolean true enables animation, false disables animation. |
LCD_BlinkEnable#
void LCD_BlinkEnable (bool enable)
Enable or disable the LCD blink.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | Boolean true enables blink, false disables blink. |
LCD_BlankEnable#
void LCD_BlankEnable (bool enable)
Disable all segments while keeping segment state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | Boolean true clears all segments, boolean false restores all segment lines. |
LCD_FrameCountEnable#
void LCD_FrameCountEnable (bool enable)
Enable or disable LCD Frame counter.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | Boolean true enables frame counter, false disables frame counter. |
LCD_AnimState#
int LCD_AnimState (void )
Return the current animation state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Animation state, in range 0-15.
LCD_BlinkState#
int LCD_BlinkState (void )
Return the current blink state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Return value is 1 if segments are enabled, 0 if disabled.
LCD_FreezeEnable#
void LCD_FreezeEnable (bool enable)
When set, LCD registers will not be updated until cleared.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | [in] | enable | When enable is true, update is stopped; when false, all registers are updated. |
LCD_SyncBusyGet#
uint32_t LCD_SyncBusyGet (void )
Return SYNCBUSY bits, indicating which registers have pending updates.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Bit fields for LCD registers that have pending updates.
LCD_SyncBusyDelay#
void LCD_SyncBusyDelay (uint32_t flags)
Poll LCD SYNCBUSY flags until the flag has been cleared.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flags | Bit fields for LCD registers that will be updated before we continue. |
LCD_IntGet#
uint32_t LCD_IntGet (void )
Get pending LCD interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Pending LCD interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the LCD module (LCD_IFS_nnn).
LCD_IntGetEnabled#
uint32_t LCD_IntGetEnabled (void )
Get enabled and pending LCD interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Event bits are not cleared by the use of this function.
Returns
Pending and enabled LCD interrupt sources. Return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in LCD_IEN_nnn register (LCD_IEN_nnn) and
the bitwise OR combination of valid interrupt flags of LCD module (LCD_IF_nnn).
LCD_IntSet#
void LCD_IntSet (uint32_t flags)
Set one or more pending LCD interrupts from SW.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flags | LCD interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the LCD module (LCD_IFS_nnn). |
LCD_IntEnable#
void LCD_IntEnable (uint32_t flags)
Enable LCD interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flags | LCD interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for LCD module (LCD_IFS_nnn). |
LCD_IntDisable#
void LCD_IntDisable (uint32_t flags)
Disable LCD interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flags | LCD interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for LCD module (LCD_IFS_nnn). |
LCD_IntClear#
void LCD_IntClear (uint32_t flags)
Clear one or more interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | flags | LCD interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for LCD module (LCD_IFS_nnn). |
Macro Definition Documentation#
LCD_INIT_DEFAULT#
#define LCD_INIT_DEFAULTValue:
Default configuration for LCD initialization structure, enables 160 segments.
LCD_FRAME_COUNTER_VAL_MAX#
#define LCD_FRAME_COUNTER_VAL_MAXValue:
64
Frame counter uses a maximum of 5 bits (FCTOP[5:0]).