QSPI Octal-SPI#
QSPI Octal-SPI Controller API.
These QSPI functions provide basic support for using the QSPI peripheral in the following configurations:
Direct Read/Write, used for memory mapped access to external memory.
STIG Command, used for configuring and executing commands on the external memory device.
Indirect read/write, PHY configuration, and Execute-In-Place (XIP) configurations are not supported.
The example below shows how to set up the QSPI for direct read and write operation:
CMU_ClockEnable(cmuClock_GPIO, true);
CMU_ClockEnable(cmuClock_QSPI0, true);
QSPI_Init_TypeDef initQspi = QSPI_INIT_DEFAULT;
QSPI_Init(QSPI0, &initQspi);
// Configure QSPI pins.
GPIO_PinModeSet(EXTFLASH_PORT_CS, EXTFLASH_PIN_CS, gpioModePushPull, 0);
GPIO_PinModeSet(EXTFLASH_PORT_SCLK, EXTFLASH_PIN_SCLK, gpioModePushPull, 0);
GPIO_PinModeSet(EXTFLASH_PORT_DQ0, EXTFLASH_PIN_DQ0, gpioModePushPull, 0);
GPIO_PinModeSet(EXTFLASH_PORT_DQ1, EXTFLASH_PIN_DQ1, gpioModePushPull, 0);
GPIO_PinModeSet(EXTFLASH_PORT_DQ2, EXTFLASH_PIN_DQ2, gpioModePushPull, 0);
GPIO_PinModeSet(EXTFLASH_PORT_DQ3, EXTFLASH_PIN_DQ3, gpioModePushPull, 0);
// Configure QSPI routing to GPIO.
QSPI0->ROUTELOC0 = EXTFLASH_QSPI_LOC;
QSPI0->ROUTEPEN = QSPI_ROUTEPEN_SCLKPEN
| EXTFLASH_QSPI_CSPEN
| QSPI_ROUTEPEN_DQ0PEN
| QSPI_ROUTEPEN_DQ1PEN
| QSPI_ROUTEPEN_DQ2PEN
| QSPI_ROUTEPEN_DQ3PEN;
// Configure the direct read.
QSPI_ReadConfig_TypeDef readConfig = QSPI_READCONFIG_DEFAULT;
readConfig.dummyCycles = 8;
readConfig.opCode = 0x6B;
readConfig.instTransfer = qspiTransferSingle;
readConfig.addrTransfer = qspiTransferSingle;
readConfig.dataTransfer = qspiTransferQuad;
QSPI_ReadConfig(QSPI0, &readConfig);
// Configure the direct write.
QSPI_WriteConfig_TypeDef writeConfig = QSPI_WRITECONFIG_DEFAULT;
writeConfig.dummyCycles = 0;
writeConfig.opCode = 0x38;
writeConfig.addrTransfer = qspiTransferQuad;
writeConfig.dataTransfer = qspiTransferQuad;
writeConfig.autoWEL = true;
QSPI_WriteConfig(QSPI0, &writeConfig);
To configure an external flash, commands can be set up and executed using the Software Triggered Instruction Generator (STIG) function of the QSPI, as shown in the example below:
uint8_t status;
QSPI_StigCmd_TypeDef stigCmd = {0};
stigCmd.cmdOpcode = EXTFLASH_OPCODE_READ_STATUS;
stigCmd.readDataSize = 1;
stigCmd.readBuffer = &status;
QSPI_ExecStigCmd(QSPI0, &stigCmd);
Modules#
Enumerations#
Transfer type.
Functions#
Initialize QSPI.
Configure Read Operations.
Configure Write Operations.
Execute a STIG command.
Wait for the QSPI to go into idle state.
Get the fill level of the write partition of the QSPI internal SRAM.
Get the fill level of the read partition of the QSPI internal SRAM.
Enable/disable Quad SPI.
Get the current interrupt flags.
Clear interrupt flags.
Enable interrupts.
Disable interrupts.
Macros#
Default Read Configuration Structure.
Default Write Configuration Structure.
Default configuration for QSPI_Init_TypeDef structure.
Enumeration Documentation#
QSPI_TransferType_TypeDef#
QSPI_TransferType_TypeDef
Transfer type.
| Enumerator | |
|---|---|
| qspiTransferSingle | Single IO mode. |
| qspiTransferDual | Dual I/O transfer. |
| qspiTransferQuad | Quad I/O transfer. |
| qspiTransferOctal | Octal I/O transfer. |
Function Documentation#
QSPI_Init#
void QSPI_Init (QSPI_TypeDef * qspi, const QSPI_Init_TypeDef * init)
Initialize QSPI.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | A pointer to the QSPI peripheral register block. |
| const QSPI_Init_TypeDef * | [in] | init | A pointer to the initialization structure used to configure QSPI. |
QSPI_ReadConfig#
void QSPI_ReadConfig (QSPI_TypeDef * qspi, const QSPI_ReadConfig_TypeDef * config)
Configure Read Operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | A pointer to the QSPI peripheral register block. |
| const QSPI_ReadConfig_TypeDef * | [in] | config | A pointer to the configuration structure for QSPI read operations. |
QSPI_WriteConfig#
void QSPI_WriteConfig (QSPI_TypeDef * qspi, const QSPI_WriteConfig_TypeDef * config)
Configure Write Operations.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | A pointer to the QSPI peripheral register block. |
| const QSPI_WriteConfig_TypeDef * | [in] | config | A pointer to the configuration structure for QSPI write operations. |
QSPI_ExecStigCmd#
void QSPI_ExecStigCmd (QSPI_TypeDef * qspi, const QSPI_StigCmd_TypeDef * stigCmd)
Execute a STIG command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | A pointer to the QSPI peripheral register block. |
| const QSPI_StigCmd_TypeDef * | [in] | stigCmd | A pointer to a structure that describes the STIG command. |
STIG is used when the application needs to access status registers, configuration registers or perform erase functions. STIG commands can be used to perform any instruction that the flash device supports.
QSPI_WaitForIdle#
void QSPI_WaitForIdle (QSPI_TypeDef * qspi)
Wait for the QSPI to go into idle state.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | Pointer to QSPI peripheral register block. |
QSPI_GetWriteLevel#
uint16_t QSPI_GetWriteLevel (QSPI_TypeDef * qspi)
Get the fill level of the write partition of the QSPI internal SRAM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | Pointer to QSPI peripheral register block. |
Returns
SRAM fill level of the write partition. The value is the number of 4 byte words in the write partition.
QSPI_GetReadLevel#
uint16_t QSPI_GetReadLevel (QSPI_TypeDef * qspi)
Get the fill level of the read partition of the QSPI internal SRAM.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | Pointer to QSPI peripheral register block. |
Returns
SRAM fill level of the read partition. The value is the number of 4 byte words in the read partition.
QSPI_Enable#
void QSPI_Enable (QSPI_TypeDef * qspi, bool enable)
Enable/disable Quad SPI.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | Pointer to QSPI peripheral register block. |
| bool | [in] | enable | true to enable Quad SPI, false to disable Quad SPI. |
QSPI_IntGet#
uint32_t QSPI_IntGet (QSPI_TypeDef * qspi)
Get the current interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | Pointer to QSPI peripheral register block. |
Returns
This functions returns the current interrupt flags that are set.
QSPI_IntClear#
void QSPI_IntClear (QSPI_TypeDef * qspi, uint32_t flags)
Clear interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | Pointer to QSPI peripheral register block. |
| uint32_t | [in] | flags | The interrupt flags to clear. |
QSPI_IntEnable#
void QSPI_IntEnable (QSPI_TypeDef * qspi, uint32_t flags)
Enable interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | Pointer to QSPI peripheral register block. |
| uint32_t | [in] | flags | The interrupt flags to enable. |
QSPI_IntDisable#
void QSPI_IntDisable (QSPI_TypeDef * qspi, uint32_t flags)
Disable interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| QSPI_TypeDef * | [in] | qspi | Pointer to QSPI peripheral register block. |
| uint32_t | [in] | flags | The interrupt flags to disable. |