IDAC - Current DAC#

Current Digital-to-Analog Converter (IDAC) Peripheral API.

IDAC can source or sink a configurable constant current, which can be output on, or sinked from pin or ADC. Current is configurable with several ranges of various step sizes. IDAC can be used with PRS and can operate down to EM3.

The following steps are necessary for basic operation:

Clock enable:

/* IDAC is a HFPERCLK peripheral */
CMU_ClockEnable(cmuClock_HFPER, true);
CMU_ClockEnable(cmuClock_IDAC0, true);

Initialize peripheral with default settings and modify selected fields, such as output select:

/* Initialize with default settings. Change output to ADC. */
IDAC_Init_TypeDef init = IDAC_INIT_DEFAULT;
init.outMode = idacOutputADC;
IDAC_Init(IDAC0, &init);

Set output:

/* Set 50nA step and enable output */
IDAC_StepSet(IDAC0, 0);
IDAC_OutEnable(IDAC0, true);

Modules#

IDAC_Init_TypeDef

Enumerations#

enum
idacOutputPin = IDAC_CTRL_OUTMODE_PIN
idacOutputADC = IDAC_CTRL_OUTMODE_ADC
}

Output mode.

enum
idacPRSSELCh0 = IDAC_CTRL_PRSSEL_PRSCH0
idacPRSSELCh1 = IDAC_CTRL_PRSSEL_PRSCH1
idacPRSSELCh2 = IDAC_CTRL_PRSSEL_PRSCH2
idacPRSSELCh3 = IDAC_CTRL_PRSSEL_PRSCH3
idacPRSSELCh4 = IDAC_CTRL_PRSSEL_PRSCH4
idacPRSSELCh5 = IDAC_CTRL_PRSSEL_PRSCH5
}

Selects which Peripheral Reflex System (PRS) signal to use when PRS is set to control IDAC output.

enum
idacCurrentRange0 = IDAC_CURPROG_RANGESEL_RANGE0
idacCurrentRange1 = IDAC_CURPROG_RANGESEL_RANGE1
idacCurrentRange2 = IDAC_CURPROG_RANGESEL_RANGE2
idacCurrentRange3 = IDAC_CURPROG_RANGESEL_RANGE3
}

Selects which current range to use.

Functions#

void
IDAC_Init(IDAC_TypeDef *idac, const IDAC_Init_TypeDef *init)

Initialize IDAC.

void
IDAC_Enable(IDAC_TypeDef *idac, bool enable)

Enable/disable IDAC.

void
IDAC_Reset(IDAC_TypeDef *idac)

Reset IDAC to the same state that it was in after a hardware reset.

void
IDAC_MinimalOutputTransitionMode(IDAC_TypeDef *idac, bool enable)

Enable/disable Minimal Output Transition mode.

void
IDAC_RangeSet(IDAC_TypeDef *idac, const IDAC_Range_TypeDef range)

Set the current range of the IDAC output.

void
IDAC_StepSet(IDAC_TypeDef *idac, const uint32_t step)

Set the current step of the IDAC output.

void
IDAC_OutEnable(IDAC_TypeDef *idac, bool enable)

Enable/disable the IDAC OUT pin.

Macros#

#define

Default configuration for IDAC initialization structure.

Enumeration Documentation#

IDAC_OutMode_TypeDef#

IDAC_OutMode_TypeDef

Output mode.

Enumerator
idacOutputPin

Output to IDAC OUT pin.

idacOutputADC

Output to ADC.


IDAC_PRSSEL_TypeDef#

IDAC_PRSSEL_TypeDef

Selects which Peripheral Reflex System (PRS) signal to use when PRS is set to control IDAC output.

Enumerator
idacPRSSELCh0

PRS channel 0.

idacPRSSELCh1

PRS channel 1.

idacPRSSELCh2

PRS channel 2.

idacPRSSELCh3

PRS channel 3.

idacPRSSELCh4

PRS channel 4.

idacPRSSELCh5

PRS channel 5.


IDAC_Range_TypeDef#

IDAC_Range_TypeDef

Selects which current range to use.

Enumerator
idacCurrentRange0

current range 0.

idacCurrentRange1

current range 1.

idacCurrentRange2

current range 2.

idacCurrentRange3

current range 3.


Function Documentation#

IDAC_Init#

void IDAC_Init (IDAC_TypeDef * idac, const IDAC_Init_TypeDef * init)

Initialize IDAC.

Parameters
TypeDirectionArgument NameDescription
IDAC_TypeDef *[in]idac

A pointer to the IDAC peripheral register block.

const IDAC_Init_TypeDef *[in]init

A pointer to the IDAC initialization structure.

Initializes IDAC according to the initialization structure parameter and sets the default calibration value stored in the DEVINFO structure.

Note

  • This function will disable IDAC prior to configuration.


IDAC_Enable#

void IDAC_Enable (IDAC_TypeDef * idac, bool enable)

Enable/disable IDAC.

Parameters
TypeDirectionArgument NameDescription
IDAC_TypeDef *[in]idac

A pointer to the IDAC peripheral register block.

bool[in]enable

True to enable IDAC, false to disable.


IDAC_Reset#

void IDAC_Reset (IDAC_TypeDef * idac)

Reset IDAC to the same state that it was in after a hardware reset.

Parameters
TypeDirectionArgument NameDescription
IDAC_TypeDef *[in]idac

A pointer to the IDAC peripheral register block.


IDAC_MinimalOutputTransitionMode#

void IDAC_MinimalOutputTransitionMode (IDAC_TypeDef * idac, bool enable)

Enable/disable Minimal Output Transition mode.

Parameters
TypeDirectionArgument NameDescription
IDAC_TypeDef *[in]idac

A pointer to the IDAC peripheral register block.

bool[in]enable

True to enable Minimal Output Transition mode, false to disable.


IDAC_RangeSet#

void IDAC_RangeSet (IDAC_TypeDef * idac, const IDAC_Range_TypeDef range)

Set the current range of the IDAC output.

Parameters
TypeDirectionArgument NameDescription
IDAC_TypeDef *[in]idac

A pointer to the IDAC peripheral register block.

const IDAC_Range_TypeDef[in]range

The current range value.

This function sets the current range of the IDAC output. The function also updates the IDAC calibration register (IDAC_CAL) with the default calibration value from DEVINFO (factory calibration) corresponding to the specified range.


IDAC_StepSet#

void IDAC_StepSet (IDAC_TypeDef * idac, const uint32_t step)

Set the current step of the IDAC output.

Parameters
TypeDirectionArgument NameDescription
IDAC_TypeDef *[in]idac

A pointer to the IDAC peripheral register block.

const uint32_t[in]step

A step value for the IDAC output. A valid range is 0-31.


IDAC_OutEnable#

void IDAC_OutEnable (IDAC_TypeDef * idac, bool enable)

Enable/disable the IDAC OUT pin.

Parameters
TypeDirectionArgument NameDescription
IDAC_TypeDef *[in]idac

A pointer to the IDAC peripheral register block.

bool[in]enable

True to enable the IDAC OUT pin, false to disable.

Warnings

  • This function will not enable/disable the IDAC OUT pin if APORTOUTENPRS is set because output enable will be controlled by PRS.


Macro Definition Documentation#

IDAC_INIT_DEFAULT#

#define IDAC_INIT_DEFAULT
Value:
{ \
false, /**< Leave IDAC disabled when initialization done. */ \
idacOutputPin, /**< Output to IDAC output pin. */ \
false, /**< Disable PRS triggering. */ \
idacPRSSELCh0, /**< Select PRS ch0 (if PRS triggering enabled). */ \
false /**< Disable current sink mode. */ \
}

Default configuration for IDAC initialization structure.