GPIO - General Purpose Input/Output#

General Purpose Input/Output (GPIO) API.

This module contains functions to control the GPIO peripheral of Silicon Labs 32-bit MCUs and SoCs. The GPIO peripheral is used for pin configuration and direct pin manipulation and sensing as well as routing for peripheral pin connections.

Enumerations#

enum
gpioPortA = 0
gpioPortB = 1
gpioPortC = 2
gpioPortD = 3
gpioPortF = 5
gpioPortI = 8
gpioPortJ = 9
gpioPortK = 10
}

GPIO ports IDs.

enum
gpioDriveStrengthWeakAlternateWeak = GPIO_P_CTRL_DRIVESTRENGTH_WEAK | GPIO_P_CTRL_DRIVESTRENGTHALT_WEAK
gpioDriveStrengthWeakAlternateStrong = GPIO_P_CTRL_DRIVESTRENGTH_WEAK | GPIO_P_CTRL_DRIVESTRENGTHALT_STRONG
gpioDriveStrengthStrongAlternateWeak = GPIO_P_CTRL_DRIVESTRENGTH_STRONG | GPIO_P_CTRL_DRIVESTRENGTHALT_WEAK
gpioDriveStrengthStrongAlternateStrong = GPIO_P_CTRL_DRIVESTRENGTH_STRONG | GPIO_P_CTRL_DRIVESTRENGTHALT_STRONG
}

GPIO drive strength.

enum
gpioModeDisabled = _GPIO_P_MODEL_MODE0_DISABLED
gpioModeInput = _GPIO_P_MODEL_MODE0_INPUT
gpioModeInputPull = _GPIO_P_MODEL_MODE0_INPUTPULL
gpioModeInputPullFilter = _GPIO_P_MODEL_MODE0_INPUTPULLFILTER
gpioModePushPull = _GPIO_P_MODEL_MODE0_PUSHPULL
gpioModePushPullAlternate = _GPIO_P_MODEL_MODE0_PUSHPULLALT
gpioModeWiredOr = _GPIO_P_MODEL_MODE0_WIREDOR
gpioModeWiredOrPullDown = _GPIO_P_MODEL_MODE0_WIREDORPULLDOWN
gpioModeWiredAnd = _GPIO_P_MODEL_MODE0_WIREDAND
gpioModeWiredAndFilter = _GPIO_P_MODEL_MODE0_WIREDANDFILTER
gpioModeWiredAndPullUp = _GPIO_P_MODEL_MODE0_WIREDANDPULLUP
gpioModeWiredAndPullUpFilter = _GPIO_P_MODEL_MODE0_WIREDANDPULLUPFILTER
gpioModeWiredAndAlternate = _GPIO_P_MODEL_MODE0_WIREDANDALT
gpioModeWiredAndAlternateFilter = _GPIO_P_MODEL_MODE0_WIREDANDALTFILTER
gpioModeWiredAndAlternatePullUp = _GPIO_P_MODEL_MODE0_WIREDANDALTPULLUP
gpioModeWiredAndAlternatePullUpFilter = _GPIO_P_MODEL_MODE0_WIREDANDALTPULLUPFILTER
}

Pin mode.

Functions#

void
GPIO_DbgLocationSet(unsigned int location)

Sets the pin location of the debug pins (Serial Wire interface).

void

Enable/disable serial wire clock pin.

void
GPIO_DbgSWDIOEnable(bool enable)

Enable/disable serial wire data I/O pin.

void
GPIO_DbgSWOEnable(bool enable)

Enable/Disable serial wire output pin.

void
GPIO_DriveStrengthSet(GPIO_Port_TypeDef port, GPIO_DriveStrength_TypeDef strength)

Sets the drive strength for a GPIO port.

void
GPIO_EM4DisablePinWakeup(uint32_t pinmask)

Disable GPIO pin wake-up from EM4.

void
GPIO_EM4EnablePinWakeup(uint32_t pinmask, uint32_t polaritymask)

Enable GPIO pin wake-up from EM4.

uint32_t

Check which GPIO pin(s) that caused a wake-up from EM4.

void

Enable GPIO pin retention of output enable, output value, pull enable, and pull direction in EM4.

void
GPIO_ExtIntConfig(GPIO_Port_TypeDef port, unsigned int pin, unsigned int intNo, bool risingEdge, bool fallingEdge, bool enable)

Configure the GPIO external pin interrupt.

void
GPIO_EM4WUExtIntConfig(GPIO_Port_TypeDef port, unsigned int pin, uint32_t intNo, bool polarity, bool enable)

Configure EM4WU pins as external level-sensitive interrupts.

void
GPIO_InputSenseSet(uint32_t val, uint32_t mask)

Enable/disable input sensing.

void
GPIO_IntClear(uint32_t flags)

Clear one or more pending GPIO interrupts.

void
GPIO_IntDisable(uint32_t flags)

Disable one or more GPIO interrupts.

void
GPIO_IntEnable(uint32_t flags)

Enable one or more GPIO interrupts.

uint32_t

Get enabled GPIO interrupts.

uint32_t

Get pending GPIO interrupts.

uint32_t

Get enabled and pending GPIO interrupt flags.

void
GPIO_IntSet(uint32_t flags)

Set one or more pending GPIO interrupts from SW.

void
GPIO_Lock(void)

Lock the GPIO configuration.

unsigned int
GPIO_PinInGet(GPIO_Port_TypeDef port, unsigned int pin)

Read the pad value for a single pin in a GPIO port.

void
GPIO_PinLock(GPIO_Port_TypeDef port, unsigned int pin)

Lock all GPIO configuration settings for a given pin.

GPIO_PinModeGet(GPIO_Port_TypeDef port, unsigned int pin)

Get the mode for a GPIO pin.

void
GPIO_PinModeSet(GPIO_Port_TypeDef port, unsigned int pin, GPIO_Mode_TypeDef mode, unsigned int out)

Set the mode for a GPIO pin.

void
GPIO_PinOutClear(GPIO_Port_TypeDef port, unsigned int pin)

Set a single pin in GPIO data out port register to 0.

unsigned int
GPIO_PinOutGet(GPIO_Port_TypeDef port, unsigned int pin)

Get current setting for a pin in a GPIO port data out register.

void
GPIO_PinOutSet(GPIO_Port_TypeDef port, unsigned int pin)

Set a single pin in GPIO data out register to 1.

void
GPIO_PinOutToggle(GPIO_Port_TypeDef port, unsigned int pin)

Toggle a single pin in GPIO port data out register.

uint32_t
GPIO_PortInGet(GPIO_Port_TypeDef port)

Read the pad values for GPIO port.

void
GPIO_PortOutClear(GPIO_Port_TypeDef port, uint32_t pins)

Set bits in DOUT register for a port to 0.

uint32_t
GPIO_PortOutGet(GPIO_Port_TypeDef port)

Get the current setting for a GPIO port data out register.

void
GPIO_PortOutSet(GPIO_Port_TypeDef port, uint32_t pins)

Set bits GPIO data out register to 1.

void
GPIO_PortOutSetVal(GPIO_Port_TypeDef port, uint32_t val, uint32_t mask)

Set GPIO port data out register.

void
GPIO_PortOutToggle(GPIO_Port_TypeDef port, uint32_t pins)

Toggle pins in GPIO port data out register.

void
GPIO_SlewrateSet(GPIO_Port_TypeDef port, uint32_t slewrate, uint32_t slewrateAlt)

Set slewrate for pins on a GPIO port.

void

Unlock the GPIO configuration.

Enumeration Documentation#

GPIO_Port_TypeDef#

GPIO_Port_TypeDef

GPIO ports IDs.

Enumerator
gpioPortA

Port A.

gpioPortB

Port B.

gpioPortC

Port C.

gpioPortD

Port D.

gpioPortF

Port F.

gpioPortI

Port I.

gpioPortJ

Port J.

gpioPortK

Port K.


GPIO_DriveStrength_TypeDef#

GPIO_DriveStrength_TypeDef

GPIO drive strength.

Enumerator
gpioDriveStrengthWeakAlternateWeak

GPIO weak 1mA and alternate function weak 1mA.

gpioDriveStrengthWeakAlternateStrong

GPIO weak 1mA and alternate function strong 10mA.

gpioDriveStrengthStrongAlternateWeak

GPIO strong 10mA and alternate function weak 1mA.

gpioDriveStrengthStrongAlternateStrong

GPIO strong 10mA and alternate function strong 10mA.


GPIO_Mode_TypeDef#

GPIO_Mode_TypeDef

Pin mode.

For more details on each mode, refer to the reference manual.

Enumerator
gpioModeDisabled

Input disabled.

gpioModeInput

Input enabled.

gpioModeInputPull

Input enabled.

gpioModeInputPullFilter

Input enabled with filter.

gpioModePushPull

Push-pull output.

gpioModePushPullAlternate

Push-pull using alternate control.

gpioModeWiredOr

Wired-or output.

gpioModeWiredOrPullDown

Wired-or output with pull-down.

gpioModeWiredAnd

Open-drain output.

gpioModeWiredAndFilter

Open-drain output with filter.

gpioModeWiredAndPullUp

Open-drain output with pull-up.

gpioModeWiredAndPullUpFilter

Open-drain output with filter and pull-up.

gpioModeWiredAndAlternate

Open-drain output using alternate control.

gpioModeWiredAndAlternateFilter

Open-drain output using alternate control with filter.

gpioModeWiredAndAlternatePullUp

Open-drain output using alternate control with pull-up.

gpioModeWiredAndAlternatePullUpFilter

Open-drain output using alternate control with filter and pull-up.


Function Documentation#

GPIO_DbgLocationSet#

void GPIO_DbgLocationSet (unsigned int location)

Sets the pin location of the debug pins (Serial Wire interface).

Parameters
TypeDirectionArgument NameDescription
unsigned int[in]location

The debug pin location to use (0-3).

Note

  • Changing the pins used for debugging uncontrolled, may result in a lockout.


GPIO_DbgSWDClkEnable#

void GPIO_DbgSWDClkEnable (bool enable)

Enable/disable serial wire clock pin.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable
  • false - disable serial wire clock.

  • true - enable serial wire clock (default after reset).

Note

  • Disabling SWDClk will disable the debug interface, which may result in a lockout if done early in startup (before debugger is able to halt core).


GPIO_DbgSWDIOEnable#

void GPIO_DbgSWDIOEnable (bool enable)

Enable/disable serial wire data I/O pin.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable
  • false - disable serial wire data pin.

  • true - enable serial wire data pin (default after reset).

Note

  • Disabling SWDClk will disable the debug interface, which may result in a lockout if done early in startup (before debugger is able to halt core).


GPIO_DbgSWOEnable#

void GPIO_DbgSWOEnable (bool enable)

Enable/Disable serial wire output pin.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable
  • false - disable serial wire viewer pin (default after reset).

  • true - enable serial wire viewer pin.

Note

  • Enabling this pin is not sufficient to fully enable serial wire output, which is also dependent on issues outside the GPIO module. Refer to DBG_SWOEnable().

Warnings

  • If debug port is locked, SWO pin is not disabled automatically. To avoid information leakage through SWO, disable SWO pin after locking debug port.


GPIO_DriveStrengthSet#

void GPIO_DriveStrengthSet (GPIO_Port_TypeDef port, GPIO_DriveStrength_TypeDef strength)

Sets the drive strength for a GPIO port.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

GPIO_DriveStrength_TypeDef[in]strength

The drive strength to use for the port.


GPIO_EM4DisablePinWakeup#

void GPIO_EM4DisablePinWakeup (uint32_t pinmask)

Disable GPIO pin wake-up from EM4.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]pinmask

Bit mask containing the bitwise logic OR of which GPIO pin(s) to disable. Refer to Reference Manuals for pinmask to GPIO port/pin mapping.


GPIO_EM4EnablePinWakeup#

void GPIO_EM4EnablePinWakeup (uint32_t pinmask, uint32_t polaritymask)

Enable GPIO pin wake-up from EM4.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]pinmask

A bitmask containing the bitwise logic OR of which GPIO pin(s) to enable. See Reference Manuals for a pinmask to the GPIO port/pin mapping.

uint32_t[in]polaritymask

A bitmask containing the bitwise logic OR of GPIO pin(s) wake-up polarity. See Reference Manuals for pinmask-to-GPIO port/pin mapping.

When the function exits, EM4 mode can be safely entered.

Note


GPIO_EM4GetPinWakeupCause#

uint32_t GPIO_EM4GetPinWakeupCause (void )

Check which GPIO pin(s) that caused a wake-up from EM4.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Bit mask containing the bitwise logic OR of which GPIO pin(s) caused the wake-up. Refer to Reference Manuals for pinmask to GPIO port/pin mapping.


GPIO_EM4SetPinRetention#

void GPIO_EM4SetPinRetention (bool enable)

Enable GPIO pin retention of output enable, output value, pull enable, and pull direction in EM4.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable
  • true - enable EM4 pin retention.

  • false - disable EM4 pin retention.

Note

  • On series 0 devices EM4 gpio retention can either be turned on or off. On series 1 devices there are three EM4 GPIO retention modes available. These modes are "Disabled", "EM4EXIT" and "SWUNLATCH". Use the EMU_EM4Init() to configure the GPIO retention mode on a series 1 device.

The behavior of this function depends on the configured GPIO retention mode. If the GPIO retention mode is configured to be "SWUNLATCH" then this function will not change anything. If the retention mode is anything else then this function will set the GPIO retention mode to "EM4EXIT" when the enable argument is true, and "Disabled" when false.


GPIO_ExtIntConfig#

void GPIO_ExtIntConfig (GPIO_Port_TypeDef port, unsigned int pin, unsigned int intNo, bool risingEdge, bool fallingEdge, bool enable)

Configure the GPIO external pin interrupt.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The port to associate with the pin.

unsigned int[in]pin

The pin number on the port.

unsigned int[in]intNo

The interrupt number to trigger.

bool[in]risingEdge

Set to true if the interrupt will be enabled on the rising edge. Otherwise, false.

bool[in]fallingEdge

Set to true if the interrupt will be enabled on the falling edge. Otherwise, false.

bool[in]enable

Set to true if the interrupt will be enabled after the configuration is complete. False to leave disabled. See GPIO_IntDisable() and GPIO_IntEnable().

It is recommended to disable interrupts before configuring the GPIO pin interrupt. See GPIO_IntDisable() for more information.

The GPIO interrupt handler must be in place before enabling the interrupt.

Notice that any pending interrupt for the selected interrupt is cleared by this function.

Note

  • On series 0 devices, the pin number parameter is not used. The pin number used on these devices is hardwired to the interrupt with the same number. On series 1 devices, the pin number can be selected freely within a group. Interrupt numbers are divided into 4 groups (intNo / 4) and valid pin number within the interrupt groups are: 0: pins 0-3 (interrupt number 0-3) 1: pins 4-7 (interrupt number 4-7) 2: pins 8-11 (interrupt number 8-11) 3: pins 12-15 (interrupt number 12-15)


GPIO_EM4WUExtIntConfig#

void GPIO_EM4WUExtIntConfig (GPIO_Port_TypeDef port, unsigned int pin, uint32_t intNo, bool polarity, bool enable)

Configure EM4WU pins as external level-sensitive interrupts.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The port to associate with the pin.

unsigned int[in]pin

The pin number on the port.

uint32_t[in]intNo

The EM4WU interrupt number to trigger.

bool[in]polarity

true = Active high level-sensitive interrupt. false = Active low level-sensitive interrupt.

bool[in]enable

Set to true if the interrupt will be enabled after the configuration is complete. False to leave disabled. See GPIO_IntDisable() and GPIO_IntEnable().

It is recommended to disable interrupts before configuring the GPIO pin interrupt. See GPIO_IntDisable() for more information.

The GPIO interrupt handler must be in place before enabling the interrupt.

Notice that any pending interrupt for the selected interrupt is cleared by this function.

Note

  • The selected port/pin must be mapped to an existant EM4WU interrupt. Each EM4WU signal is connected to a fixed pin. Refer to the Alternate Function Table in the device Datasheet for the location of each EM4WU signal. For example, on xG22 device, the interrupt of EM4WU6 is fixed to pin PC00.


GPIO_InputSenseSet#

void GPIO_InputSenseSet (uint32_t val, uint32_t mask)

Enable/disable input sensing.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]val

Bitwise logic OR of one or more of:

  • GPIO_INSENSE_INT - interrupt input sensing.

  • GPIO_INSENSE_PRS - peripheral reflex system input sensing.

uint32_t[in]mask

Mask containing bitwise logic OR of bits similar as for val used to indicate which input sense options to disable/enable.

Disabling input sensing if not used, can save some energy consumption.


GPIO_IntClear#

void GPIO_IntClear (uint32_t flags)

Clear one or more pending GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

Bitwise logic OR of GPIO interrupt sources to clear.


GPIO_IntDisable#

void GPIO_IntDisable (uint32_t flags)

Disable one or more GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

GPIO interrupt sources to disable.


GPIO_IntEnable#

void GPIO_IntEnable (uint32_t flags)

Enable one or more GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

GPIO interrupt sources to enable.

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using GPIO_IntClear() prior to enabling the interrupt.


GPIO_EnabledIntGet#

uint32_t GPIO_EnabledIntGet (void )

Get enabled GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Enabled GPIO interrupt sources.


GPIO_IntGet#

uint32_t GPIO_IntGet (void )

Get pending GPIO interrupts.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • GPIO interrupt sources pending.


GPIO_IntGetEnabled#

uint32_t GPIO_IntGetEnabled (void )

Get enabled and pending GPIO interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by the use of this function.

Returns

  • Pending and enabled GPIO interrupt sources. The return value is the bitwise AND combination of

    • the OR combination of enabled interrupt sources in GPIO_IEN register and

    • the OR combination of valid interrupt flags in GPIO_IF register.


GPIO_IntSet#

void GPIO_IntSet (uint32_t flags)

Set one or more pending GPIO interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

GPIO interrupt sources to set to pending.


GPIO_Lock#

void GPIO_Lock (void )

Lock the GPIO configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A

GPIO_PinInGet#

unsigned int GPIO_PinInGet (GPIO_Port_TypeDef port, unsigned int pin)

Read the pad value for a single pin in a GPIO port.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

unsigned int[in]pin

The pin number to read.

Returns

  • The pin value, 0 or 1.


GPIO_PinLock#

void GPIO_PinLock (GPIO_Port_TypeDef port, unsigned int pin)

Lock all GPIO configuration settings for a given pin.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

unsigned int[in]pin

The pin number to lock.

The lock can only be cleared by a chip reset.


GPIO_PinModeGet#

GPIO_Mode_TypeDef GPIO_PinModeGet (GPIO_Port_TypeDef port, unsigned int pin)

Get the mode for a GPIO pin.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

unsigned int[in]pin

The pin number in the port.

Returns

  • The pin mode.


GPIO_PinModeSet#

void GPIO_PinModeSet (GPIO_Port_TypeDef port, unsigned int pin, GPIO_Mode_TypeDef mode, unsigned int out)

Set the mode for a GPIO pin.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

unsigned int[in]pin

The pin number in the port.

GPIO_Mode_TypeDef[in]mode

The desired pin mode.

unsigned int[in]out

A value to set for the pin in the DOUT register. The DOUT setting is important for some input mode configurations to determine the pull-up/down direction.


GPIO_PinOutClear#

void GPIO_PinOutClear (GPIO_Port_TypeDef port, unsigned int pin)

Set a single pin in GPIO data out port register to 0.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

unsigned int[in]pin

The pin to set.

Note

  • To ensure that the setting takes effect on the output pad, the pin must be configured properly. If not, it will take effect whenever the pin has been properly configured.


GPIO_PinOutGet#

unsigned int GPIO_PinOutGet (GPIO_Port_TypeDef port, unsigned int pin)

Get current setting for a pin in a GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

unsigned int[in]pin

The pin to get setting for.

Returns

  • The DOUT setting for the requested pin, 0 or 1.


GPIO_PinOutSet#

void GPIO_PinOutSet (GPIO_Port_TypeDef port, unsigned int pin)

Set a single pin in GPIO data out register to 1.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

unsigned int[in]pin

The pin to set.

Note

  • To ensure that the setting takes effect on the output pad, the pin must be configured properly. If not, it will take effect whenever the pin has been properly configured.


GPIO_PinOutToggle#

void GPIO_PinOutToggle (GPIO_Port_TypeDef port, unsigned int pin)

Toggle a single pin in GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

unsigned int[in]pin

The pin to toggle.

Note

  • To ensure that the setting takes effect on the output pad, the pin must be configured properly. If not, it will take effect whenever the pin has been properly configured.


GPIO_PortInGet#

uint32_t GPIO_PortInGet (GPIO_Port_TypeDef port)

Read the pad values for GPIO port.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

Returns

  • The pad values for the GPIO port.


GPIO_PortOutClear#

void GPIO_PortOutClear (GPIO_Port_TypeDef port, uint32_t pins)

Set bits in DOUT register for a port to 0.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

uint32_t[in]pins

Bit mask for bits to clear in DOUT register.

Note

  • To ensure that the setting takes effect on the output pad, the pin must be configured properly. If not, it will take effect whenever the pin has been properly configured.


GPIO_PortOutGet#

uint32_t GPIO_PortOutGet (GPIO_Port_TypeDef port)

Get the current setting for a GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

Returns

  • The data out setting for the requested port.


GPIO_PortOutSet#

void GPIO_PortOutSet (GPIO_Port_TypeDef port, uint32_t pins)

Set bits GPIO data out register to 1.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

uint32_t[in]pins

Bit mask for bits to set to 1 in DOUT register.

Note

  • To ensure that the setting takes effect on the respective output pads, the pins must be configured properly. If not, it will take effect whenever the pin has been properly configured.


GPIO_PortOutSetVal#

void GPIO_PortOutSetVal (GPIO_Port_TypeDef port, uint32_t val, uint32_t mask)

Set GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

uint32_t[in]val

Value to write to port data out register.

uint32_t[in]mask

Mask indicating which bits to modify.

Note

  • To ensure that the setting takes effect on the respective output pads, the pins must be configured properly. If not, it will take effect whenever the pin has been properly configured.


GPIO_PortOutToggle#

void GPIO_PortOutToggle (GPIO_Port_TypeDef port, uint32_t pins)

Toggle pins in GPIO port data out register.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to access.

uint32_t[in]pins

Bit mask with pins to toggle.

Note

  • To ensure that the setting takes effect on the output pad, the pin must be configured properly. If not, it will take effect whenever the pin has been properly configured.


GPIO_SlewrateSet#

void GPIO_SlewrateSet (GPIO_Port_TypeDef port, uint32_t slewrate, uint32_t slewrateAlt)

Set slewrate for pins on a GPIO port.

Parameters
TypeDirectionArgument NameDescription
GPIO_Port_TypeDef[in]port

The GPIO port to configure.

uint32_t[in]slewrate

The slewrate to configure for pins on this GPIO port.

uint32_t[in]slewrateAlt

The slewrate to configure for pins using alternate modes on this GPIO port.


GPIO_Unlock#

void GPIO_Unlock (void )

Unlock the GPIO configuration.

Parameters
TypeDirectionArgument NameDescription
voidN/A