ACMP initialization structure.

Public Attributes#

uint32_t

Bias current.

ACMP accuracy mode.

bool

Inactive value emitted by ACMP during warmup.

uint32_t

VDD division factor.

bool

If true, ACMP is enabled after configuration.

Public Attribute Documentation#

biasProg#

uint32_t ACMP_Init_TypeDef::biasProg

Bias current.

See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.


inputRange#

ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange

Input range.

Adjust this setting to optimize the performance for a given input voltage range.


accuracy#

ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy

ACMP accuracy mode.

Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.


hysteresisLevel#

ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel

Hysteresis level.


inactiveValue#

bool ACMP_Init_TypeDef::inactiveValue

Inactive value emitted by ACMP during warmup.


vrefDiv#

uint32_t ACMP_Init_TypeDef::vrefDiv

VDD division factor.

VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.


enable#

bool ACMP_Init_TypeDef::enable

If true, ACMP is enabled after configuration.