Ash#

See ash-protocol.h for source code.

Use the Asynchronous Serial Host (ASH) Framework interfaces on a host microcontroller when it communicates with an Ember chip via EZSP-UART.

See ash-common.h for source code.

Variables#

bool

set false to start decoding a new frame

uint16_t

rec'd ack timer (msecs)

uint16_t

rec'd ack timer period (msecs)

uint8_t

not ready timer (16 msec units)

Functions#

uint8_t
ashEncodeByte(uint8_t len, uint8_t byte, uint8_t *offset)

Builds an ASH frame.

EzspStatus
ashDecodeByte(uint8_t byte, uint8_t *out, uint8_t *outLen)

Decodes and validates an ASH frame.

uint8_t
ashRandomizeArray(uint8_t seed, uint8_t *buf, uint8_t len)

Randomizes array contents by XORing with an 8-bit pseudo random sequence.

void

Sets ashAckTimer to the specified period and starts it running.

bool

Indicates whether or not ashAckTimer has expired.

void
ashAdjustAckPeriod(bool expired)

Adapts the acknowledgement timer period to the observed ACK delay.

void

Starts the Not Ready timer.

bool

Tests whether the Not Ready timer has expired or has stopped.

Macros#

#define

Stops and clears ashAckTimer.

#define

protocol version

#define

frame delimiter

#define
ASH_ESC 0x7D

byte stuffing escape byte

#define
ASH_XON 0x11

flow control byte - means resume transmission

#define

flow control byte - means suspend transmission

#define
ASH_SUB 0x18

replaces bytes w framing, overrun or overflow errors

#define
ASH_CAN 0x1A

frame cancel byte

#define

wake signal byte (also means NCP data pending)

#define

XOR mask used in byte stuffing.

#define
ASH_MIN_DATA_FIELD_LEN EZSP_MIN_FRAME_LENGTH

ash min data field len

#define
ASH_MAX_DATA_FIELD_LEN EZSP_MAX_FRAME_LENGTH

ash max data field len

#define
ASH_MIN_DATA_FRAME_LEN (ASH_MIN_DATA_FIELD_LEN + 1)

with control

#define

control plus data field, but not CRC

#define
ASH_MAX_FRAME_LEN (ASH_MAX_DATA_FIELD_LEN + 1)

ash max frame len

#define

ash crc len

#define
ASH_MIN_FRAME_WITH_CRC_LEN (ASH_MIN_FRAME_LEN + ASH_CRC_LEN)

ash min frame with crc len

#define
ASH_MAX_FRAME_WITH_CRC_LEN (ASH_MAX_FRAME_LEN + ASH_CRC_LEN)

ash max frame with crc len

#define

longest non-data frame received

#define

longest non-data frame sent

#define

longest non-data frame received

#define

longest non-data frame sent

#define

ash dframe mask

#define

ash control data

#define

ash shframe mask

#define

ash control ack

#define

ash control nak

#define

ash control rst

#define

ash control rstack

#define

ash control error

#define

acknowledge frame number

#define

ash acknum bit

#define

retransmitted frame flag

#define

ash rflag bit

#define

receiver not ready flag

#define

ash nflag bit

#define

flag reserved for future use

#define

ash pflag bit

#define

DATA frame number.

#define

ash frmnum bit

#define

ash get rflag(ctl)

#define

ash get nflag(ctl)

#define

ash get frmnum(ctl)

#define

ash get acknum(ctl)

#define
ASH_FRAME_LEN_DATA_MIN (ASH_MIN_DATA_FIELD_LEN + 1)

ash frame len data min

#define
#define
#define
#define

control, version, reset reason

#define

control, version, error

#define
MOD8 (n)

mask to frame number modulus

#define
INC8 (n)

increment in frame number modulus

#define
WITHIN_RANGE (lo, n, hi)

within range lo and hi

#define

Indicates whether or not ashAckTimer is currently running.

#define

Indicates whether or not ashAckTimer is currently running.

#define

Sets the acknowledgement timer period (in msec) and stops the timer.

#define

Returns the acknowledgement timer period (in msec).

#define

Sets the acknowledgement timer period (in msec), and starts the timer running.

#define

log2 of msecs per NR timer unit

#define

Stops the Not Ready timer.

#define

Indicates whether or not ashNrTimer is currently running.

Variable Documentation#

ashDecodeInProgress#

bool ashDecodeInProgress

set false to start decoding a new frame


ashAckTimer#

uint16_t ashAckTimer

rec'd ack timer (msecs)


ashAckPeriod#

uint16_t ashAckPeriod

rec'd ack timer period (msecs)


ashNrTimer#

uint8_t ashNrTimer

not ready timer (16 msec units)


Function Documentation#

ashEncodeByte#

uint8_t ashEncodeByte (uint8_t len, uint8_t byte, uint8_t * offset)

Builds an ASH frame.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Alen

new frame flag / length of the frame to be encoded. A non-zero value begins a new frame, so all subsequent calls must use zero. The length includes control byte and data field, but not the flag or crc. This function does not validate the length.

uint8_tN/Abyte

the next byte of data to add to the frame. Note that in general the same byte of data may have to be passed more than once as escape bytes, the CRC and the end flag byte are output.

uint8_t *N/Aoffset

pointer to the offset of the next input byte. (If the frame data is the array data[], the next byte would be data[offset].) Is set to 0 when starting a new frame (ie, len is non-zero). Is set to 0xFF when the last byte of the frame is returned.

Byte stuffs the control and data fields as required, computes and appends the CRC and adds the ending flag byte. Called with the next byte to encode, this function may return several output bytes before it's ready for the next byte.

Returns

  • next encoded output byte in frame.


ashDecodeByte#

EzspStatus ashDecodeByte (uint8_t byte, uint8_t * out, uint8_t * outLen)

Decodes and validates an ASH frame.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Abyte

the next byte of data to add to the frame

uint8_t *N/Aout

pointer to where to write an output byte

uint8_t *N/AoutLen

number of bytes output so far

Data is passed to it one byte at a time. Decodes byte stuffing, checks crc, finds the end flag and (if enabled) terminates the frame early on CAN or SUB bytes. The number of bytes output will not exceed the max valid frame length, which does not include the flag or the crc.

Returns

  • status of frame decoding

    • ::EZSP_SUCCESS

    • ::EZSP_ASH_IN_PROGRESS

    • ::EZSP_ASH_CANCELLED

    • ::EZSP_ASH_BAD_CRC

    • ::EZSP_ASH_COMM_ERROR

    • ::EZSP_ASH_TOO_SHORT

    • ::EZSP_ASH_TOO_LONG


ashRandomizeArray#

uint8_t ashRandomizeArray (uint8_t seed, uint8_t * buf, uint8_t len)

Randomizes array contents by XORing with an 8-bit pseudo random sequence.

Parameters
TypeDirectionArgument NameDescription
uint8_tN/Aseed

zero initializes the random sequence a non-zero value continues from a previous invocation

uint8_t *N/Abuf

pointer to the array whose contents will be randomized

uint8_tN/Alen

number of bytes in the array to modify

This reduces the likelihood that byte-stuffing will greatly increase the size of the payload. (This could happen if a DATA frame contained repeated instances of the same reserved byte value.)

Returns

  • last value of the sequence. If a buffer is processed in two or more chunks, as with linked buffers, this value should be passed back as the value of the seed argument


ashStartAckTimer#

void ashStartAckTimer (void )

Sets ashAckTimer to the specified period and starts it running.

Parameters
TypeDirectionArgument NameDescription
voidN/A

ashAckTimerHasExpired#

bool ashAckTimerHasExpired (void )

Indicates whether or not ashAckTimer has expired.

Parameters
TypeDirectionArgument NameDescription
voidN/A

If the timer is stopped then it is not expired.

Returns

  • bool


ashAdjustAckPeriod#

void ashAdjustAckPeriod (bool expired)

Adapts the acknowledgement timer period to the observed ACK delay.

Parameters
TypeDirectionArgument NameDescription
boolN/Aexpired

true if timer has expired

If the timer is not running, it does nothing. If the timer has expired, the timeourt period is doubled. If the timer has not expired, the elapsed time is fed into simple IIR filter: T[n+1] = (7*T[n] + elapsedTime) / 8 The timeout period, ashAckPeriod, is limited such that: ASH_xxx_TIME_DATA_MIN <= ashAckPeriod <= ASH_xxx_TIME_DATA_MAX, where xxx is either HOST or NCP.

The acknowledgement timer is always stopped by this function.


ashStartNrTimer#

void ashStartNrTimer (void )

Starts the Not Ready timer.

Parameters
TypeDirectionArgument NameDescription
voidN/A

On the host, this times nFlag refreshing when the host doesn't have room for callbacks for a prolonged period.

On the NCP, if this times out the NCP resumes sending callbacks.


ashNrTimerHasExpired#

bool ashNrTimerHasExpired (void )

Tests whether the Not Ready timer has expired or has stopped.

Parameters
TypeDirectionArgument NameDescription
voidN/A

If expired, it is stopped.

Returns

  • true if the Not Ready timer has expired or stopped


Macro Definition Documentation#

ashStopAckTimer#

#define ashStopAckTimer
Value:
(void)

Stops and clears ashAckTimer.


ASH_VERSION#

#define ASH_VERSION
Value:
2

protocol version


ASH_FLAG#

#define ASH_FLAG
Value:
0x7E

frame delimiter


ASH_ESC#

#define ASH_ESC
Value:
0x7D

byte stuffing escape byte


ASH_XON#

#define ASH_XON
Value:
0x11

flow control byte - means resume transmission


ASH_XOFF#

#define ASH_XOFF
Value:
0x13

flow control byte - means suspend transmission


ASH_SUB#

#define ASH_SUB
Value:
0x18

replaces bytes w framing, overrun or overflow errors


ASH_CAN#

#define ASH_CAN
Value:
0x1A

frame cancel byte


ASH_WAKE#

#define ASH_WAKE
Value:
0xFF

wake signal byte (also means NCP data pending)


ASH_FLIP#

#define ASH_FLIP
Value:
0x20

XOR mask used in byte stuffing.


ASH_MIN_DATA_FIELD_LEN#

#define ASH_MIN_DATA_FIELD_LEN
Value:
EZSP_MIN_FRAME_LENGTH

ash min data field len


ASH_MAX_DATA_FIELD_LEN#

#define ASH_MAX_DATA_FIELD_LEN
Value:
EZSP_MAX_FRAME_LENGTH

ash max data field len


ASH_MIN_DATA_FRAME_LEN#

#define ASH_MIN_DATA_FRAME_LEN
Value:
(ASH_MIN_DATA_FIELD_LEN + 1)

with control


ASH_MIN_FRAME_LEN#

#define ASH_MIN_FRAME_LEN
Value:
1

control plus data field, but not CRC


ASH_MAX_FRAME_LEN#

#define ASH_MAX_FRAME_LEN
Value:
(ASH_MAX_DATA_FIELD_LEN + 1)

ash max frame len


ASH_CRC_LEN#

#define ASH_CRC_LEN
Value:
2

ash crc len


ASH_MIN_FRAME_WITH_CRC_LEN#

#define ASH_MIN_FRAME_WITH_CRC_LEN
Value:
(ASH_MIN_FRAME_LEN + ASH_CRC_LEN)

ash min frame with crc len


ASH_MAX_FRAME_WITH_CRC_LEN#

#define ASH_MAX_FRAME_WITH_CRC_LEN
Value:
(ASH_MAX_FRAME_LEN + ASH_CRC_LEN)

ash max frame with crc len


ASH_NCP_SHFRAME_RX_LEN#

#define ASH_NCP_SHFRAME_RX_LEN
Value:
2

longest non-data frame received


ASH_NCP_SHFRAME_TX_LEN#

#define ASH_NCP_SHFRAME_TX_LEN
Value:
3

longest non-data frame sent


ASH_HOST_SHFRAME_RX_LEN#

#define ASH_HOST_SHFRAME_RX_LEN
Value:
3

longest non-data frame received


ASH_HOST_SHFRAME_TX_LEN#

#define ASH_HOST_SHFRAME_TX_LEN
Value:
2

longest non-data frame sent


ASH_DFRAME_MASK#

#define ASH_DFRAME_MASK
Value:
0x80

ash dframe mask


ASH_CONTROL_DATA#

#define ASH_CONTROL_DATA
Value:
0x00

ash control data


ASH_SHFRAME_MASK#

#define ASH_SHFRAME_MASK
Value:
0xE0

ash shframe mask


ASH_CONTROL_ACK#

#define ASH_CONTROL_ACK
Value:
0x80

ash control ack


ASH_CONTROL_NAK#

#define ASH_CONTROL_NAK
Value:
0xA0

ash control nak


ASH_CONTROL_RST#

#define ASH_CONTROL_RST
Value:
0xC0

ash control rst


ASH_CONTROL_RSTACK#

#define ASH_CONTROL_RSTACK
Value:
0xC1

ash control rstack


ASH_CONTROL_ERROR#

#define ASH_CONTROL_ERROR
Value:
0xC2

ash control error


ASH_ACKNUM_MASK#

#define ASH_ACKNUM_MASK
Value:
0x07

acknowledge frame number


ASH_ACKNUM_BIT#

#define ASH_ACKNUM_BIT
Value:
0

ash acknum bit


ASH_RFLAG_MASK#

#define ASH_RFLAG_MASK
Value:
0x08

retransmitted frame flag


ASH_RFLAG_BIT#

#define ASH_RFLAG_BIT
Value:
3

ash rflag bit


ASH_NFLAG_MASK#

#define ASH_NFLAG_MASK
Value:
0x08

receiver not ready flag


ASH_NFLAG_BIT#

#define ASH_NFLAG_BIT
Value:
3

ash nflag bit


ASH_PFLAG_MASK#

#define ASH_PFLAG_MASK
Value:
0x10

flag reserved for future use


ASH_PFLAG_BIT#

#define ASH_PFLAG_BIT
Value:
4

ash pflag bit


ASH_FRMNUM_MASK#

#define ASH_FRMNUM_MASK
Value:
0x70

DATA frame number.


ASH_FRMNUM_BIT#

#define ASH_FRMNUM_BIT
Value:
4

ash frmnum bit


ASH_GET_RFLAG#

#define ASH_GET_RFLAG
Value:
(ctl)

ash get rflag(ctl)


ASH_GET_NFLAG#

#define ASH_GET_NFLAG
Value:
(ctl)

ash get nflag(ctl)


ASH_GET_FRMNUM#

#define ASH_GET_FRMNUM
Value:
(ctl)

ash get frmnum(ctl)


ASH_GET_ACKNUM#

#define ASH_GET_ACKNUM
Value:
(ctl)

ash get acknum(ctl)


ASH_FRAME_LEN_DATA_MIN#

#define ASH_FRAME_LEN_DATA_MIN
Value:
(ASH_MIN_DATA_FIELD_LEN + 1)

ash frame len data min


ASH_FRAME_LEN_ACK#

#define ASH_FRAME_LEN_ACK
Value:
1

control


ASH_FRAME_LEN_NAK#

#define ASH_FRAME_LEN_NAK
Value:
1

control


ASH_FRAME_LEN_RST#

#define ASH_FRAME_LEN_RST
Value:
1

control


ASH_FRAME_LEN_RSTACK#

#define ASH_FRAME_LEN_RSTACK
Value:
3

control, version, reset reason


ASH_FRAME_LEN_ERROR#

#define ASH_FRAME_LEN_ERROR
Value:
3

control, version, error


MOD8#

#define MOD8
Value:
(n)

mask to frame number modulus


INC8#

#define INC8
Value:
(n)

increment in frame number modulus


WITHIN_RANGE#

#define WITHIN_RANGE
Value:
(lo, n, hi)

within range lo and hi


ashAckTimerIsRunning#

#define ashAckTimerIsRunning
Value:
()

Indicates whether or not ashAckTimer is currently running.

The timer may be running even if expired.


ashAckTimerIsNotRunning#

#define ashAckTimerIsNotRunning
Value:
()

Indicates whether or not ashAckTimer is currently running.

The timer may be running even if expired.


ashSetAckPeriod#

#define ashSetAckPeriod
Value:
(msec)

Sets the acknowledgement timer period (in msec) and stops the timer.


ashGetAckPeriod#

#define ashGetAckPeriod
Value:
()

Returns the acknowledgement timer period (in msec).


ashSetAndStartAckTimer#

#define ashSetAndStartAckTimer
Value:
(msec)

Sets the acknowledgement timer period (in msec), and starts the timer running.


ASH_NR_TIMER_BIT#

#define ASH_NR_TIMER_BIT
Value:
4

log2 of msecs per NR timer unit


ashStopNrTimer#

#define ashStopNrTimer
Value:
()

Stops the Not Ready timer.


ashNrTimerIsNotRunning#

#define ashNrTimerIsNotRunning
Value:
()

Indicates whether or not ashNrTimer is currently running.