Single conversion initialization structure.

Public Attributes#

Peripheral reflex system trigger selection.

Acquisition time (in ADC clock cycles).

Sample reference selection.

Sample resolution.

Select positive input for single channel conversion mode.

Select negative input for single channel conversion mode.

bool

Select if single-ended or differential input.

bool

Peripheral reflex system trigger enable.

bool

Select if left adjustment should be done.

bool

Select if continuous conversion until explicit stop.

bool

When true, DMA is available in EM2 for single conversion.

bool

When true, FIFO overwrites old data when full.

Public Attribute Documentation#

prsSel#

ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel

Peripheral reflex system trigger selection.

Only applicable if prsEnable is enabled.


acqTime#

ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime

Acquisition time (in ADC clock cycles).


reference#

ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference

Sample reference selection.

Note that, for external references, the ADC calibration register must be set explicitly.


resolution#

ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution

Sample resolution.


posSel#

ADC_PosSel_TypeDef ADC_InitSingle_TypeDef::posSel

Select positive input for single channel conversion mode.


negSel#

ADC_NegSel_TypeDef ADC_InitSingle_TypeDef::negSel

Select negative input for single channel conversion mode.

Negative input is grounded for single-ended (non-differential) conversion.


diff#

bool ADC_InitSingle_TypeDef::diff

Select if single-ended or differential input.


prsEnable#

bool ADC_InitSingle_TypeDef::prsEnable

Peripheral reflex system trigger enable.


leftAdjust#

bool ADC_InitSingle_TypeDef::leftAdjust

Select if left adjustment should be done.


rep#

bool ADC_InitSingle_TypeDef::rep

Select if continuous conversion until explicit stop.


singleDmaEm2Wu#

bool ADC_InitSingle_TypeDef::singleDmaEm2Wu

When true, DMA is available in EM2 for single conversion.


fifoOverwrite#

bool ADC_InitSingle_TypeDef::fifoOverwrite

When true, FIFO overwrites old data when full.

If false, FIFO discards new data. The SCANOF IRQ is triggered in both cases.