TIMER compare/capture initialization structure.

Public Attributes#

Input capture event control.

Input capture edge select.

Peripheral reflex system trigger selection.

Counter underflow output action.

Counter overflow output action.

Counter match output action.

Compare/capture channel mode.

bool

Enable digital filter.

bool

Select TIMERnCCx (false) or PRS input (true).

bool

Compare output initial state.

bool

Invert output from compare/capture channel.

PRS output configuration.

Public Attribute Documentation#

eventCtrl#

TIMER_Event_TypeDef TIMER_InitCC_TypeDef::eventCtrl

Input capture event control.


edge#

TIMER_Edge_TypeDef TIMER_InitCC_TypeDef::edge

Input capture edge select.


prsSel#

TIMER_PRSSEL_TypeDef TIMER_InitCC_TypeDef::prsSel

Peripheral reflex system trigger selection.

Only applicable if prsInput is enabled.


cufoa#

TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cufoa

Counter underflow output action.


cofoa#

TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cofoa

Counter overflow output action.


cmoa#

TIMER_OutputAction_TypeDef TIMER_InitCC_TypeDef::cmoa

Counter match output action.


mode#

TIMER_CCMode_TypeDef TIMER_InitCC_TypeDef::mode

Compare/capture channel mode.


filter#

bool TIMER_InitCC_TypeDef::filter

Enable digital filter.


prsInput#

bool TIMER_InitCC_TypeDef::prsInput

Select TIMERnCCx (false) or PRS input (true).


coist#

bool TIMER_InitCC_TypeDef::coist

Compare output initial state.

Only used in Output Compare and PWM mode. When true, the compare/PWM output is set high when the counter is disabled. When counting resumes, this value will represent the initial value for the compare/PWM output. If the bit is cleared, the output will be cleared when the counter is disabled.


outInvert#

bool TIMER_InitCC_TypeDef::outInvert

Invert output from compare/capture channel.


prsOutput#

TIMER_PrsOutput_t TIMER_InitCC_TypeDef::prsOutput

PRS output configuration.

PRS output from a timer can either be a pulse output or a level output that follows the CC out value.