Watchdog initialization structure.

Public Attributes#

bool

Enable Watchdog when initialization completed.

bool

Counter keeps running during debug halt.

bool

Select WDOG clear source: False: Write to the clear bit will clear the WDOG counter True: Rising edge on the PRS Source 0 will clear the WDOG counter.

bool

Counter keeps running when in EM2.

bool

Counter keeps running when in EM3.

bool

Block EMU from entering EM4.

bool

Block SW from disabling LFRCO/LFXO oscillators.

bool

Block SW from modifying the configuration (a reset is needed to reconfigure).

Clock source to use for Watchdog.

Watchdog timeout period.

Select warning time as % of the Watchdog timeout.

Select illegal window time as % of the Watchdog timeout.

bool

Disable Watchdog reset output if true.

Public Attribute Documentation#

enable#

bool WDOG_Init_TypeDef::enable

Enable Watchdog when initialization completed.


debugRun#

bool WDOG_Init_TypeDef::debugRun

Counter keeps running during debug halt.


clrSrc#

bool WDOG_Init_TypeDef::clrSrc

Select WDOG clear source: False: Write to the clear bit will clear the WDOG counter True: Rising edge on the PRS Source 0 will clear the WDOG counter.


em2Run#

bool WDOG_Init_TypeDef::em2Run

Counter keeps running when in EM2.


em3Run#

bool WDOG_Init_TypeDef::em3Run

Counter keeps running when in EM3.


em4Block#

bool WDOG_Init_TypeDef::em4Block

Block EMU from entering EM4.


swoscBlock#

bool WDOG_Init_TypeDef::swoscBlock

Block SW from disabling LFRCO/LFXO oscillators.


lock#

bool WDOG_Init_TypeDef::lock

Block SW from modifying the configuration (a reset is needed to reconfigure).


clkSel#

WDOG_ClkSel_TypeDef WDOG_Init_TypeDef::clkSel

Clock source to use for Watchdog.


perSel#

WDOG_PeriodSel_TypeDef WDOG_Init_TypeDef::perSel

Watchdog timeout period.


warnSel#

WDOG_WarnSel_TypeDef WDOG_Init_TypeDef::warnSel

Select warning time as % of the Watchdog timeout.


winSel#

WDOG_WinSel_TypeDef WDOG_Init_TypeDef::winSel

Select illegal window time as % of the Watchdog timeout.


resetDisable#

bool WDOG_Init_TypeDef::resetDisable

Disable Watchdog reset output if true.