LETIMER initialization structure.

Public Attributes#

bool

Start counting when initialization completes.

bool

Counter shall keep running during debug halt.

bool

Load COMP0 register into CNT when counter underflows.

bool

Load COMP1 into COMP0 when REP0 reaches 0.

uint8_t

Idle value for output 0.

uint8_t

Idle value for output 1.

Underflow output 0 action.

Underflow output 1 action.

uint32_t

Top value.

Public Attribute Documentation#

enable#

bool LETIMER_Init_TypeDef::enable

Start counting when initialization completes.


Definition at line 87 of file platform/emlib/inc/em_letimer.h

debugRun#

bool LETIMER_Init_TypeDef::debugRun

Counter shall keep running during debug halt.


Definition at line 88 of file platform/emlib/inc/em_letimer.h

comp0Top#

bool LETIMER_Init_TypeDef::comp0Top

Load COMP0 register into CNT when counter underflows.


Definition at line 93 of file platform/emlib/inc/em_letimer.h

bufTop#

bool LETIMER_Init_TypeDef::bufTop

Load COMP1 into COMP0 when REP0 reaches 0.


Definition at line 94 of file platform/emlib/inc/em_letimer.h

out0Pol#

uint8_t LETIMER_Init_TypeDef::out0Pol

Idle value for output 0.


Definition at line 95 of file platform/emlib/inc/em_letimer.h

out1Pol#

uint8_t LETIMER_Init_TypeDef::out1Pol

Idle value for output 1.


Definition at line 96 of file platform/emlib/inc/em_letimer.h

ufoa0#

LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa0

Underflow output 0 action.


Definition at line 97 of file platform/emlib/inc/em_letimer.h

ufoa1#

LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa1

Underflow output 1 action.


Definition at line 98 of file platform/emlib/inc/em_letimer.h

repMode#

LETIMER_RepeatMode_TypeDef LETIMER_Init_TypeDef::repMode

Repeat mode.


Definition at line 99 of file platform/emlib/inc/em_letimer.h

topValue#

uint32_t LETIMER_Init_TypeDef::topValue

Top value.

Counter wraps when top value matches counter value is reached.


Definition at line 100 of file platform/emlib/inc/em_letimer.h