RTC - Real Time Counter#

Real Time Counter (RTC) Peripheral API.

This module contains functions to control the RTC peripheral of Silicon Labs 32-bit MCUs and SoCs. The RTC ensures timekeeping in low energy modes.

Modules#

RTC_Init_TypeDef

Functions#

uint32_t
RTC_CompareGet(unsigned int comp)

Get the RTC compare register value.

void
RTC_CompareSet(unsigned int comp, uint32_t value)

Set the RTC compare register value.

void
RTC_Enable(bool enable)

Enable/disable RTC.

void
RTC_FreezeEnable(bool enable)

RTC register synchronization freeze control.

void
RTC_Init(const RTC_Init_TypeDef *init)

Initialize RTC.

void
RTC_Reset(void)

Restore RTC to reset state.

void

Restart the RTC counter from zero.

uint32_t

Get RTC counter value.

void
RTC_CounterSet(uint32_t value)

Set the RTC counter value.

void
RTC_IntClear(uint32_t flags)

Clear one or more pending RTC interrupts.

void
RTC_IntDisable(uint32_t flags)

Disable one or more RTC interrupts.

void
RTC_IntEnable(uint32_t flags)

Enable one or more RTC interrupts.

uint32_t

Get pending RTC interrupt flags.

uint32_t

Get enabled and pending RTC interrupt flags.

void
RTC_IntSet(uint32_t flags)

Set one or more pending RTC interrupts from SW.

Macros#

#define
NUM_RTC_CHANNELS 2U

The RTC peripheral on series 0 devices support 2 compare channels while the RTC peripheral on series 1 devices support 6 compare channels.

#define
RTC_INIT_DEFAULT undefined

Suggested default configuration for RTC initialization structure.

Function Documentation#

RTC_CompareGet#

uint32_t RTC_CompareGet (unsigned int comp)

Get the RTC compare register value.

Parameters
TypeDirectionArgument NameDescription
unsigned int[in]comp

A compare register to get. This value must be less than NUM_RTC_CHANNELS.

Returns

  • A compare register value, 0 if invalid register selected.


RTC_CompareSet#

void RTC_CompareSet (unsigned int comp, uint32_t value)

Set the RTC compare register value.

Parameters
TypeDirectionArgument NameDescription
unsigned int[in]comp

A compare register to set. This value must be less than NUM_RTC_CHANNELS.

uint32_t[in]value

An initialization value (<= 0x00ffffff).

Note

  • The setting of a compare register requires synchronization into the low-frequency domain. If the same register is modified before a previous update has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.


RTC_Enable#

void RTC_Enable (bool enable)

Enable/disable RTC.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable

True to enable counting, false to disable.

Note

  • The enabling/disabling of RTC modifies the RTC CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.


RTC_FreezeEnable#

void RTC_FreezeEnable (bool enable)

RTC register synchronization freeze control.

Parameters
TypeDirectionArgument NameDescription
bool[in]enable
  • True - enable freeze, modified registers are not propagated to the LF domain

  • False - disables freeze, modified registers are propagated to LF domain

Some RTC registers require synchronization into the low-frequency (LF) domain. The freeze feature allows for several registers to be modified before passing them to the LF domain simultaneously (which takes place when the freeze mode is disabled).

Note

  • When enabling freeze mode, this function will wait for all current ongoing RTC synchronization to LF domain to complete (normally synchronization will not be in progress.) However, for this reason, when using freeze mode, modifications of registers requiring LF synchronization should be done within one freeze enable/disable block to avoid unnecessary stalling. This only applies to the Gecko Family. See the reference manual chapter about Access to Low Energy Peripherals (Asynchronos Registers) for details.


RTC_Init#

void RTC_Init (const RTC_Init_TypeDef * init)

Initialize RTC.

Parameters
TypeDirectionArgument NameDescription
const RTC_Init_TypeDef *[in]init

A pointer to the RTC initialization structure.

Note that the compare values must be set separately with RTC_CompareSet() prior to the use of this function if configuring the RTC to start when initialization is completed.

Note

  • The initialization of the RTC modifies the RTC CTRL register which requires synchronization into the low-frequency domain. If this register is modified before a previous update to the same register has completed, this function will stall until the previous synchronization has completed. This only applies to the Gecko Family. See comments in the regSync() internal function call.


RTC_Reset#

void RTC_Reset (void )

Restore RTC to reset state.

Parameters
TypeDirectionArgument NameDescription
voidN/A

RTC_CounterReset#

void RTC_CounterReset (void )

Restart the RTC counter from zero.

Parameters
TypeDirectionArgument NameDescription
voidN/A

RTC_CounterGet#

uint32_t RTC_CounterGet (void )

Get RTC counter value.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • Current RTC counter value.


RTC_CounterSet#

void RTC_CounterSet (uint32_t value)

Set the RTC counter value.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]value

The new RTC counter value.


RTC_IntClear#

void RTC_IntClear (uint32_t flags)

Clear one or more pending RTC interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

RTC interrupt sources to clear. Use a set of interrupt flags OR-ed together to clear multiple interrupt sources for the RTC module (RTC_IFS_nnn).


RTC_IntDisable#

void RTC_IntDisable (uint32_t flags)

Disable one or more RTC interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

RTC interrupt sources to disable. Use a set of interrupt flags OR-ed together to disable multiple interrupt sources for the RTC module (RTC_IFS_nnn).


RTC_IntEnable#

void RTC_IntEnable (uint32_t flags)

Enable one or more RTC interrupts.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

RTC interrupt sources to enable. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the RTC module (RTC_IFS_nnn).

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using RTC_IntClear() prior to enabling the interrupt.


RTC_IntGet#

uint32_t RTC_IntGet (void )

Get pending RTC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Note

  • Event bits are not cleared by using this function.

Returns

  • Pending RTC interrupt sources. Returns a set of interrupt flags OR-ed together for multiple interrupt sources in the RTC module (RTC_IFS_nnn).


RTC_IntGetEnabled#

uint32_t RTC_IntGetEnabled (void )

Get enabled and pending RTC interrupt flags.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by using this function.

Returns

  • Pending and enabled RTC interrupt sources. The return value is the bitwise AND of

    • the enabled interrupt sources in RTC_IEN and

    • the pending interrupt flags RTC_IF.


RTC_IntSet#

void RTC_IntSet (uint32_t flags)

Set one or more pending RTC interrupts from SW.

Parameters
TypeDirectionArgument NameDescription
uint32_t[in]flags

RTC interrupt sources to set to pending. Use a set of interrupt flags OR-ed together to set multiple interrupt sources for the RTC module (RTC_IFS_nnn).