Board Control#

Functions to control Silicon Labs board features.

Enumerations#

enum
SL_BOARD_SENSOR_RHT = (1UL << 0UL)
SL_BOARD_SENSOR_LIGHT = (1UL << 1UL)
SL_BOARD_SENSOR_PRESSURE = (1UL << 2UL)
SL_BOARD_SENSOR_HALL = (1UL << 3UL)
SL_BOARD_SENSOR_GAS = (1UL << 4UL)
SL_BOARD_SENSOR_IMU = (1UL << 5UL)
SL_BOARD_SENSOR_MICROPHONE = (1UL << 6UL)
}

Board Sensor Type.

enum
SL_BOARD_MEMORY_SDCARD = (1UL << 0UL)
SL_BOARD_MEMORY_QSPI = (1UL << 1UL)
}

Board Memory Type.

enum
SL_BOARD_OSCILLATOR_TCXO = (1UL << 0UL)
}

Board Oscillator Type.

Functions#

sl_status_t

Configure Virtual COM UART.

sl_status_t

Enable Virtual COM UART.

sl_status_t

Disable Virtual COM UART.

sl_status_t
sl_board_enable_sensor(sl_board_sensor_t sensor)

Enable a sensor.

sl_status_t
sl_board_disable_sensor(sl_board_sensor_t sensor)

Disable a sensor.

sl_status_t

Enable display.

sl_status_t

Disable display.

sl_status_t
sl_board_enable_memory(sl_board_memory_t memory)

Enable memory.

sl_status_t
sl_board_disable_memory(sl_board_memory_t memory)

Disable memory.

sl_status_t
sl_board_enable_oscillator(sl_board_oscillator_t oscillator)

Enable an oscillator.

sl_status_t
sl_board_disable_oscillator(sl_board_oscillator_t oscillator)

Disable a oscillator.

Enumeration Documentation#

sl_board_sensor_t#

sl_board_sensor_t

Board Sensor Type.

Enumerator
SL_BOARD_SENSOR_RHT

Relative Humidity and Temperature Sensor.

SL_BOARD_SENSOR_LIGHT

UV Index and Ambient Light Sensor.

SL_BOARD_SENSOR_PRESSURE

Barometric Pressure Sensor.

SL_BOARD_SENSOR_HALL

Hall Effect Sensor.

SL_BOARD_SENSOR_GAS

Gas Sensor.

SL_BOARD_SENSOR_IMU

Inertial Measurement Unit (Accelerometer/Gyroscope)

SL_BOARD_SENSOR_MICROPHONE

Microphone.


Definition at line 47 of file hardware/board/inc/sl_board_control.h

sl_board_memory_t#

sl_board_memory_t

Board Memory Type.

Enumerator
SL_BOARD_MEMORY_SDCARD

SD Card.

SL_BOARD_MEMORY_QSPI

Quad SPI Flash.


Definition at line 58 of file hardware/board/inc/sl_board_control.h

sl_board_oscillator_t#

sl_board_oscillator_t

Board Oscillator Type.

Enumerator
SL_BOARD_OSCILLATOR_TCXO

TCXO.


Definition at line 64 of file hardware/board/inc/sl_board_control.h

Function Documentation#

sl_board_configure_vcom#

sl_status_t sl_board_configure_vcom (void)

Configure Virtual COM UART.

Parameters
N/A

Returns

  • Status code


Definition at line 77 of file hardware/board/inc/sl_board_control.h

sl_board_enable_vcom#

sl_status_t sl_board_enable_vcom (void)

Enable Virtual COM UART.

Parameters
N/A

Returns

  • Status code


Definition at line 87 of file hardware/board/inc/sl_board_control.h

sl_board_disable_vcom#

sl_status_t sl_board_disable_vcom (void)

Disable Virtual COM UART.

Parameters
N/A

Returns

  • Status code


Definition at line 97 of file hardware/board/inc/sl_board_control.h

sl_board_enable_sensor#

sl_status_t sl_board_enable_sensor (sl_board_sensor_t sensor)

Enable a sensor.

Parameters
[in]sensor

Sensor to enable

Warnings

  • On boards 4166A, 4184A, and 4184B sensors

    • Pressure Sensor, RH/Temp Sensor, and UV/Ambient Light Sensor;

    • UV/Ambient Light Sensor, Hall-effect Sensor, and RH/Temp Sensor;

    • Ambient Light Sensor, Hall-effect Sensor, and RH/Temp Sensor respectively, are tied to the same enable pin. Calling the enable function for only one of these sensors has the side-effect of enabling all three; and calling the disable function for only one of them has the side-effect of disabling all three. The latter scenario seems less than desirable.

Returns

  • Status code


Definition at line 120 of file hardware/board/inc/sl_board_control.h

sl_board_disable_sensor#

sl_status_t sl_board_disable_sensor (sl_board_sensor_t sensor)

Disable a sensor.

Parameters
[in]sensor

Sensors to disable

Warnings

  • On boards 4166A, 4184A, and 4184B sensors

    • Pressure Sensor, RH/Temp Sensor, and UV/Ambient Light Sensor;

    • UV/Ambient Light Sensor, Hall-effect Sensor, and RH/Temp Sensor;

    • Ambient Light Sensor, Hall-effect Sensor, and RH/Temp Sensor respectively, are tied to the same enable pin. Calling the enable function for only one of these sensors has the side-effect of enabling all three; and calling the disable function for only one of them has the side-effect of disabling all three. The latter scenario seems less than desirable.

Returns

  • Status code


Definition at line 143 of file hardware/board/inc/sl_board_control.h

sl_board_enable_display#

sl_status_t sl_board_enable_display (void)

Enable display.

Parameters
N/A

Returns

  • Status code


Definition at line 153 of file hardware/board/inc/sl_board_control.h

sl_board_disable_display#

sl_status_t sl_board_disable_display (void)

Disable display.

Parameters
N/A

Returns

  • Status code


Definition at line 163 of file hardware/board/inc/sl_board_control.h

sl_board_enable_memory#

sl_status_t sl_board_enable_memory (sl_board_memory_t memory)

Enable memory.

Parameters
[in]memory

Memory to enable

Returns

  • Status code


Definition at line 175 of file hardware/board/inc/sl_board_control.h

sl_board_disable_memory#

sl_status_t sl_board_disable_memory (sl_board_memory_t memory)

Disable memory.

Parameters
[in]memory

Memory to disable

Returns

  • Status code


Definition at line 187 of file hardware/board/inc/sl_board_control.h

sl_board_enable_oscillator#

sl_status_t sl_board_enable_oscillator (sl_board_oscillator_t oscillator)

Enable an oscillator.

Parameters
[in]oscillator

Oscillator to enable

Returns

  • Status code


Definition at line 199 of file hardware/board/inc/sl_board_control.h

sl_board_disable_oscillator#

sl_status_t sl_board_disable_oscillator (sl_board_oscillator_t oscillator)

Disable a oscillator.

Parameters
[in]oscillator

Oscillator to disable

Returns

  • Status code


Definition at line 211 of file hardware/board/inc/sl_board_control.h