Status Flags#
*brief Status Flags
These constant values are returned by USBX_blockRead() and USBX_blockWrite().
Macros#
#define
USBX_STATUS_OK USB_STATUS_OK
Success.
#define
USBX_STATUS_EP_BUSY USB_STATUS_EP_BUSY
Failed because the endpoint is busy.
#define
USBX_STATUS_ILLEGAL USB_STATUS_ILLEGAL
Failed due to an illegal parameter.
#define
USBX_STATUS_EP_STALLED USB_STATUS_EP_STALLED
Failed because the endpoint is stalled.
#define
USBX_STATUS_DEVICE_UNCONFIGURED USB_STATUS_DEVICE_UNCONFIGURED
Failed because the device is not configured.
Macro Definition Documentation#
USBX_STATUS_EP_BUSY#
#define USBX_STATUS_EP_BUSYValue:
USB_STATUS_EP_BUSY
Failed because the endpoint is busy.
USBX_STATUS_ILLEGAL#
#define USBX_STATUS_ILLEGALValue:
USB_STATUS_ILLEGAL
Failed due to an illegal parameter.
USBX_STATUS_EP_STALLED#
#define USBX_STATUS_EP_STALLEDValue:
USB_STATUS_EP_STALLED
Failed because the endpoint is stalled.
USBX_STATUS_DEVICE_UNCONFIGURED#
#define USBX_STATUS_DEVICE_UNCONFIGUREDValue:
USB_STATUS_DEVICE_UNCONFIGURED
Failed because the device is not configured.