Struct representing an instance of the CLI storage RAM.

Public Attributes#

The CLI instance associated with this instance.

char *

The command prompt.

char *

The string that define the end of definition.

size_t

The number of command lines that can be stored in RAM.

size_t

The next free line in RAM.

char *

Pointer to the RAM buffer.

bool

True if the command shell execute when defined.

bool

True when definition is in progress.

bool

True when execute is in progress.

Public Attribute Documentation#

cli_handle#

sl_cli_handle_t cli_storage_ram_t::cli_handle

The CLI instance associated with this instance.


prompt#

char* cli_storage_ram_t::prompt

The command prompt.


end_string#

char* cli_storage_ram_t::end_string

The string that define the end of definition.


ram_size#

size_t cli_storage_ram_t::ram_size

The number of command lines that can be stored in RAM.


ram_next#

size_t cli_storage_ram_t::ram_next

The next free line in RAM.


ram_buffer#

char* cli_storage_ram_t::ram_buffer

Pointer to the RAM buffer.


execute_while_define#

bool cli_storage_ram_t::execute_while_define

True if the command shell execute when defined.


define_in_progress#

bool cli_storage_ram_t::define_in_progress

True when definition is in progress.


execute_in_progress#

bool cli_storage_ram_t::execute_in_progress

True when execute is in progress.