LFRCO Initialization#

Initialize the LFRCO oscillator.

Initialize the low frequency RC oscillator. On Series 2 devices with precision mode support, the precision mode is configured in the configuration header sl_device_init_lfrco_config.h. On other devices, there is nothing to configure.

If using Simplicity Studio, this configuration header is also configurable through the Project Configurator, by selecting the "Device Init: LFRCO" configuration component.

Functions#

sl_status_t

Initialize LFRCO.

Function Documentation#

sl_device_init_lfrco#

sl_status_t sl_device_init_lfrco (void )

Initialize LFRCO.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize the low frequency RC oscillator. On devices that support high precision mode, this function configures the precision mode based on the configuration option SL_DEVICE_INIT_LFRCO_PRECISION.

Returns

  • Status code

Return values

  • SL_STATUS_OK: LFRCO initialized successfully