Define crash registers as structs so a debugger can display their bit fields.

Public Attributes#

uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
uint32_t
struct HalCrashxPsrType::@1

bits

uint32_t

word

Public Attribute Documentation#

EXCPT#

uint32_t HalCrashxPsrType::EXCPT

ICIIT_LOW#

uint32_t HalCrashxPsrType::ICIIT_LOW

__pad0__#

uint32_t HalCrashxPsrType::__pad0__

T#

uint32_t HalCrashxPsrType::T

ICIIT_HIGH#

uint32_t HalCrashxPsrType::ICIIT_HIGH

Q#

uint32_t HalCrashxPsrType::Q

V#

uint32_t HalCrashxPsrType::V

C#

uint32_t HalCrashxPsrType::C

Z#

uint32_t HalCrashxPsrType::Z

N#

uint32_t HalCrashxPsrType::N

bits#

struct HalCrashxPsrType::@1 HalCrashxPsrType::bits

bits


word#

uint32_t HalCrashxPsrType::word

word