Struct representing an I/O Stream EUSART context.

Public Attributes#

EUSART_TypeDef *

eusart

CMU_Clock_TypeDef

Peripheral Clock.

GPIO_Port_TypeDef

Transmit port.

unsigned int

Transmit pin.

GPIO_Port_TypeDef

Receive port.

unsigned int

Receive pin.

GPIO_Port_TypeDef

Flow control, CTS port.

unsigned int

Flow control, CTS pin.

GPIO_Port_TypeDef

Flow control, RTS port.

unsigned int

Flow control, RTS pin.

uint8_t

Configuration flags.

sl_slist_node_t

Public Attribute Documentation#

context#

sl_iostream_uart_context_t sl_iostream_eusart_context_t::context

context


Definition at line 113 of file platform/service/iostream/inc/sl_iostream_eusart.h

eusart#

EUSART_TypeDef* sl_iostream_eusart_context_t::eusart

eusart


Definition at line 114 of file platform/service/iostream/inc/sl_iostream_eusart.h

clock#

CMU_Clock_TypeDef sl_iostream_eusart_context_t::clock

Peripheral Clock.


Definition at line 115 of file platform/service/iostream/inc/sl_iostream_eusart.h

tx_port#

GPIO_Port_TypeDef sl_iostream_eusart_context_t::tx_port

Transmit port.


Definition at line 116 of file platform/service/iostream/inc/sl_iostream_eusart.h

tx_pin#

unsigned int sl_iostream_eusart_context_t::tx_pin

Transmit pin.


Definition at line 117 of file platform/service/iostream/inc/sl_iostream_eusart.h

rx_port#

GPIO_Port_TypeDef sl_iostream_eusart_context_t::rx_port

Receive port.


Definition at line 118 of file platform/service/iostream/inc/sl_iostream_eusart.h

rx_pin#

unsigned int sl_iostream_eusart_context_t::rx_pin

Receive pin.


Definition at line 119 of file platform/service/iostream/inc/sl_iostream_eusart.h

cts_port#

GPIO_Port_TypeDef sl_iostream_eusart_context_t::cts_port

Flow control, CTS port.


Definition at line 120 of file platform/service/iostream/inc/sl_iostream_eusart.h

cts_pin#

unsigned int sl_iostream_eusart_context_t::cts_pin

Flow control, CTS pin.


Definition at line 121 of file platform/service/iostream/inc/sl_iostream_eusart.h

rts_port#

GPIO_Port_TypeDef sl_iostream_eusart_context_t::rts_port

Flow control, RTS port.


Definition at line 122 of file platform/service/iostream/inc/sl_iostream_eusart.h

rts_pin#

unsigned int sl_iostream_eusart_context_t::rts_pin

Flow control, RTS pin.


Definition at line 123 of file platform/service/iostream/inc/sl_iostream_eusart.h

flags#

uint8_t sl_iostream_eusart_context_t::flags

Configuration flags.


Definition at line 124 of file platform/service/iostream/inc/sl_iostream_eusart.h

node#

sl_slist_node_t sl_iostream_eusart_context_t::node

Definition at line 126 of file platform/service/iostream/inc/sl_iostream_eusart.h