DAC - Digital to Analog Converter#
Digital to Analog Converter (DAC) Peripheral API.
This module contains functions to control the DAC peripheral of Silicon Labs 32-bit MCUs and SoCs. The DAC converts digital values to analog signals at up to 500 ksps with 12-bit accuracy. The DAC is designed for low-energy consumption and can also provide very good performance.
Modules#
Enumerations#
Conversion mode.
Output mode.
Peripheral Reflex System signal used to trigger single sample.
Reference voltage for DAC.
Refresh interval.
Functions#
Enable/disable the DAC channel.
Initialize DAC.
Initialize DAC channel.
Set the output signal of a DAC channel to a given value.
Calculate prescaler value used to determine the DAC clock.
Reset DAC to the same state that it was in after a hardware reset.
Set the output signal of DAC channel 0 to a given value.
Set the output signal of DAC channel 1 to a given value.
Clear one or more pending DAC interrupts.
Disable one or more DAC interrupts.
Enable one or more DAC interrupts.
Get pending DAC interrupt flags.
Get enabled and pending DAC interrupt flags.
Set one or more pending DAC interrupts from SW.
Macros#
Default configuration for DAC initialization structure.
Default configuration for DAC channel initialization structure.
Enumeration Documentation#
DAC_ConvMode_TypeDef#
DAC_ConvMode_TypeDef
Conversion mode.
| Enumerator | |
|---|---|
| dacConvModeContinuous | Continuous mode. |
| dacConvModeSampleHold | Sample/hold mode. |
| dacConvModeSampleOff | Sample/shut off mode. |
DAC_Output_TypeDef#
DAC_Output_TypeDef
Output mode.
| Enumerator | |
|---|---|
| dacOutputDisable | Output to pin and ADC disabled. |
| dacOutputPin | Output to pin only. |
| dacOutputADC | Output to ADC only. |
| dacOutputPinADC | Output to pin and ADC. |
DAC_PRSSEL_TypeDef#
DAC_PRSSEL_TypeDef
Peripheral Reflex System signal used to trigger single sample.
| Enumerator | |
|---|---|
| dacPRSSELCh0 | PRS channel 0. |
| dacPRSSELCh1 | PRS channel 1. |
| dacPRSSELCh2 | PRS channel 2. |
| dacPRSSELCh3 | PRS channel 3. |
| dacPRSSELCh4 | PRS channel 4. |
| dacPRSSELCh5 | PRS channel 5. |
| dacPRSSELCh6 | PRS channel 6. |
| dacPRSSELCh7 | PRS channel 7. |
DAC_Ref_TypeDef#
DAC_Ref_TypeDef
Reference voltage for DAC.
| Enumerator | |
|---|---|
| dacRef1V25 | Internal 1.25V bandgap reference. |
| dacRef2V5 | Internal 2.5V bandgap reference. |
| dacRefVDD | VDD reference. |
DAC_Refresh_TypeDef#
DAC_Refresh_TypeDef
Refresh interval.
| Enumerator | |
|---|---|
| dacRefresh8 | Refresh every 8 prescaled cycles. |
| dacRefresh16 | Refresh every 16 prescaled cycles. |
| dacRefresh32 | Refresh every 32 prescaled cycles. |
| dacRefresh64 | Refresh every 64 prescaled cycles. |
Function Documentation#
DAC_Enable#
void DAC_Enable (DAC_TypeDef * dac, unsigned int ch, bool enable)
Enable/disable the DAC channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | A pointer to the DAC peripheral register block. |
| unsigned int | [in] | ch | A channel to enable/disable. |
| bool | [in] | enable | true to enable DAC channel, false to disable. |
DAC_Init#
void DAC_Init (DAC_TypeDef * dac, const DAC_Init_TypeDef * init)
Initialize DAC.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | A pointer to the DAC peripheral register block. |
| const DAC_Init_TypeDef * | [in] | init | A pointer to the DAC initialization structure. |
Initializes common parts for both channels. In addition, channel control configuration must be done. See DAC_InitChannel().
Note
This function will disable both channels prior to configuration.
DAC_InitChannel#
void DAC_InitChannel (DAC_TypeDef * dac, const DAC_InitChannel_TypeDef * init, unsigned int ch)
Initialize DAC channel.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | A pointer to the DAC peripheral register block. |
| const DAC_InitChannel_TypeDef * | [in] | init | A pointer to the DAC initialization structure. |
| unsigned int | [in] | ch | A channel number to initialize. |
DAC_ChannelOutputSet#
void DAC_ChannelOutputSet (DAC_TypeDef * dac, unsigned int channel, uint32_t value)
Set the output signal of a DAC channel to a given value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | A pointer to the DAC peripheral register block. |
| unsigned int | [in] | channel | A channel number to set the output. |
| uint32_t | [in] | value | A value to write to the channel output register CHnDATA. |
This function sets the output signal of a DAC channel by writing value to the corresponding CHnDATA register.
DAC_PrescaleCalc#
uint8_t DAC_PrescaleCalc (uint32_t dacFreq, uint32_t hfperFreq)
Calculate prescaler value used to determine the DAC clock.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t | [in] | dacFreq | DAC frequency wanted. The frequency will automatically be adjusted to be below the maximum allowed DAC clock. |
| uint32_t | [in] | hfperFreq | Frequency in Hz of the reference HFPER clock. Set to 0 to use the currently defined HFPER clock setting. |
The DAC clock is given by: HFPERCLK / (prescale ^ 2). If the requested DAC frequency is low and the maximum prescaler value can't adjust the actual DAC frequency lower than the requested DAC frequency, the maximum prescaler value is returned resulting in a higher DAC frequency than requested.
Returns
Prescaler value to use for DAC to achieve a clock value <=
dacFreq.
DAC_Reset#
void DAC_Reset (DAC_TypeDef * dac)
Reset DAC to the same state that it was in after a hardware reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | A pointer to the ADC peripheral register block. |
DAC_Channel0OutputSet#
void DAC_Channel0OutputSet (DAC_TypeDef * dac, uint32_t value)
Set the output signal of DAC channel 0 to a given value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | Pointer to DAC peripheral register block. |
| uint32_t | [in] | value | Value to write to the channel 0 output register CH0DATA. |
This function sets the output signal of DAC channel 0 by writing value to the CH0DATA register.
DAC_Channel1OutputSet#
void DAC_Channel1OutputSet (DAC_TypeDef * dac, uint32_t value)
Set the output signal of DAC channel 1 to a given value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | Pointer to DAC peripheral register block. |
| uint32_t | [in] | value | Value to write to the channel 1 output register CH1DATA. |
Sets the output signal of DAC channel 1 by writing value to the CH1DATA register.
DAC_IntClear#
void DAC_IntClear (DAC_TypeDef * dac, uint32_t flags)
Clear one or more pending DAC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | Pointer to DAC peripheral register block. |
| uint32_t | [in] | flags | Pending DAC interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn). |
DAC_IntDisable#
void DAC_IntDisable (DAC_TypeDef * dac, uint32_t flags)
Disable one or more DAC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | Pointer to DAC peripheral register block. |
| uint32_t | [in] | flags | DAC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn). |
DAC_IntEnable#
void DAC_IntEnable (DAC_TypeDef * dac, uint32_t flags)
Enable one or more DAC interrupts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | Pointer to DAC peripheral register block. |
| uint32_t | [in] | flags | DAC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn). |
Note
Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using DAC_IntClear() prior to enabling the interrupt.
DAC_IntGet#
uint32_t DAC_IntGet (DAC_TypeDef * dac)
Get pending DAC interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | Pointer to DAC peripheral register block. |
Note
Event bits are not cleared by the use of this function.
Returns
DAC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn).
DAC_IntGetEnabled#
uint32_t DAC_IntGetEnabled (DAC_TypeDef * dac)
Get enabled and pending DAC interrupt flags.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | Pointer to DAC peripheral register block. |
Useful for handling more interrupt sources in the same interrupt handler.
Note
Interrupt flags are not cleared by the use of this function.
Returns
Pending and enabled DAC interrupt sources. Return value is the bitwise AND combination of
the OR combination of enabled interrupt sources in DACx_IEN_nnn register (DACx_IEN_nnn) and
the OR combination of valid interrupt flags of the DAC module (DACx_IF_nnn).
DAC_IntSet#
void DAC_IntSet (DAC_TypeDef * dac, uint32_t flags)
Set one or more pending DAC interrupts from SW.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| DAC_TypeDef * | [in] | dac | Pointer to DAC peripheral register block. |
| uint32_t | [in] | flags | DAC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the DAC module (DAC_IF_nnn). |
Macro Definition Documentation#
DAC_INIT_DEFAULT#
#define DAC_INIT_DEFAULTValue:
Default configuration for DAC initialization structure.
DAC_INITCHANNEL_DEFAULT#
#define DAC_INITCHANNEL_DEFAULTValue:
Default configuration for DAC channel initialization structure.