OPAMP - Operational Amplifier#

Operational Amplifier (OPAMP) peripheral API.

This module contains functions to:

All OPAMP functions assume that the DAC clock is running. If DAC is not used, the clock can be turned off when OPAMPs are configured.

If the available gain values don't suit the application at hand, the resistor ladders can be disabled and external gain programming resistors used.

A number of predefined OPAMP setup macros are available for configuration of the most common OPAMP topologies (see figures below).

Note

  • The terms POSPAD and NEGPAD in the figures are used to indicate that these pads should be connected to a suitable signal ground.


Unity gain voltage follower.
Use predefined macros OPA_INIT_UNITY_GAIN and OPA_INIT_UNITY_GAIN_OPA2.

                    |\
         ___________|+\
                    |  \_______
                 ___|_ /    |
                |   | /     |
                |   |/      |
                |___________|


Non-inverting amplifier.
Use predefined macros OPA_INIT_NON_INVERTING and OPA_INIT_NON_INVERTING_OPA2.

                    |\
         ___________|+\
                    |  \_______
                 ___|_ /    |
                |   | /     |
                |   |/      |
                |_____R2____|
                |
                R1
                |
              NEGPAD 


Inverting amplifier.
Use predefined macros OPA_INIT_INVERTING and OPA_INIT_INVERTING_OPA2.

                 _____R2____
                |           |
                |   |\      |
         ____R1_|___|_\     |
                    |  \____|___
                 ___|  /
                |   |+/
                |   |/
                |
              POSPAD 


Cascaded non-inverting amplifiers.
Use predefined macros OPA_INIT_CASCADED_NON_INVERTING_OPA0, OPA_INIT_CASCADED_NON_INVERTING_OPA1 and OPA_INIT_CASCADED_NON_INVERTING_OPA2.

                    |\                       |\                       |\
         ___________|+\ OPA0      ___________|+\ OPA1      ___________|+\ OPA2
                    |  \_________|           |  \_________|           |  \_______
                 ___|_ /    |             ___|_ /    |             ___|_ /    |
                |   | /     |            |   | /     |            |   | /     |
                |   |/      |            |   |/      |            |   |/      |
                |_____R2____|            |_____R2____|            |_____R2____|
                |                        |                        |
                R1                       R1                       R1
                |                        |                        |
              NEGPAD                   NEGPAD                   NEGPAD 


Cascaded inverting amplifiers.
Use predefined macros OPA_INIT_CASCADED_INVERTING_OPA0, OPA_INIT_CASCADED_INVERTING_OPA1 and OPA_INIT_CASCADED_INVERTING_OPA2.

                 _____R2____              _____R2____              _____R2____
                |           |            |           |            |           |
                |   |\      |            |   |\      |            |   |\      |
         ____R1_|___|_\     |     ____R1_|___|_\     |     ____R1_|___|_\     |
                    |  \____|____|           |  \____|___|            |  \____|__
                 ___|  /                  ___|  /                  ___|  /
                |   |+/ OPA0             |   |+/ OPA1             |   |+/ OPA2
                |   |/                   |   |/                   |   |/
                |                        |                        |
              POSPAD                   POSPAD                   POSPAD 


Differential driver with two opamp's.
Use predefined macros OPA_INIT_DIFF_DRIVER_OPA0 and OPA_INIT_DIFF_DRIVER_OPA1.

                                  __________________________
                                 |                          +
                                 |        _____R2____
                    |\           |       |           |
         ___________|+\ OPA0     |       |   |\ OPA1 |
                    |  \_________|____R1_|___|_\     |      _
                 ___|_ /         |           |  \____|______
                |   | /          |        ___|  /
                |   |/           |       |   |+/
                |________________|       |   |/
                                         |
                                       POSPAD 


Differential receiver with three opamp's.
Use predefined macros OPA_INIT_DIFF_RECEIVER_OPA0, OPA_INIT_DIFF_RECEIVER_OPA1 and OPA_INIT_DIFF_RECEIVER_OPA2.

                    |\
          __________|+\ OPA1
         _          |  \_________
                 ___|_ /    |    |        _____R2____
                |   | /     |    |       |           |
                |   |/      |    |       |   |\      |
                |___________|    |____R1_|___|_\     |
                                             |  \____|___
                    |\            ____R1_ ___|  /
         +__________|+\ OPA0     |       |   |+/ OPA2
                    |  \_________|       |   |/
                 ___|_ /    |            R2
                |   | /     |            |
                |   |/      |          NEGPAD OPA0
                |___________|

Modules#

OPAMP_Init_TypeDef

Enumerations#

enum
OPA0 = 0
OPA1 = 1
OPA2 = 2
}

OPAMP selector values.

enum
opaNegSelDisable = DAC_OPA0MUX_NEGSEL_DISABLE
opaNegSelUnityGain = DAC_OPA0MUX_NEGSEL_UG
opaNegSelResTap = DAC_OPA0MUX_NEGSEL_OPATAP
opaNegSelNegPad = DAC_OPA0MUX_NEGSEL_NEGPAD
}

OPAMP negative terminal input selection values.

enum
opaPosSelDisable = DAC_OPA0MUX_POSSEL_DISABLE
opaPosSelDac = DAC_OPA0MUX_POSSEL_DAC
opaPosSelPosPad = DAC_OPA0MUX_POSSEL_POSPAD
opaPosSelOpaIn = DAC_OPA0MUX_POSSEL_OPA0INP
opaPosSelResTapOpa0 = DAC_OPA0MUX_POSSEL_OPATAP
}

OPAMP positive terminal input selection values.

enum
opaOutModeDisable = DAC_OPA0MUX_OUTMODE_DISABLE
opaOutModeMain = DAC_OPA0MUX_OUTMODE_MAIN
opaOutModeAlt = DAC_OPA0MUX_OUTMODE_ALT
opaOutModeAll = DAC_OPA0MUX_OUTMODE_ALL
}

OPAMP output terminal selection values.

enum
opaResSelDefault = DAC_OPA0MUX_RESSEL_DEFAULT
opaResSelR2eq0_33R1 = DAC_OPA0MUX_RESSEL_RES0
opaResSelR2eqR1 = DAC_OPA0MUX_RESSEL_RES1
opaResSelR1eq1_67R1 = DAC_OPA0MUX_RESSEL_RES2
opaResSelR2eq2R1 = DAC_OPA0MUX_RESSEL_RES3
opaResSelR2eq3R1 = DAC_OPA0MUX_RESSEL_RES4
opaResSelR2eq4_33R1 = DAC_OPA0MUX_RESSEL_RES5
opaResSelR2eq7R1 = DAC_OPA0MUX_RESSEL_RES6
opaResSelR2eq15R1 = DAC_OPA0MUX_RESSEL_RES7
}

OPAMP gain values.

enum
opaResInMuxDisable = DAC_OPA0MUX_RESINMUX_DISABLE
opaResInMuxOpaIn = DAC_OPA0MUX_RESINMUX_OPA0INP
opaResInMuxNegPad = DAC_OPA0MUX_RESINMUX_NEGPAD
opaResInMuxPosPad = DAC_OPA0MUX_RESINMUX_POSPAD
opaResInMuxVss = DAC_OPA0MUX_RESINMUX_VSS
}

OPAMP resistor ladder input selector values.

Functions#

void
OPAMP_Disable(DAC_TypeDef *dac, OPAMP_TypeDef opa)

Disable an Operational Amplifier.

void
OPAMP_Enable(DAC_TypeDef *dac, OPAMP_TypeDef opa, const OPAMP_Init_TypeDef *init)

Configure and enable an Operational Amplifier.

Macros#

#define
OPA_INIT_UNITY_GAIN undefined

Configuration of OPA0/1 in unity gain voltage follower mode.

#define
OPA_INIT_UNITY_GAIN_OPA2 undefined

Configuration of OPA2 in unity gain voltage follower mode.

#define
OPA_INIT_NON_INVERTING undefined

Configuration of OPA0/1 in non-inverting amplifier mode.

#define
OPA_INIT_NON_INVERTING_OPA2 undefined

Configuration of OPA2 in non-inverting amplifier mode.

#define
OPA_INIT_INVERTING undefined

Configuration of OPA0/1 in inverting amplifier mode.

#define
OPA_INIT_INVERTING_OPA2 undefined

Configuration of OPA2 in inverting amplifier mode.

#define
OPA_INIT_CASCADED_NON_INVERTING_OPA0 undefined

Configuration of OPA0 in cascaded non-inverting amplifier mode.

#define
OPA_INIT_CASCADED_NON_INVERTING_OPA1 undefined

Configuration of OPA1 in cascaded non-inverting amplifier mode.

#define
OPA_INIT_CASCADED_NON_INVERTING_OPA2 undefined

Configuration of OPA2 in cascaded non-inverting amplifier mode.

#define
OPA_INIT_CASCADED_INVERTING_OPA0 undefined

Configuration of OPA0 in cascaded inverting amplifier mode.

#define
OPA_INIT_CASCADED_INVERTING_OPA1 undefined

Configuration of OPA1 in cascaded inverting amplifier mode.

#define
OPA_INIT_CASCADED_INVERTING_OPA2 undefined

Configuration of OPA2 in cascaded inverting amplifier mode.

#define
OPA_INIT_DIFF_DRIVER_OPA0 undefined

Configuration of OPA0 in two-opamp differential driver mode.

#define
OPA_INIT_DIFF_DRIVER_OPA1 undefined

Configuration of OPA1 in two-opamp differential driver mode.

#define
OPA_INIT_DIFF_RECEIVER_OPA0 undefined

Configuration of OPA0 in three-opamp differential receiver mode.

#define
OPA_INIT_DIFF_RECEIVER_OPA1 undefined

Configuration of OPA1 in three-opamp differential receiver mode.

#define
OPA_INIT_DIFF_RECEIVER_OPA2 undefined

Configuration of OPA2 in three-opamp differential receiver mode.

Enumeration Documentation#

OPAMP_TypeDef#

OPAMP_TypeDef

OPAMP selector values.

Enumerator
OPA0

Select OPA0.

OPA1

Select OPA1.

OPA2

Select OPA2.


OPAMP_NegSel_TypeDef#

OPAMP_NegSel_TypeDef

OPAMP negative terminal input selection values.

Enumerator
opaNegSelDisable

Input disabled.

opaNegSelUnityGain

Unity gain feedback path.

opaNegSelResTap

Feedback resistor ladder tap.

opaNegSelNegPad

Negative pad as input.


OPAMP_PosSel_TypeDef#

OPAMP_PosSel_TypeDef

OPAMP positive terminal input selection values.

Enumerator
opaPosSelDisable

Input disabled.

opaPosSelDac

DAC as input (not OPA2).

opaPosSelPosPad

Positive pad as input.

opaPosSelOpaIn

Input from OPAx.

opaPosSelResTapOpa0

Feedback resistor ladder tap from OPA0.


OPAMP_OutMode_TypeDef#

OPAMP_OutMode_TypeDef

OPAMP output terminal selection values.

Enumerator
opaOutModeDisable

OPA output disabled.

opaOutModeMain

Main output to pin enabled.

opaOutModeAlt

Alternate output(s) enabled (not OPA2).

opaOutModeAll

Both main and alternate enabled (not OPA2).


OPAMP_ResSel_TypeDef#

OPAMP_ResSel_TypeDef

OPAMP gain values.

Enumerator
opaResSelDefault

Default value when resistor ladder is unused.

opaResSelR2eq0_33R1

R2 = 0.33 * R1.

opaResSelR2eqR1

R2 = R1

opaResSelR1eq1_67R1

R2 = 1.67 R1

opaResSelR2eq2R1

R2 = 2 * R1

opaResSelR2eq3R1

R2 = 3 * R1

opaResSelR2eq4_33R1

R2 = 4.33 * R1.

opaResSelR2eq7R1

R2 = 7 * R1

opaResSelR2eq15R1

R2 = 15 * R1


OPAMP_ResInMux_TypeDef#

OPAMP_ResInMux_TypeDef

OPAMP resistor ladder input selector values.

Enumerator
opaResInMuxDisable

Resistor ladder disabled.

opaResInMuxOpaIn

Input from OPAx.

opaResInMuxNegPad

Input from negative pad.

opaResInMuxPosPad

Input from positive pad.

opaResInMuxVss

Input connected to Vss.


Function Documentation#

OPAMP_Disable#

void OPAMP_Disable (DAC_TypeDef * dac, OPAMP_TypeDef opa)

Disable an Operational Amplifier.

Parameters
TypeDirectionArgument NameDescription
DAC_TypeDef *[in]dac

A pointer to the DAC peripheral register block.

OPAMP_TypeDef[in]opa

Selects an OPA, valid values are OPA0, OPA1, and OPA2.


OPAMP_Enable#

void OPAMP_Enable (DAC_TypeDef * dac, OPAMP_TypeDef opa, const OPAMP_Init_TypeDef * init)

Configure and enable an Operational Amplifier.

Parameters
TypeDirectionArgument NameDescription
DAC_TypeDef *[in]dac

A pointer to the DAC peripheral register block.

OPAMP_TypeDef[in]opa

Selects an OPA, valid values are OPA0, OPA1, and OPA2.

const OPAMP_Init_TypeDef *[in]init

A pointer to a structure containing OPAMP initialization information.

Note

  • The value of the alternate output enable bit mask in the OPAMP_Init_TypeDef structure should consist of one or more of the DAC_OPA[opa#]MUX_OUTPEN_OUT[output#] flags (defined in <part_name>_dac.h) OR'ed together.

    For OPA0:

    • DAC_OPA0MUX_OUTPEN_OUT0

    • DAC_OPA0MUX_OUTPEN_OUT1

    • DAC_OPA0MUX_OUTPEN_OUT2

    • DAC_OPA0MUX_OUTPEN_OUT3

    • DAC_OPA0MUX_OUTPEN_OUT4

    For OPA1:

    • DAC_OPA1MUX_OUTPEN_OUT0

    • DAC_OPA1MUX_OUTPEN_OUT1

    • DAC_OPA1MUX_OUTPEN_OUT2

    • DAC_OPA1MUX_OUTPEN_OUT3

    • DAC_OPA1MUX_OUTPEN_OUT4

    For OPA2:

    • DAC_OPA2MUX_OUTPEN_OUT0

    • DAC_OPA2MUX_OUTPEN_OUT1

    E.g:
    init.outPen = DAC_OPA0MUX_OUTPEN_OUT0 | DAC_OPA0MUX_OUTPEN_OUT4;