DEFINES ***********************************.

Defines each text symbol's segment in terms of COM and BIT numbers, in a way that we can enumerate each bit for each text segment in the following bit pattern:

*  -------0------
*
* |   \7  |8  /9 |
* |5   \  |  /   |1
*
*  --6---  ---10--
*
* |    /  |  \11 |
* |4  /13 |12 \  |2
*
*  -------3------
* 

E.g.: First text character bit pattern #3 (above) is Segment 1D for Display Location COM 3, BIT 0

Public Attributes#

uint8_t

LCD COM line (for multiplexing)

uint8_t

LCD bit number.

Public Attribute Documentation#

com#

uint8_t sl_segment_lcd_char_t::com[14]

LCD COM line (for multiplexing)


Definition at line 133 of file hardware/driver/segment_lcd/inc/sl_segmentlcd.h

bit#

uint8_t sl_segment_lcd_char_t::bit[14]

LCD bit number.


Definition at line 134 of file hardware/driver/segment_lcd/inc/sl_segmentlcd.h