Public Attributes#

uint64_t

Total length of the encrypted data.

uint64_t

Total length of the additional data.

uint8_t

SE state.

uint8_t

Input data saved for finish operation.

uint8_t

Length of data saved.

bool

First operation.

Public Attribute Documentation#

len#

uint64_t sl_se_gcm_multipart_context_t::len

Total length of the encrypted data.


Definition at line 365 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

add_len#

uint64_t sl_se_gcm_multipart_context_t::add_len

Total length of the additional data.


Definition at line 366 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

se_ctx#

uint8_t sl_se_gcm_multipart_context_t::se_ctx[32]

SE state.


Definition at line 371 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

final_data#

uint8_t sl_se_gcm_multipart_context_t::final_data[16]

Input data saved for finish operation.


Definition at line 372 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

final_data_length#

uint8_t sl_se_gcm_multipart_context_t::final_data_length

Length of data saved.


Definition at line 373 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

mode#

sl_se_cipher_operation_t sl_se_gcm_multipart_context_t::mode

GCM mode.


Definition at line 374 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h

first_operation#

bool sl_se_gcm_multipart_context_t::first_operation

First operation.


Definition at line 375 of file platform/security/sl_component/se_manager/inc/sl_se_manager_types.h