A Cycle Counter Instance.

Public Attributes#

uint32_t

Cycle counter at start of recording.

uint32_t

Cycles elapsed in last recording.

uint32_t

Max recorded cycles since last reset or init.

Public Attribute Documentation#

start#

uint32_t sl_cycle_counter_handle_t::start

Cycle counter at start of recording.


Definition at line 103 of file platform/driver/cycle_counter/inc/sl_cycle_counter.h

cycles#

uint32_t sl_cycle_counter_handle_t::cycles

Cycles elapsed in last recording.


Definition at line 104 of file platform/driver/cycle_counter/inc/sl_cycle_counter.h

max#

uint32_t sl_cycle_counter_handle_t::max

Max recorded cycles since last reset or init.


Definition at line 105 of file platform/driver/cycle_counter/inc/sl_cycle_counter.h