DMA - Direct Memory Access#

Direct Memory Access (DMA) Peripheral API.

DMA access functions provide basic support for the following types of DMA cycles:

  • Basic, used for transferring data between memory and peripherals.

  • Auto-request, used for transferring data between memory locations.

  • Ping-pong, used for for continuous transfer of data between memory and peripherals, automatically toggling between primary and alternate descriptors.

  • Memoryscatter-gather, used for transferring a number of buffers between memory locations.

  • Peripheralscatter-gather, used for transferring a number of buffers between memory and peripherals.

A basic understanding of the DMA controller is assumed. See the reference manual for more details.

The term 'descriptor' is synonymous to the 'channel control data structure' term.

To use the DMA controller, the initialization function must have been executed once (normally during the system initialization):

* DMA_Init();
* 

Normally, a DMA channel is configured:

* DMA_CfgChannel();
* 

The channel configuration only has to be done once if reusing the channel for the same purpose later.

To set up a DMA cycle, the primary and/or alternate descriptor has to be set up as indicated below.

For basic or auto-request cycles, use once on either primary or alternate descriptor:

* DMA_CfgDescr();
* 

For ping-pong cycles, configure both primary or alternate descriptors:

* DMA_CfgDescr(); // Primary descriptor config
* DMA_CfgDescr(); // Alternate descriptor config
* 

For scatter-gather cycles, program the alternate descriptor array:

* // 'n' is the number of scattered buffers
* // 'descr' points to the start of the alternate descriptor array
*
* // Fill in 'cfg'
* DMA_CfgDescrScatterGather(descr, 0, cfg);
* // Fill in 'cfg'
* DMA_CfgDescrScatterGather(descr, 1, cfg);
* :
* // Fill in 'cfg'
* DMA_CfgDescrScatterGather(descr, n - 1, cfg);
* 

In many cases, the descriptor configuration only has to be done once if re-using the channel for the same type of DMA cycles later.

To activate the DMA cycle, use the respective DMA_Activate...() function.

For ping-pong DMA cycles, use DMA_RefreshPingPong() from the callback to prepare the completed descriptor for reuse. Notice that the refresh must be done prior to the other active descriptor completes, otherwise the ping-pong DMA cycle will halt.

Modules#

DMA_CB_TypeDef

DMA_CfgChannel_TypeDef

DMA_CfgDescr_TypeDef

DMA_CfgLoop_TypeDef

DMA_CfgRect_TypeDef

DMA_CfgDescrSGAlt_TypeDef

DMA_Init_TypeDef

Enumerations#

enum
dmaDataInc1 = _DMA_CTRL_SRC_INC_BYTE
dmaDataInc2 = _DMA_CTRL_SRC_INC_HALFWORD
dmaDataInc4 = _DMA_CTRL_SRC_INC_WORD
dmaDataIncNone = _DMA_CTRL_SRC_INC_NONE
}

Amount source/destination address should be incremented for each data transfer.

enum
dmaDataSize1 = _DMA_CTRL_SRC_SIZE_BYTE
dmaDataSize2 = _DMA_CTRL_SRC_SIZE_HALFWORD
dmaDataSize4 = _DMA_CTRL_SRC_SIZE_WORD
}

Data sizes (in number of bytes) to be read/written by DMA transfer.

enum
dmaCycleCtrlBasic = _DMA_CTRL_CYCLE_CTRL_BASIC
dmaCycleCtrlAuto = _DMA_CTRL_CYCLE_CTRL_AUTO
dmaCycleCtrlPingPong = _DMA_CTRL_CYCLE_CTRL_PINGPONG
dmaCycleCtrlMemScatterGather = _DMA_CTRL_CYCLE_CTRL_MEM_SCATTER_GATHER
dmaCycleCtrlPerScatterGather = _DMA_CTRL_CYCLE_CTRL_PER_SCATTER_GATHER
}

Types of DMA transfer.

enum
dmaArbitrate1 = _DMA_CTRL_R_POWER_1
dmaArbitrate2 = _DMA_CTRL_R_POWER_2
dmaArbitrate4 = _DMA_CTRL_R_POWER_4
dmaArbitrate8 = _DMA_CTRL_R_POWER_8
dmaArbitrate16 = _DMA_CTRL_R_POWER_16
dmaArbitrate32 = _DMA_CTRL_R_POWER_32
dmaArbitrate64 = _DMA_CTRL_R_POWER_64
dmaArbitrate128 = _DMA_CTRL_R_POWER_128
dmaArbitrate256 = _DMA_CTRL_R_POWER_256
dmaArbitrate512 = _DMA_CTRL_R_POWER_512
dmaArbitrate1024 = _DMA_CTRL_R_POWER_1024
}

Number of transfers before controller does new arbitration.

Typedefs#

typedef void(*
DMA_FuncPtr_TypeDef)(unsigned int channel, bool primary, void *user)

DMA interrupt callback function pointer.

Functions#

void

Interrupt handler for the DMA cycle completion handling.

void
DMA_ActivateAuto(unsigned int channel, bool primary, void *dst, const void *src, unsigned int nMinus1)

Activate the DMA auto-request cycle (used for memory-memory transfers).

void
DMA_ActivateBasic(unsigned int channel, bool primary, bool useBurst, void *dst, const void *src, unsigned int nMinus1)

Activate the DMA basic cycle (used for memory-peripheral transfers).

void
DMA_ActivatePingPong(unsigned int channel, bool useBurst, void *primDst, const void *primSrc, unsigned int primNMinus1, void *altDst, const void *altSrc, unsigned int altNMinus1)

Activate a DMA ping-pong cycle (used for memory-peripheral transfers).

void
DMA_ActivateScatterGather(unsigned int channel, bool useBurst, DMA_DESCRIPTOR_TypeDef *altDescr, unsigned int count)

Activate the DMA scatter-gather cycle (used for either memory-peripheral or memory-memory transfers).

void
DMA_CfgChannel(unsigned int channel, DMA_CfgChannel_TypeDef *cfg)

Configure a DMA channel.

void
DMA_CfgDescr(unsigned int channel, bool primary, DMA_CfgDescr_TypeDef *cfg)

Configure the DMA descriptor for auto-request, basic, or ping-pong DMA cycles.

void
DMA_CfgLoop(unsigned int channel, DMA_CfgLoop_TypeDef *cfg)

Configure the DMA channel for Loop mode or 2D transfer.

void
DMA_CfgRect(unsigned int channel, DMA_CfgRect_TypeDef *cfg)

Configure the DMA channel 2D transfer properties.

void
DMA_CfgDescrScatterGather(DMA_DESCRIPTOR_TypeDef *descr, unsigned int indx, DMA_CfgDescrSGAlt_TypeDef *cfg)

Configure an alternate DMA descriptor for use with scatter-gather DMA cycles.

void
DMA_ChannelEnable(unsigned int channel, bool enable)

Enable or disable a DMA channel.

bool
DMA_ChannelEnabled(unsigned int channel)

Check if the DMA channel is enabled.

void
DMA_ChannelRequestEnable(unsigned int channel, bool enable)

Enable or disable a DMA channel request.

void
DMA_Init(DMA_Init_TypeDef *init)

Initialize the DMA controller.

void
DMA_RefreshPingPong(unsigned int channel, bool primary, bool useBurst, void *dst, const void *src, unsigned int nMinus1, bool stop)

Refresh a descriptor used in a DMA ping-pong cycle.

void
DMA_Reset(void)

Reset the DMA controller.

void
DMA_ResetLoop(unsigned int channel)

Clear Loop configuration for channel.

void
DMA_ResetRect(unsigned int channel)

Clear Rect/2D DMA configuration for channel.

void
DMA_IntClear(uint32_t flags)

Clear one or more pending DMA interrupts.

void
DMA_IntDisable(uint32_t flags)

Disable one or more DMA interrupts.

void
DMA_IntEnable(uint32_t flags)

Enable one or more DMA interrupts.

uint32_t

Get pending DMA interrupt flags.

uint32_t

Get enabled and pending DMA interrupt flags.

void
DMA_IntSet(uint32_t flags)

Set one or more pending DMA interrupts.

Enumeration Documentation#

DMA_DataInc_TypeDef#

DMA_DataInc_TypeDef

Amount source/destination address should be incremented for each data transfer.

Enumerator
dmaDataInc1

Increment address 1 byte.

dmaDataInc2

Increment address 2 bytes.

dmaDataInc4

Increment address 4 bytes.

dmaDataIncNone

Do not increment address.


Definition at line 57 of file platform/emlib/inc/em_dma.h

DMA_DataSize_TypeDef#

DMA_DataSize_TypeDef

Data sizes (in number of bytes) to be read/written by DMA transfer.

Enumerator
dmaDataSize1

1 byte DMA transfer size.

dmaDataSize2

2 byte DMA transfer size.

dmaDataSize4

4 byte DMA transfer size.


Definition at line 65 of file platform/emlib/inc/em_dma.h

DMA_CycleCtrl_TypeDef#

DMA_CycleCtrl_TypeDef

Types of DMA transfer.

Enumerator
dmaCycleCtrlBasic

Basic DMA cycle.

dmaCycleCtrlAuto

Auto-request DMA cycle.

dmaCycleCtrlPingPong

Ping-pong DMA cycle.

dmaCycleCtrlMemScatterGather

Memory scatter-gather DMA cycle.

dmaCycleCtrlPerScatterGather

Peripheral scatter-gather DMA cycle.


Definition at line 72 of file platform/emlib/inc/em_dma.h

DMA_ArbiterConfig_TypeDef#

DMA_ArbiterConfig_TypeDef

Number of transfers before controller does new arbitration.

Enumerator
dmaArbitrate1

Arbitrate after 1 DMA transfer.

dmaArbitrate2

Arbitrate after 2 DMA transfers.

dmaArbitrate4

Arbitrate after 4 DMA transfers.

dmaArbitrate8

Arbitrate after 8 DMA transfers.

dmaArbitrate16

Arbitrate after 16 DMA transfers.

dmaArbitrate32

Arbitrate after 32 DMA transfers.

dmaArbitrate64

Arbitrate after 64 DMA transfers.

dmaArbitrate128

Arbitrate after 128 DMA transfers.

dmaArbitrate256

Arbitrate after 256 DMA transfers.

dmaArbitrate512

Arbitrate after 512 DMA transfers.

dmaArbitrate1024

Arbitrate after 1024 DMA transfers.


Definition at line 86 of file platform/emlib/inc/em_dma.h

Typedef Documentation#

DMA_FuncPtr_TypeDef#

typedef void(* DMA_FuncPtr_TypeDef) (unsigned int channel, bool primary, void *user) )(unsigned int channel, bool primary, void *user)

DMA interrupt callback function pointer.

Parameters:

  • channel - DMA channel the callback function is invoked for.

  • primary - Indicates if callback is invoked for completion of primary (true) or alternate (false) descriptor. Mainly useful for ping-pong DMA cycles, to know which descriptor to refresh.

  • user - User definable reference that may be used to pass information to be used by the callback handler. If used, referenced data must be valid at the point when the interrupt handler invokes callback. If callback changes any data in the provided user structure, remember that those changes are done in interrupt context and proper protection of data may be required.


Definition at line 120 of file platform/emlib/inc/em_dma.h

Function Documentation#

DMA_IRQHandler#

void DMA_IRQHandler (void )

Interrupt handler for the DMA cycle completion handling.

Parameters
N/A

Clears any pending flags and calls registered callback (if any).

If using the default interrupt vector table setup provided, this function is automatically placed in the IRQ table due to weak linking. If taking control over the interrupt vector table in some other way, this interrupt handler must be installed to support callback actions.

For the user to implement a custom IRQ handler or run without a DMA IRQ handler, define EXCLUDE_DEFAULT_DMA_IRQ_HANDLER with a #define statement or with the compiler option -D.


Definition at line 259 of file platform/emlib/src/em_dma.c

DMA_ActivateAuto#

void DMA_ActivateAuto (unsigned int channel, bool primary, void * dst, const void * src, unsigned int nMinus1)

Activate the DMA auto-request cycle (used for memory-memory transfers).

Parameters
[in]channel

The DMA channel to activate the DMA cycle for.

[in]primary
  • true - activate using the primary descriptor

  • false - activate using an alternate descriptor

[in]dst

An ddress to a start location to transfer data to. If NULL, leave setting in descriptor as is from a previous activation.

[in]src

An address to a start location to transfer data from. If NULL, leave setting in descriptor as is from a previous activation.

[in]nMinus1

A number of DMA transfer elements (minus 1) to transfer (<= 1023). The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr().

Prior to activating the DMA cycle, the channel and descriptor to be used must have been properly configured.

Note

  • If using this function on a channel already activated and in use by the DMA controller, the behavior is undefined.


Definition at line 355 of file platform/emlib/src/em_dma.c

DMA_ActivateBasic#

void DMA_ActivateBasic (unsigned int channel, bool primary, bool useBurst, void * dst, const void * src, unsigned int nMinus1)

Activate the DMA basic cycle (used for memory-peripheral transfers).

Parameters
[in]channel

The DMA channel to activate the DMA cycle for.

[in]primary
  • true - activate using the primary descriptor

  • false - activate using an alternate descriptor

[in]useBurst

The burst feature is only used on peripherals supporting DMA bursts. Bursts must not be used if the total length (as given by nMinus1) is less than the arbitration rate configured for the descriptor. See the reference manual for more details on burst usage.

[in]dst

An address to a start location to transfer data to. If NULL, leave setting in descriptor as is from a previous activation.

[in]src

An address to a start location to transfer data from. If NULL, leave setting in descriptor as is from a previous activation.

[in]nMinus1

A number of DMA transfer elements (minus 1) to transfer (<= 1023). The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr().

Prior to activating the DMA cycle, the channel and descriptor to be used must have been properly configured.

Note

  • If using this function on a channel already activated and in use by the DMA controller, the behavior is undefined.


Definition at line 417 of file platform/emlib/src/em_dma.c

DMA_ActivatePingPong#

void DMA_ActivatePingPong (unsigned int channel, bool useBurst, void * primDst, const void * primSrc, unsigned int primNMinus1, void * altDst, const void * altSrc, unsigned int altNMinus1)

Activate a DMA ping-pong cycle (used for memory-peripheral transfers).

Parameters
[in]channel

The DMA channel to activate DMA cycle for.

[in]useBurst

The burst feature is only used on peripherals supporting DMA bursts. Bursts must not be used if the total length (as given by nMinus1) is less than the arbitration rate configured for the descriptors. See the reference manual for more details on burst usage. Notice that this setting is used for both the primary and alternate descriptors.

[in]primDst

An address to a start location to transfer data to, for the primary descriptor. If NULL, leave setting in descriptor as is from a previous activation.

[in]primSrc

An address to a start location to transfer data from, for the primary descriptor. If NULL, leave setting in the descriptor as is from a previous activation.

[in]primNMinus1

A number of DMA transfer elements (minus 1) to transfer (<= 1023), for primary descriptor. The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr().

[in]altDst

An address to a start location to transfer data to, for an alternate descriptor. If NULL, leave setting in descriptor as is from a previous activation.

[in]altSrc

An address to a start location to transfer data from, for an alternate descriptor. If NULL, leave setting in descriptor as is from a previous activation.

[in]altNMinus1

A number of DMA transfer elements (minus 1) to transfer (<= 1023), for an alternate descriptor. The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr().

Prior to activating the DMA cycle, the channel and both descriptors must have been properly configured. The primary descriptor is always the first descriptor to be used by the DMA controller.

Note

  • If using this function on a channel already activated and in use by the DMA controller, the behavior is undefined.


Definition at line 488 of file platform/emlib/src/em_dma.c

DMA_ActivateScatterGather#

void DMA_ActivateScatterGather (unsigned int channel, bool useBurst, DMA_DESCRIPTOR_TypeDef * altDescr, unsigned int count)

Activate the DMA scatter-gather cycle (used for either memory-peripheral or memory-memory transfers).

Parameters
[in]channel

The DMA channel to activate DMA cycle for.

[in]useBurst

The burst feature is only used on peripherals supporting DMA bursts (this parameter is ignored for memory scatter-gather cycles). This parameter determines if bursts should be enabled during DMA transfers using the alternate descriptors. Bursts must not be used if the total length (as given by nMinus1 for the alternate descriptor) is less than the arbitration rate configured for the descriptor. See the reference manual for more details on burst usage.

[inout]altDescr

A pointer to a start of an array with prepared alternate descriptors. The last descriptor will have its cycle control type reprogrammed to a basic type.

[in]count

A number of alternate descriptors in altDescr array. The maximum number of alternate descriptors is 256.

Prior to activating the DMA cycle, the array with alternate descriptors must have been properly configured. This function can be reused without reconfiguring the alternate descriptors, as long as count is the same.

Note

  • If using this function on a channel already activated and in use by the DMA controller, the behavior is undefined.


Definition at line 557 of file platform/emlib/src/em_dma.c

DMA_CfgChannel#

void DMA_CfgChannel (unsigned int channel, DMA_CfgChannel_TypeDef * cfg)

Configure a DMA channel.

Parameters
[in]channel

The DMA channel to configure.

[in]cfg

The configuration to use.

Configure miscellaneous issues for a DMA channel. This function is typically used once to set up a channel for a certain type of use.

Note

  • If using this function on a channel already in use by the DMA controller, the behavior is undefined.


Definition at line 661 of file platform/emlib/src/em_dma.c

DMA_CfgDescr#

void DMA_CfgDescr (unsigned int channel, bool primary, DMA_CfgDescr_TypeDef * cfg)

Configure the DMA descriptor for auto-request, basic, or ping-pong DMA cycles.

Parameters
[in]channel

The DMA channel to configure for.

[in]primary
  • true - configure the primary descriptor

  • false - configure an alternate descriptor

[in]cfg

The configuration to use.

This function is used to configure a descriptor for the following DMA cycle types:

  • auto-request - used for a memory/memory transfer

  • basic - used for a peripheral/memory transfer

  • ping-pong - used for a ping-pong-based peripheral/memory transfer style providing time to refresh one descriptor while the other is in use.

The DMA cycle is not activated. See DMA_ActivateAuto(), DMA_ActivateBasic(), or DMA_ActivatePingPong() to activate the DMA cycle. In many cases, the configuration only has to be done once, and all subsequent cycles may be activated with the activate function.

For ping-pong DMA cycles, this function must be used both on the primary and the alternate descriptor prior to activating the DMA cycle.

Notice that the DMA channel must also be configured. See DMA_CfgChannel().

Note

  • If using this function on a descriptor already activated and in use by the DMA controller, the behavior is undefined.


Definition at line 729 of file platform/emlib/src/em_dma.c

DMA_CfgLoop#

void DMA_CfgLoop (unsigned int channel, DMA_CfgLoop_TypeDef * cfg)

Configure the DMA channel for Loop mode or 2D transfer.

Parameters
[in]channel

The DMA channel to configure for.

[in]cfg

The configuration to use.

For 2D transfer, set cfg->enable to "false" and only configure nMinus1 to the same width as the channel descriptor.


Definition at line 773 of file platform/emlib/src/em_dma.c

DMA_CfgRect#

void DMA_CfgRect (unsigned int channel, DMA_CfgRect_TypeDef * cfg)

Configure the DMA channel 2D transfer properties.

Parameters
[in]channel

The DMA channel to configure for.

[in]cfg

The configuration to use.


Definition at line 802 of file platform/emlib/src/em_dma.c

DMA_CfgDescrScatterGather#

void DMA_CfgDescrScatterGather (DMA_DESCRIPTOR_TypeDef * descr, unsigned int indx, DMA_CfgDescrSGAlt_TypeDef * cfg)

Configure an alternate DMA descriptor for use with scatter-gather DMA cycles.

Parameters
[in]descr

Points to the start of a memory area holding the alternate descriptors.

[in]indx

An alternate descriptor index number to configure (numbered from 0).

[in]cfg

The configuration to use.

In scatter-gather mode, the alternate descriptors are located in one contiguous memory area. Each of the alternate descriptors must be fully configured prior to starting the scatter-gather DMA cycle.

The DMA cycle is not activated by this function. See DMA_ActivateScatterGather() to activate the DMA cycle. In some cases, the alternate configuration only has to be done once and all subsequent transfers may be activated with the activate function.

Notice that the DMA channel must also be configured, see DMA_CfgChannel().


Definition at line 844 of file platform/emlib/src/em_dma.c

DMA_ChannelEnable#

void DMA_ChannelEnable (unsigned int channel, bool enable)

Enable or disable a DMA channel.

Parameters
[in]channel

The DMA channel to enable or disable.

[in]enable

If 'true', the channel will be enabled. If 'false', the channel will be disabled.

Use this function to explicitly enable or disable a DMA channel. A DMA channel is automatically disabled when the DMA controller has finished a transaction.


Definition at line 910 of file platform/emlib/src/em_dma.c

DMA_ChannelEnabled#

bool DMA_ChannelEnabled (unsigned int channel)

Check if the DMA channel is enabled.

Parameters
[in]channel

The DMA channel to check.

The DMA channel is disabled when the DMA controller has finished a DMA cycle.

Returns

  • True if the channel is enabled, false if not.


Definition at line 935 of file platform/emlib/src/em_dma.c

DMA_ChannelRequestEnable#

void DMA_ChannelRequestEnable (unsigned int channel, bool enable)

Enable or disable a DMA channel request.

Parameters
[in]channel

The DMA channel to enable or disable the request on.

[in]enable

If 'true', the request will be enabled. If 'false', the request will be disabled.

Use this function to enable or disable a DMA channel request. This will prevent the DMA from proceeding after its current transaction if disabled.


Definition at line 956 of file platform/emlib/src/em_dma.c

DMA_Init#

void DMA_Init (DMA_Init_TypeDef * init)

Initialize the DMA controller.

Parameters
[in]init

A pointer to a structure containing the DMA initialization information.

This function resets and prepares the DMA controller for use. Although it may be used several times, it is normally only used during system initialization. If reused during a normal operation, any ongoing DMA transfers will be aborted. When complete, the DMA controller is in an enabled state.

Note

  • Must be invoked before using the DMA controller.


Definition at line 984 of file platform/emlib/src/em_dma.c

DMA_RefreshPingPong#

void DMA_RefreshPingPong (unsigned int channel, bool primary, bool useBurst, void * dst, const void * src, unsigned int nMinus1, bool stop)

Refresh a descriptor used in a DMA ping-pong cycle.

Parameters
[in]channel

The DMA channel to refresh the ping-pong descriptor for.

[in]primary
  • true - refresh the primary descriptor

  • false - refresh an alternate descriptor

[in]useBurst

The burst feature is only used on peripherals supporting DMA bursts. Bursts must not be used if the total length (as given by nMinus1) is less than the arbitration rate configured for the descriptor. See the reference manual for more details on burst usage.

[in]dst

An address to a start location to transfer data to. If NULL, leave setting in descriptor as is.

[in]src

An address to a start location to transfer data from. If NULL, leave setting in descriptor as is.

[in]nMinus1

A number of DMA transfer elements (minus 1) to transfer (<= 1023). The size of the DMA transfer element (1, 2 or 4 bytes) is configured with DMA_CfgDescr().

[in]stop

Indicate that the DMA ping-pong cycle stops when done using this descriptor.

During a ping-pong DMA cycle, the DMA controller automatically alternates between the primary and alternate descriptors, when completing use of a descriptor. While the other descriptor is in use by the DMA controller, the software should refresh the completed descriptor. This is typically done from the callback defined for the ping-pong cycle.


Definition at line 1061 of file platform/emlib/src/em_dma.c

DMA_Reset#

void DMA_Reset (void )

Reset the DMA controller.

Parameters
N/A

This functions will disable the DMA controller and set it to a reset state.

Note

  • Note that any ongoing transfers will be aborted.


Definition at line 1135 of file platform/emlib/src/em_dma.c

DMA_ResetLoop#

void DMA_ResetLoop (unsigned int channel)

Clear Loop configuration for channel.

Parameters
[in]channel

Channel to reset loop configuration for.


Definition at line 373 of file platform/emlib/inc/em_dma.h

DMA_ResetRect#

void DMA_ResetRect (unsigned int channel)

Clear Rect/2D DMA configuration for channel.

Parameters
[in]channel

Channel to reset loop configuration for.


Definition at line 397 of file platform/emlib/inc/em_dma.h

DMA_IntClear#

void DMA_IntClear (uint32_t flags)

Clear one or more pending DMA interrupts.

Parameters
[in]flags

Pending DMA interrupt sources to clear. Use one or more valid interrupt flags for the DMA module (DMA_IFC_nnn).


Definition at line 430 of file platform/emlib/inc/em_dma.h

DMA_IntDisable#

void DMA_IntDisable (uint32_t flags)

Disable one or more DMA interrupts.

Parameters
[in]flags

DMA interrupt sources to disable. Use one or more valid interrupt flags for the DMA module (DMA_IEN_nnn).


Definition at line 443 of file platform/emlib/inc/em_dma.h

DMA_IntEnable#

void DMA_IntEnable (uint32_t flags)

Enable one or more DMA interrupts.

Parameters
[in]flags

DMA interrupt sources to enable. Use one or more valid interrupt flags for the DMA module (DMA_IEN_nnn).

Note

  • Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using DMA_IntClear() prior to enabling the interrupt.


Definition at line 461 of file platform/emlib/inc/em_dma.h

DMA_IntGet#

uint32_t DMA_IntGet (void )

Get pending DMA interrupt flags.

Parameters
N/A

Note

  • Event bits are not cleared by the use of this function.

Returns

  • DMA interrupt sources pending. Returns one or more valid interrupt flags for the DMA module (DMA_IF_nnn).


Definition at line 477 of file platform/emlib/inc/em_dma.h

DMA_IntGetEnabled#

uint32_t DMA_IntGetEnabled (void )

Get enabled and pending DMA interrupt flags.

Parameters
N/A

Useful for handling more interrupt sources in the same interrupt handler.

Note

  • Interrupt flags are not cleared by the use of this function.

Returns

  • Pending and enabled DMA interrupt sources Return value is the bitwise AND of

    • the enabled interrupt sources in DMA_IEN and

    • the pending interrupt flags DMA_IF.


Definition at line 496 of file platform/emlib/inc/em_dma.h

DMA_IntSet#

void DMA_IntSet (uint32_t flags)

Set one or more pending DMA interrupts.

Parameters
[in]flags

DMA interrupt sources to set to pending. Use one or more valid interrupt flags for the DMA module (DMA_IFS_nnn).


Definition at line 512 of file platform/emlib/inc/em_dma.h