USB HOST endpoint status data.

A host application should not manipulate the contents of this struct.

Public Attributes#

A SETUP package.

uint8_t

Error counter for SETUP transfers.

The device the endpoint belongs to.

uint8_t

Endpoint type.

uint16_t

Packet size, current transfer.

uint8_t

Host channel number assigned for OUT transfers.

uint8_t

Host channel number assigned for IN transfers.

bool

Endpoint direction.

uint8_t

Endpoint data toggle.

uint8_t

Endpoint address.

uint8_t *

Transfer buffer.

volatile bool

Transfer completion flag.

Transfer completion callback function.

uint32_t

Number of bytes transferred.

uint32_t

Number of bytes remaining.

uint32_t

Transfer timeout.

Public Attribute Documentation#

setup#

USB_Setup_TypeDef USBH_Ep_TypeDef::setup

A SETUP package.



setupErrCnt#

uint8_t USBH_Ep_TypeDef::setupErrCnt

Error counter for SETUP transfers.



epDesc#

USB_EndpointDescriptor_TypeDef USBH_Ep_TypeDef::epDesc

Endpoint descriptor.



parentDevice#

struct USBH_Device_TypeDef* USBH_Ep_TypeDef::parentDevice

The device the endpoint belongs to.



type#

uint8_t USBH_Ep_TypeDef::type

Endpoint type.



packetSize#

uint16_t USBH_Ep_TypeDef::packetSize

Packet size, current transfer.



hcOut#

uint8_t USBH_Ep_TypeDef::hcOut

Host channel number assigned for OUT transfers.



hcIn#

uint8_t USBH_Ep_TypeDef::hcIn

Host channel number assigned for IN transfers.



in#

bool USBH_Ep_TypeDef::in

Endpoint direction.



toggle#

uint8_t USBH_Ep_TypeDef::toggle

Endpoint data toggle.



state#

USBH_EpState_TypeDef USBH_Ep_TypeDef::state

Endpoint state.



addr#

uint8_t USBH_Ep_TypeDef::addr

Endpoint address.



buf#

uint8_t* USBH_Ep_TypeDef::buf

Transfer buffer.



xferCompleted#

volatile bool USBH_Ep_TypeDef::xferCompleted

Transfer completion flag.



xferStatus#

USB_Status_TypeDef USBH_Ep_TypeDef::xferStatus

Transfer status.



xferCompleteCb#

USB_XferCompleteCb_TypeDef USBH_Ep_TypeDef::xferCompleteCb

Transfer completion callback function.



xferred#

uint32_t USBH_Ep_TypeDef::xferred

Number of bytes transferred.



remaining#

uint32_t USBH_Ep_TypeDef::remaining

Number of bytes remaining.



timeout#

uint32_t USBH_Ep_TypeDef::timeout

Transfer timeout.