Authenticated encryption with associated data (AEAD)#

Functions#

psa_aead_encrypt(mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *nonce, size_t nonce_length, const uint8_t *additional_data, size_t additional_data_length, const uint8_t *plaintext, size_t plaintext_length, uint8_t *ciphertext, size_t ciphertext_size, size_t *ciphertext_length)

Process an authenticated encryption operation.

psa_aead_decrypt(mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t *nonce, size_t nonce_length, const uint8_t *additional_data, size_t additional_data_length, const uint8_t *ciphertext, size_t ciphertext_length, uint8_t *plaintext, size_t plaintext_size, size_t *plaintext_length)

Process an authenticated decryption operation.

psa_aead_operation_t

Return an initial value for an AEAD operation object.

psa_aead_encrypt_setup(psa_aead_operation_t *operation, mbedtls_svc_key_id_t key, psa_algorithm_t alg)

Set the key for a multipart authenticated encryption operation.

psa_aead_decrypt_setup(psa_aead_operation_t *operation, mbedtls_svc_key_id_t key, psa_algorithm_t alg)

Set the key for a multipart authenticated decryption operation.

psa_aead_generate_nonce(psa_aead_operation_t *operation, uint8_t *nonce, size_t nonce_size, size_t *nonce_length)

Generate a random nonce for an authenticated encryption operation.

psa_aead_set_nonce(psa_aead_operation_t *operation, const uint8_t *nonce, size_t nonce_length)

Set the nonce for an authenticated encryption or decryption operation.

psa_aead_set_lengths(psa_aead_operation_t *operation, size_t ad_length, size_t plaintext_length)

Declare the lengths of the message and additional data for AEAD.

psa_aead_update_ad(psa_aead_operation_t *operation, const uint8_t *input, size_t input_length)

Pass additional data to an active AEAD operation.

psa_aead_update(psa_aead_operation_t *operation, const uint8_t *input, size_t input_length, uint8_t *output, size_t output_size, size_t *output_length)

Encrypt or decrypt a message fragment in an active AEAD operation.

psa_aead_finish(psa_aead_operation_t *operation, uint8_t *ciphertext, size_t ciphertext_size, size_t *ciphertext_length, uint8_t *tag, size_t tag_size, size_t *tag_length)

Finish encrypting a message in an AEAD operation.

psa_aead_verify(psa_aead_operation_t *operation, uint8_t *plaintext, size_t plaintext_size, size_t *plaintext_length, const uint8_t *tag, size_t tag_length)

Finish authenticating and decrypting a message in an AEAD operation.

psa_aead_abort(psa_aead_operation_t *operation)

Abort an AEAD operation.

Function Documentation#

psa_aead_encrypt#

psa_status_t psa_aead_encrypt (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * nonce, size_t nonce_length, const uint8_t * additional_data, size_t additional_data_length, const uint8_t * plaintext, size_t plaintext_length, uint8_t * ciphertext, size_t ciphertext_size, size_t * ciphertext_length)

Process an authenticated encryption operation.

Parameters
N/Akey

Identifier of the key to use for the operation. It must allow the usage PSA_KEY_USAGE_ENCRYPT.

N/Aalg

The AEAD algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).

[in]nonce

Nonce or IV to use.

N/Anonce_length

Size of the nonce buffer in bytes.

[in]additional_data

Additional data that will be authenticated but not encrypted.

N/Aadditional_data_length

Size of additional_data in bytes.

[in]plaintext

Data that will be authenticated and encrypted.

N/Aplaintext_length

Size of plaintext in bytes.

[out]ciphertext

Output buffer for the authenticated and encrypted data. The additional data is not part of this output. For algorithms where the encrypted data and the authentication tag are defined as separate outputs, the authentication tag is appended to the encrypted data.

N/Aciphertext_size

Size of the ciphertext buffer in bytes. This must be appropriate for the selected algorithm and key:

  • A sufficient output size is #PSA_AEAD_ENCRYPT_OUTPUT_SIZE(key_type, alg, plaintext_length) where key_type is the type of key.

  • #PSA_AEAD_ENCRYPT_OUTPUT_MAX_SIZE(plaintext_length) evaluates to the maximum ciphertext size of any supported AEAD encryption.

[out]ciphertext_length

On success, the size of the output in the ciphertext buffer.


Definition at line 2108 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_decrypt#

psa_status_t psa_aead_decrypt (mbedtls_svc_key_id_t key, psa_algorithm_t alg, const uint8_t * nonce, size_t nonce_length, const uint8_t * additional_data, size_t additional_data_length, const uint8_t * ciphertext, size_t ciphertext_length, uint8_t * plaintext, size_t plaintext_size, size_t * plaintext_length)

Process an authenticated decryption operation.

Parameters
N/Akey

Identifier of the key to use for the operation. It must allow the usage PSA_KEY_USAGE_DECRYPT.

N/Aalg

The AEAD algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).

[in]nonce

Nonce or IV to use.

N/Anonce_length

Size of the nonce buffer in bytes.

[in]additional_data

Additional data that has been authenticated but not encrypted.

N/Aadditional_data_length

Size of additional_data in bytes.

[in]ciphertext

Data that has been authenticated and encrypted. For algorithms where the encrypted data and the authentication tag are defined as separate inputs, the buffer must contain the encrypted data followed by the authentication tag.

N/Aciphertext_length

Size of ciphertext in bytes.

[out]plaintext

Output buffer for the decrypted data.

N/Aplaintext_size

Size of the plaintext buffer in bytes. This must be appropriate for the selected algorithm and key:

  • A sufficient output size is #PSA_AEAD_DECRYPT_OUTPUT_SIZE(key_type, alg, ciphertext_length) where key_type is the type of key.

  • #PSA_AEAD_DECRYPT_OUTPUT_MAX_SIZE(ciphertext_length) evaluates to the maximum plaintext size of any supported AEAD decryption.

[out]plaintext_length

On success, the size of the output in the plaintext buffer.


Definition at line 2181 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_operation_init#

static psa_aead_operation_t psa_aead_operation_init (void )

Return an initial value for an AEAD operation object.

Parameters
N/A

Definition at line 2231 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_encrypt_setup#

psa_status_t psa_aead_encrypt_setup (psa_aead_operation_t * operation, mbedtls_svc_key_id_t key, psa_algorithm_t alg)

Set the key for a multipart authenticated encryption operation.

Parameters
[inout]operation

The operation object to set up. It must have been initialized as per the documentation for #psa_aead_operation_t and not yet in use.

N/Akey

Identifier of the key to use for the operation. It must remain valid until the operation terminates. It must allow the usage PSA_KEY_USAGE_ENCRYPT.

N/Aalg

The AEAD algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).

The sequence of operations to encrypt a message with authentication is as follows:

  1. Allocate an operation object which will be passed to all the functions listed here.

  2. Initialize the operation object with one of the methods described in the documentation for #psa_aead_operation_t, e.g. #PSA_AEAD_OPERATION_INIT.

  3. Call psa_aead_encrypt_setup() to specify the algorithm and key.

  4. If needed, call psa_aead_set_lengths() to specify the length of the inputs to the subsequent calls to psa_aead_update_ad() and psa_aead_update(). See the documentation of psa_aead_set_lengths() for details.

  5. Call either psa_aead_generate_nonce() or psa_aead_set_nonce() to generate or set the nonce. You should use psa_aead_generate_nonce() unless the protocol you are implementing requires a specific nonce value.

  6. Call psa_aead_update_ad() zero, one or more times, passing a fragment of the non-encrypted additional authenticated data each time.

  7. Call psa_aead_update() zero, one or more times, passing a fragment of the message to encrypt each time.

  8. Call psa_aead_finish().

If an error occurs at any step after a call to psa_aead_encrypt_setup(), the operation will need to be reset by a call to psa_aead_abort(). The application may call psa_aead_abort() at any time after the operation has been initialized.

After a successful call to psa_aead_encrypt_setup(), the application must eventually terminate the operation. The following events terminate an operation:


Definition at line 2299 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_decrypt_setup#

psa_status_t psa_aead_decrypt_setup (psa_aead_operation_t * operation, mbedtls_svc_key_id_t key, psa_algorithm_t alg)

Set the key for a multipart authenticated decryption operation.

Parameters
[inout]operation

The operation object to set up. It must have been initialized as per the documentation for #psa_aead_operation_t and not yet in use.

N/Akey

Identifier of the key to use for the operation. It must remain valid until the operation terminates. It must allow the usage PSA_KEY_USAGE_DECRYPT.

N/Aalg

The AEAD algorithm to compute (PSA_ALG_XXX value such that PSA_ALG_IS_AEAD(alg) is true).

The sequence of operations to decrypt a message with authentication is as follows:

  1. Allocate an operation object which will be passed to all the functions listed here.

  2. Initialize the operation object with one of the methods described in the documentation for #psa_aead_operation_t, e.g. #PSA_AEAD_OPERATION_INIT.

  3. Call psa_aead_decrypt_setup() to specify the algorithm and key.

  4. If needed, call psa_aead_set_lengths() to specify the length of the inputs to the subsequent calls to psa_aead_update_ad() and psa_aead_update(). See the documentation of psa_aead_set_lengths() for details.

  5. Call psa_aead_set_nonce() with the nonce for the decryption.

  6. Call psa_aead_update_ad() zero, one or more times, passing a fragment of the non-encrypted additional authenticated data each time.

  7. Call psa_aead_update() zero, one or more times, passing a fragment of the ciphertext to decrypt each time.

  8. Call psa_aead_verify().

If an error occurs at any step after a call to psa_aead_decrypt_setup(), the operation will need to be reset by a call to psa_aead_abort(). The application may call psa_aead_abort() at any time after the operation has been initialized.

After a successful call to psa_aead_decrypt_setup(), the application must eventually terminate the operation. The following events terminate an operation:


Definition at line 2365 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_generate_nonce#

psa_status_t psa_aead_generate_nonce (psa_aead_operation_t * operation, uint8_t * nonce, size_t nonce_size, size_t * nonce_length)

Generate a random nonce for an authenticated encryption operation.

Parameters
[inout]operation

Active AEAD operation.

[out]nonce

Buffer where the generated nonce is to be written.

N/Anonce_size

Size of the nonce buffer in bytes.

[out]nonce_length

On success, the number of bytes of the generated nonce.

This function generates a random nonce for the authenticated encryption operation with an appropriate size for the chosen algorithm, key type and key size.

The application must call psa_aead_encrypt_setup() before calling this function.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().


Definition at line 2404 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_set_nonce#

psa_status_t psa_aead_set_nonce (psa_aead_operation_t * operation, const uint8_t * nonce, size_t nonce_length)

Set the nonce for an authenticated encryption or decryption operation.

Parameters
[inout]operation

Active AEAD operation.

[in]nonce

Buffer containing the nonce to use.

N/Anonce_length

Size of the nonce in bytes.

This function sets the nonce for the authenticated encryption or decryption operation.

The application must call psa_aead_encrypt_setup() or psa_aead_decrypt_setup() before calling this function.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().

Note

  • When encrypting, applications should use psa_aead_generate_nonce() instead of this function, unless implementing a protocol that requires a non-random IV.


Definition at line 2444 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_set_lengths#

psa_status_t psa_aead_set_lengths (psa_aead_operation_t * operation, size_t ad_length, size_t plaintext_length)

Declare the lengths of the message and additional data for AEAD.

Parameters
[inout]operation

Active AEAD operation.

N/Aad_length

Size of the non-encrypted additional authenticated data in bytes.

N/Aplaintext_length

Size of the plaintext to encrypt in bytes.

The application must call this function before calling psa_aead_update_ad() or psa_aead_update() if the algorithm for the operation requires it. If the algorithm does not require it, calling this function is optional, but if this function is called then the implementation must enforce the lengths.

You may call this function before or after setting the nonce with psa_aead_set_nonce() or psa_aead_generate_nonce().

  • For PSA_ALG_CCM, calling this function is required.

  • For the other AEAD algorithms defined in this specification, calling this function is not required.

  • For vendor-defined algorithm, refer to the vendor documentation.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().


Definition at line 2489 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_update_ad#

psa_status_t psa_aead_update_ad (psa_aead_operation_t * operation, const uint8_t * input, size_t input_length)

Pass additional data to an active AEAD operation.

Parameters
[inout]operation

Active AEAD operation.

[in]input

Buffer containing the fragment of additional data.

N/Ainput_length

Size of the input buffer in bytes.

Additional data is authenticated, but not encrypted.

You may call this function multiple times to pass successive fragments of the additional data. You may not call this function after passing data to encrypt or decrypt with psa_aead_update().

Before calling this function, you must:

  1. Call either psa_aead_encrypt_setup() or psa_aead_decrypt_setup().

  2. Set the nonce with psa_aead_generate_nonce() or psa_aead_set_nonce().

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().

Warnings


Definition at line 2537 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_update#

psa_status_t psa_aead_update (psa_aead_operation_t * operation, const uint8_t * input, size_t input_length, uint8_t * output, size_t output_size, size_t * output_length)

Encrypt or decrypt a message fragment in an active AEAD operation.

Parameters
[inout]operation

Active AEAD operation.

[in]input

Buffer containing the message fragment to encrypt or decrypt.

N/Ainput_length

Size of the input buffer in bytes.

[out]output

Buffer where the output is to be written.

N/Aoutput_size

Size of the output buffer in bytes. This must be appropriate for the selected algorithm and key:

  • A sufficient output size is #PSA_AEAD_UPDATE_OUTPUT_SIZE(key_type, alg, input_length) where key_type is the type of key and alg is the algorithm that were used to set up the operation.

  • #PSA_AEAD_UPDATE_OUTPUT_MAX_SIZE(input_length) evaluates to the maximum output size of any supported AEAD algorithm.

[out]output_length

On success, the number of bytes that make up the returned output.

Before calling this function, you must:

  1. Call either psa_aead_encrypt_setup() or psa_aead_decrypt_setup(). The choice of setup function determines whether this function encrypts or decrypts its input.

  2. Set the nonce with psa_aead_generate_nonce() or psa_aead_set_nonce().

  3. Call psa_aead_update_ad() to pass all the additional data.

If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().

Warnings

  • When decrypting, until psa_aead_verify() has returned PSA_SUCCESS, there is no guarantee that the input is valid. Therefore, until you have called psa_aead_verify() and it has returned PSA_SUCCESS:

    • Do not use the output in any way other than storing it in a confidential location. If you take any action that depends on the tentative decrypted data, this action will need to be undone if the input turns out not to be valid. Furthermore, if an adversary can observe that this action took place (for example through timing), they may be able to use this fact as an oracle to decrypt any message encrypted with the same key.

    • In particular, do not copy the output anywhere but to a memory or storage space that you have exclusive access to.

This function does not require the input to be aligned to any particular block boundary. If the implementation can only process a whole block at a time, it must consume all the input provided, but it may delay the end of the corresponding output until a subsequent call to psa_aead_update(), psa_aead_finish() or psa_aead_verify() provides sufficient input. The amount of data that can be delayed in this way is bounded by #PSA_AEAD_UPDATE_OUTPUT_SIZE.


Definition at line 2621 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_finish#

psa_status_t psa_aead_finish (psa_aead_operation_t * operation, uint8_t * ciphertext, size_t ciphertext_size, size_t * ciphertext_length, uint8_t * tag, size_t tag_size, size_t * tag_length)

Finish encrypting a message in an AEAD operation.

Parameters
[inout]operation

Active AEAD operation.

[out]ciphertext

Buffer where the last part of the ciphertext is to be written.

N/Aciphertext_size

Size of the ciphertext buffer in bytes. This must be appropriate for the selected algorithm and key:

  • A sufficient output size is #PSA_AEAD_FINISH_OUTPUT_SIZE(key_type, alg) where key_type is the type of key and alg is the algorithm that were used to set up the operation.

  • #PSA_AEAD_FINISH_OUTPUT_MAX_SIZE evaluates to the maximum output size of any supported AEAD algorithm.

[out]ciphertext_length

On success, the number of bytes of returned ciphertext.

[out]tag

Buffer where the authentication tag is to be written.

N/Atag_size

Size of the tag buffer in bytes. This must be appropriate for the selected algorithm and key:

  • The exact tag size is #PSA_AEAD_TAG_LENGTH(key_type, key_bits, alg) where key_type and key_bits are the type and bit-size of the key, and alg is the algorithm that were used in the call to psa_aead_encrypt_setup().

  • #PSA_AEAD_TAG_MAX_SIZE evaluates to the maximum tag size of any supported AEAD algorithm.

[out]tag_length

On success, the number of bytes that make up the returned tag.

The operation must have been set up with psa_aead_encrypt_setup().

This function finishes the authentication of the additional data formed by concatenating the inputs passed to preceding calls to psa_aead_update_ad() with the plaintext formed by concatenating the inputs passed to preceding calls to psa_aead_update().

This function has two output buffers:

  • ciphertext contains trailing ciphertext that was buffered from preceding calls to psa_aead_update().

  • tag contains the authentication tag.

When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().


Definition at line 2707 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_verify#

psa_status_t psa_aead_verify (psa_aead_operation_t * operation, uint8_t * plaintext, size_t plaintext_size, size_t * plaintext_length, const uint8_t * tag, size_t tag_length)

Finish authenticating and decrypting a message in an AEAD operation.

Parameters
[inout]operation

Active AEAD operation.

[out]plaintext

Buffer where the last part of the plaintext is to be written. This is the remaining data from previous calls to psa_aead_update() that could not be processed until the end of the input.

N/Aplaintext_size

Size of the plaintext buffer in bytes. This must be appropriate for the selected algorithm and key:

  • A sufficient output size is #PSA_AEAD_VERIFY_OUTPUT_SIZE(key_type, alg) where key_type is the type of key and alg is the algorithm that were used to set up the operation.

  • #PSA_AEAD_VERIFY_OUTPUT_MAX_SIZE evaluates to the maximum output size of any supported AEAD algorithm.

[out]plaintext_length

On success, the number of bytes of returned plaintext.

[in]tag

Buffer containing the authentication tag.

N/Atag_length

Size of the tag buffer in bytes.

The operation must have been set up with psa_aead_decrypt_setup().

This function finishes the authenticated decryption of the message components:

  • The additional data consisting of the concatenation of the inputs passed to preceding calls to psa_aead_update_ad().

  • The ciphertext consisting of the concatenation of the inputs passed to preceding calls to psa_aead_update().

  • The tag passed to this function call.

If the authentication tag is correct, this function outputs any remaining plaintext and reports success. If the authentication tag is not correct, this function returns PSA_ERROR_INVALID_SIGNATURE.

When this function returns successfully, the operation becomes inactive. If this function returns an error status, the operation enters an error state and must be aborted by calling psa_aead_abort().

Note

  • Implementations shall make the best effort to ensure that the comparison between the actual tag and the expected tag is performed in constant time.


Definition at line 2790 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h

psa_aead_abort#

psa_status_t psa_aead_abort (psa_aead_operation_t * operation)

Abort an AEAD operation.

Parameters
[inout]operation

Initialized AEAD operation.

Aborting an operation frees all associated resources except for the operation structure itself. Once aborted, the operation object can be reused for another operation by calling psa_aead_encrypt_setup() or psa_aead_decrypt_setup() again.

You may call this function any time after the operation object has been initialized as described in #psa_aead_operation_t.

In particular, calling psa_aead_abort() after the operation has been terminated by a call to psa_aead_abort(), psa_aead_finish() or psa_aead_verify() is safe and has no effect.


Definition at line 2822 of file util/third_party/trusted-firmware-m/interface/include/psa/crypto.h