TIMER Dead Time Insertion (DTI) initialization structure.

Public Attributes#

bool

Enable DTI or leave it disabled until TIMER_EnableDTI() is called.

bool

DTI Output Polarity.

bool

DTI Complementary Output Invert.

bool

Enable Automatic Start-up functionality (when debugger exits).

bool

Enable/disable PRS as DTI input.

Select which PRS channel as DTI input.

DTI prescaling factor, if HFPER / HFPERB clock used.

unsigned int

DTI Rise Time.

unsigned int

DTI Fall Time.

uint32_t

DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2.

bool

Enable core lockup as a fault source.

bool

Enable debugger as a fault source.

bool

Enable PRS fault source 0 (faultSourcePrsSel0).

Select which PRS signal to be PRS fault source 0.

bool

Enable PRS fault source 1 (faultSourcePrsSel1).

Select which PRS signal to be PRS fault source 1.

Public Attribute Documentation#

enable#

bool TIMER_InitDTI_TypeDef::enable

Enable DTI or leave it disabled until TIMER_EnableDTI() is called.


activeLowOut#

bool TIMER_InitDTI_TypeDef::activeLowOut

DTI Output Polarity.


invertComplementaryOut#

bool TIMER_InitDTI_TypeDef::invertComplementaryOut

DTI Complementary Output Invert.


autoRestart#

bool TIMER_InitDTI_TypeDef::autoRestart

Enable Automatic Start-up functionality (when debugger exits).


enablePrsSource#

bool TIMER_InitDTI_TypeDef::enablePrsSource

Enable/disable PRS as DTI input.


prsSel#

TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::prsSel

Select which PRS channel as DTI input.

Only valid if enablePrsSource is enabled.


prescale#

TIMER_Prescale_TypeDef TIMER_InitDTI_TypeDef::prescale

DTI prescaling factor, if HFPER / HFPERB clock used.


riseTime#

unsigned int TIMER_InitDTI_TypeDef::riseTime

DTI Rise Time.


fallTime#

unsigned int TIMER_InitDTI_TypeDef::fallTime

DTI Fall Time.


outputsEnableMask#

uint32_t TIMER_InitDTI_TypeDef::outputsEnableMask

DTI outputs enable bit mask, consisting of one bit per DTI output signal, i.e., CC0, CC1, CC2, CDTI0, CDTI1, and CDTI2.

This value should consist of one or more TIMER_DTOGEN_DTOGnnnEN flags (defined in <part_name>_timer.h) OR'ed together.


enableFaultSourceCoreLockup#

bool TIMER_InitDTI_TypeDef::enableFaultSourceCoreLockup

Enable core lockup as a fault source.


enableFaultSourceDebugger#

bool TIMER_InitDTI_TypeDef::enableFaultSourceDebugger

Enable debugger as a fault source.


enableFaultSourcePrsSel0#

bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel0

Enable PRS fault source 0 (faultSourcePrsSel0).


faultSourcePrsSel0#

TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel0

Select which PRS signal to be PRS fault source 0.


enableFaultSourcePrsSel1#

bool TIMER_InitDTI_TypeDef::enableFaultSourcePrsSel1

Enable PRS fault source 1 (faultSourcePrsSel1).


faultSourcePrsSel1#

TIMER_PRSSEL_TypeDef TIMER_InitDTI_TypeDef::faultSourcePrsSel1

Select which PRS signal to be PRS fault source 1.


faultAction#

TIMER_DtiFaultAction_TypeDef TIMER_InitDTI_TypeDef::faultAction

Fault Action.