RMU - Reset Management Unit#

Reset Management Unit (RMU) Peripheral API.

This module contains functions to control the RMU peripheral of Silicon Labs 32-bit MCUs and SoCs. RMU ensures correct reset operation and is responsible for connecting the different reset sources to the reset lines of the MCU or SoC.

Enumerations#

enum
rmuResetModeClear = 0
rmuResetModeSet = 1
}

RMU reset modes.

enum
rmuResetBU = _RMU_CTRL_BURSTEN_MASK
rmuResetLockUp = _RMU_CTRL_LOCKUPRDIS_MASK
}

RMU controlled peripheral reset control and reset source control.

Functions#

void
RMU_ResetControl(RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode)

Disable/enable reset for various peripherals and signal sources.

void

Clear the reset cause register.

uint32_t

Get the cause of the last reset.

Macros#

#define
RMU_LockupResetDisable (A)

RMU_LockupResetDisable kept for backwards compatibility.

Enumeration Documentation#

RMU_ResetMode_TypeDef#

RMU_ResetMode_TypeDef

RMU reset modes.

Enumerator
rmuResetModeClear

Reset mode clear.

rmuResetModeSet

Reset mode set.


Definition at line 54 of file platform/emlib/inc/em_rmu.h

RMU_Reset_TypeDef#

RMU_Reset_TypeDef

RMU controlled peripheral reset control and reset source control.

Enumerator
rmuResetBU

Reset control over Backup Power domain select.

rmuResetLockUp

Cortex lockup reset select.


Definition at line 70 of file platform/emlib/inc/em_rmu.h

Function Documentation#

RMU_ResetControl#

void RMU_ResetControl (RMU_Reset_TypeDef reset, RMU_ResetMode_TypeDef mode)

Disable/enable reset for various peripherals and signal sources.

Parameters
[in]reset

Reset types to enable/disable.s

[in]mode

Reset mode.


Definition at line 244 of file platform/emlib/src/em_rmu.c

RMU_ResetCauseClear#

void RMU_ResetCauseClear (void )

Clear the reset cause register.

Parameters
N/A

This function clears all the reset cause bits of the RSTCAUSE register. The reset cause bits must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseGet().


Definition at line 276 of file platform/emlib/src/em_rmu.c

RMU_ResetCauseGet#

uint32_t RMU_ResetCauseGet (void )

Get the cause of the last reset.

Parameters
N/A

To be useful, the reset cause must be cleared by software before a new reset occurs. Otherwise, reset causes may accumulate. See RMU_ResetCauseClear(). This function call will return the main cause for reset, which can be a bit mask (several causes) and clear away "noise".

Returns

  • A reset cause mask. See the reference manual for a description of the reset cause mask.


Definition at line 319 of file platform/emlib/src/em_rmu.c