EUSART - Extended USART#

Extended Universal Synchronous/Asynchronous Receiver/Transmitter.


Introduction#

This module contains functions to control the Enhanced Universal Synchronous / Asynchronous Receiver / Transmitter controller(s) (EUSART) peripheral of Silicon Labs' 32-bit MCUs and SoCs. EUSART can be used as a UART and can, therefore, be connected to an external transceiver to communicate with another host using the serial link.

It supports full duplex asynchronous UART communication as well as RS-485, SPI, MicroWire, and 3-wire. It can also interface with ISO7816 Smart-Cards, and IrDA devices.

EUSART has a wide selection of operating modes, frame formats, and baud rates. All features are supported through the API of this module.

This module does not support DMA configuration. UARTDRV and SPIDRV drivers provide full support for DMA and more.


Example#

EUSART Async TX example:

{
  EUSART_UartInit_TypeDef init = EUSART_UART_INIT_DEFAULT_HF;

  // Configure the clocks.
  CMU_ClockSelectSet(cmuClock_EUSART0CLK, cmuSelect_EM01GRPCCLK);
  CMU_ClockEnable(cmuClock_EUSART0CLK, true);
  // Initialize the EUSART
  EUSART_UartInitHf(EUSART0, &init);
  EUSART_Tx(EUSART0, data);
}

EUSART Sync SPI Transaction example:

{
  EUSART_SpiInit_TypeDef init_master = EUSART_SPI_MASTER_INIT_DEFAULT_HF;

  // Configure the clocks.
  CMU_ClockSelectSet(cmuClock_EM01GRPCCLK, cmuSelect_HFRCODPLL);
  CMU_ClockEnable(cmuClock_EUSART1, true);
  CMU_ClockEnable(cmuClock_GPIO, true);

  //Configure the SPI ports
  GPIO_PinModeSet(sclk_port, sclk_pin, gpioModePushPull, 0);
  GPIO_PinModeSet(mosi_port, mosi_pin, gpioModePushPull, 0);
  GPIO_PinModeSet(mosi_port, miso_pin, gpioModeInput, 0);

  // Connect EUSART to ports
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].TXROUTE = (mosi_port << _GPIO_EUSART_TXROUTE_PORT_SHIFT)
                                                   | (mosi_pin << _GPIO_EUSART_TXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].RXROUTE = (miso_port << _GPIO_EUSART_RXROUTE_PORT_SHIFT)
                                                   | (miso_pin << _GPIO_EUSART_RXROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].SCLKROUTE = (sclk_port << _GPIO_EUSART_SCLKROUTE_PORT_SHIFT)
                                                   | (sclk_pin << _GPIO_EUSART_SCLKROUTE_PIN_SHIFT);
  GPIO->EUSARTROUTE[EUSART_NUM(EUSART1)].ROUTEEN = GPIO_EUSART_ROUTEEN_TXPEN | GPIO_EUSART_ROUTEEN_SCLKPEN;

  // Initialize the EUSART
  EUSART_SpiInit(EUSART1, &init_master);
  EUSART_Spi_TxRx(EUSART1, data);
}


EM2 guidelines for non EM2-Capable instances#

Note

  • EUSART instances located in the PD1 power domain are non EM2-capable. The EUSART_EM2_CAPABLE() and EUSART_NOT_EM2_CAPABLE() macros can be used to determine whether or not a EUSART instance is EM2-Capable.

Follow theses steps when entering in EM2:

  1. Wait for the current transaction to complete with TXCIF interrupt

  2. Disable TX and RX using TXDIS and RXDIS cmd

  3. Poll for EUSARTn_SYNCBUSY.TXDIS and EUSARTn_SYNCBUSY.RXDIS to go low

  4. Wait for EUSARTn_STATUS.TXENS and EUSARTn_STATUS.RXENS to go low

  5. Disable SCLKPEN and CSPEN in GPIO if they were previously enabled

  6. Enter EM2

On wakeup from EM2, EUSART transmitter/receiver and relevant GPIO (SCLKPEN and CSPEN) must be re-enabled. For example:

{
  // Enable TX and RX
  EUSART_Enable(EUSART0, eusartEnable);
  BUS_RegMaskedWrite(&GPIO->EUSARTROUTE[EUSART_NUM(EUSART0)].ROUTEEN,
                     _GPIO_EUSART_ROUTEEN_TXPEN_MASK | _GPIO_EUSART_ROUTEEN_SCLKPEN_MASK,
                     GPIO_EUSART_ROUTEEN_TXPEN | GPIO_EUSART_ROUTEEN_SCLKPEN);
}

Modules#

EUSART_AdvancedInit_TypeDef

EUSART_UartInit_TypeDef

EUSART_IrDAInit_TypeDef

EUSART_PrsTriggerInit_TypeDef

EUSART_DaliInit_TypeDef

Enumerations#

enum
eusartDisable = 0x0
eusartEnableRx = (EUSART_CMD_RXEN | EUSART_CMD_TXDIS)
eusartEnableTx = (EUSART_CMD_TXEN | EUSART_CMD_RXDIS)
eusartEnable = (EUSART_CMD_RXEN | EUSART_CMD_TXEN)
}

Enable selection.

enum
eusartDataBits7 = EUSART_FRAMECFG_DATABITS_SEVEN
eusartDataBits8 = EUSART_FRAMECFG_DATABITS_EIGHT
eusartDataBits9 = EUSART_FRAMECFG_DATABITS_NINE
}

Data bit selection.

enum
eusartNoParity = EUSART_FRAMECFG_PARITY_NONE
eusartEvenParity = EUSART_FRAMECFG_PARITY_EVEN
eusartOddParity = EUSART_FRAMECFG_PARITY_ODD
}

Parity selection.

enum
eusartStopbits0p5 = EUSART_FRAMECFG_STOPBITS_HALF
eusartStopbits1p5 = EUSART_FRAMECFG_STOPBITS_ONEANDAHALF
eusartStopbits1 = EUSART_FRAMECFG_STOPBITS_ONE
eusartStopbits2 = EUSART_FRAMECFG_STOPBITS_TWO
}

Stop bits selection.

enum
eusartOVS16 = EUSART_CFG0_OVS_X16
eusartOVS8 = EUSART_CFG0_OVS_X8
eusartOVS6 = EUSART_CFG0_OVS_X6
eusartOVS4 = EUSART_CFG0_OVS_X4
eusartOVS0 = EUSART_CFG0_OVS_DISABLE
}

Oversampling selection, used for asynchronous operation.

enum
eusartHwFlowControlNone = 0
eusartHwFlowControlCts
eusartHwFlowControlRts
eusartHwFlowControlCtsAndRts
}

HW flow control config.

enum
eusartLoopbackEnable = EUSART_CFG0_LOOPBK
eusartLoopbackDisable = _EUSART_CFG0_RESETVALUE
}

Loopback enable.

enum
eusartMajorityVoteEnable = EUSART_CFG0_MVDIS_DEFAULT
eusartMajorityVoteDisable = EUSART_CFG0_MVDIS
}

Majority vote enable.

enum
eusartBlockRxEnable = EUSART_CMD_RXBLOCKEN
eusartBlockRxDisable = EUSART_CMD_RXBLOCKDIS
}

Block reception enable.

enum
eusartTristateTxEnable = EUSART_CMD_TXTRIEN
eusartTristateTxDisable = EUSART_CMD_TXTRIDIS
}

TX output tristate enable.

enum
eusartIrDARxFilterEnable = EUSART_IRHFCFG_IRHFFILT_ENABLE
eusartIrDARxFilterDisable = EUSART_IRHFCFG_IRHFFILT_DISABLE
}

IrDA filter enable.

enum
eusartIrDAPulseWidthOne = EUSART_IRHFCFG_IRHFPW_ONE
eusartIrDAPulseWidthTwo = EUSART_IRHFCFG_IRHFPW_TWO
eusartIrDAPulseWidthThree = EUSART_IRHFCFG_IRHFPW_THREE
eusartIrDAPulseWidthFour = EUSART_IRHFCFG_IRHFPW_FOUR
}

Pulse width selection for IrDA mode.

enum
eusartPrsTriggerDisable = 0x0
eusartPrsTriggerEnableRx = EUSART_TRIGCTRL_RXTEN
eusartPrsTriggerEnableTx = EUSART_TRIGCTRL_TXTEN
eusartPrsTriggerEnableRxTx = (EUSART_TRIGCTRL_RXTEN | EUSART_TRIGCTRL_TXTEN)
}

PRS trigger enable.

enum
eusartInvertIODisable = (EUSART_CFG0_RXINV_DISABLE | EUSART_CFG0_TXINV_DISABLE)
eusartInvertRxEnable = EUSART_CFG0_RXINV_ENABLE
eusartInvertTxEnable = EUSART_CFG0_TXINV_ENABLE
eusartInvertIOEnable = (EUSART_CFG0_RXINV_ENABLE | EUSART_CFG0_TXINV_ENABLE)
}

IO polarity selection.

enum
eusartAutoTxDelayNone = EUSART_TIMINGCFG_TXDELAY_NONE
eusartAutoTxDelaySingle = EUSART_TIMINGCFG_TXDELAY_SINGLE
eusartAutoTxDelayDouble = EUSART_TIMINGCFG_TXDELAY_DOUBLE
eusartAutoTxDelayTripple = EUSART_TIMINGCFG_TXDELAY_TRIPPLE
}

Auto TX delay transmission.

enum
eusartRxFiFoWatermark1Frame = EUSART_CFG1_RXFIW_ONEFRAME
eusartRxFiFoWatermark2Frame = EUSART_CFG1_RXFIW_TWOFRAMES
eusartRxFiFoWatermark3Frame = EUSART_CFG1_RXFIW_THREEFRAMES
eusartRxFiFoWatermark4Frame = EUSART_CFG1_RXFIW_FOURFRAMES
}

RX FIFO Interrupt ans Status Watermark.

enum
eusartTxFiFoWatermark1Frame = EUSART_CFG1_TXFIW_ONEFRAME
eusartTxFiFoWatermark2Frame = EUSART_CFG1_TXFIW_TWOFRAMES
eusartTxFiFoWatermark3Frame = EUSART_CFG1_TXFIW_THREEFRAMES
eusartTxFiFoWatermark4Frame = EUSART_CFG1_TXFIW_FOURFRAMES
}

TX FIFO Interrupt and Status Watermark.

Typedefs#

typedef uint8_t

PRS Channel type.

Functions#

void
EUSART_UartInitHf(EUSART_TypeDef *eusart, const EUSART_UartInit_TypeDef *init)

Initialize EUSART when used in UART mode with the high frequency clock.

void
EUSART_UartInitLf(EUSART_TypeDef *eusart, const EUSART_UartInit_TypeDef *init)

Initialize EUSART when used in UART mode with the low frequency clock.

void
EUSART_IrDAInit(EUSART_TypeDef *eusart, const EUSART_IrDAInit_TypeDef *irdaInit)

Initialize EUSART when used in IrDA mode with the high or low frequency clock.

void
EUSART_Reset(EUSART_TypeDef *eusart)

Configure EUSART to its reset state.

void
EUSART_Enable(EUSART_TypeDef *eusart, EUSART_Enable_TypeDef enable)

Enable/disable EUSART receiver and/or transmitter.

uint8_t
EUSART_Rx(EUSART_TypeDef *eusart)

Receive one 8 bit frame, (or part of 9 bit frame).

uint16_t
EUSART_RxExt(EUSART_TypeDef *eusart)

Receive one 8-16 bit frame with extended information.

void
EUSART_Tx(EUSART_TypeDef *eusart, uint8_t data)

Transmit one frame.

void
EUSART_TxExt(EUSART_TypeDef *eusart, uint16_t data)

Transmit one 8-9 bit frame with extended control.

void
EUSART_BaudrateSet(EUSART_TypeDef *eusart, uint32_t refFreq, uint32_t baudrate)

Configure the baudrate (or as close as possible to a specified baudrate).

uint32_t
EUSART_BaudrateGet(EUSART_TypeDef *eusart)

Get the current baudrate.

void
EUSART_RxBlock(EUSART_TypeDef *eusart, EUSART_BlockRx_TypeDef enable)

Enable/Disable reception operation until the configured start frame is received.

void
EUSART_TxTristateSet(EUSART_TypeDef *eusart, EUSART_TristateTx_TypeDef enable)

Enable/Disable the tristating of the transmitter output.

void
EUSART_PrsTriggerEnable(EUSART_TypeDef *eusart, const EUSART_PrsTriggerInit_TypeDef *init)

Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.

uint32_t
EUSART_StatusGet(EUSART_TypeDef *eusart)

Get EUSART STATUS register.

void
EUSART_IntClear(EUSART_TypeDef *eusart, uint32_t flags)

Clear one or more pending EUSART interrupts.

void
EUSART_IntDisable(EUSART_TypeDef *eusart, uint32_t flags)

Disable one or more EUSART interrupts.

void
EUSART_IntEnable(EUSART_TypeDef *eusart, uint32_t flags)

Enable one or more EUSART interrupts.

uint32_t
EUSART_IntGet(EUSART_TypeDef *eusart)

Get pending EUSART interrupt flags.

uint32_t
EUSART_IntGetEnabled(EUSART_TypeDef *eusart)

Get enabled and pending EUSART interrupt flags.

void
EUSART_IntSet(EUSART_TypeDef *eusart, uint32_t flags)

Set one or more pending EUSART interrupts from SW.

Macros#

#define
EUSART0_FIFO_DEPTH 4

Define EUSART FIFO Depth information.

#define
EUSART1_FIFO_DEPTH EUSART0_FIFO_DEPTH
#define
EUSART2_FIFO_DEPTH EUSART0_FIFO_DEPTH
#define
EUSART3_FIFO_DEPTH EUSART0_FIFO_DEPTH
#define
EUSART4_FIFO_DEPTH EUSART0_FIFO_DEPTH
#define
EUSART_FIFO_DEPTH (n)
#define
EUSART_UART_INIT_DEFAULT_HF undefined

Default configuration for EUSART initialization structure in UART mode with high-frequency clock.

#define
EUSART_DEFAULT_START_FRAME 0x00u

Default start frame configuration, i.e. feature disabled.

#define
EUSART_ADVANCED_INIT_DEFAULT undefined

Default configuration for EUSART advanced initialization structure.

#define
EUSART_UART_INIT_DEFAULT_LF undefined

Default configuration for EUSART initialization structure in UART mode with low-frequency clock.

#define
EUSART_IRDA_INIT_DEFAULT_HF undefined

Default configuration for EUSART initialization structure in IrDA mode with high-frequency clock.

#define
EUSART_IRDA_INIT_DEFAULT_LF undefined

Default configuration for EUSART initialization structure in IrDA mode with low-frequency clock.

Enumeration Documentation#

EUSART_Enable_TypeDef#

EUSART_Enable_TypeDef

Enable selection.

Enumerator
eusartDisable

Disable the peripheral.

eusartEnableRx

Enable receiver only, transmitter disabled.

eusartEnableTx

Enable transmitter only, receiver disabled.

eusartEnable

Enable both receiver and transmitter.


Definition at line 176 of file platform/emlib/inc/em_eusart.h

EUSART_Databits_TypeDef#

EUSART_Databits_TypeDef

Data bit selection.

Enumerator
eusartDataBits7

7 data bits.

eusartDataBits8

8 data bits.

eusartDataBits9

9 data bits.


Definition at line 191 of file platform/emlib/inc/em_eusart.h

EUSART_Parity_TypeDef#

EUSART_Parity_TypeDef

Parity selection.

Enumerator
eusartNoParity

No parity.

eusartEvenParity

Even parity.

eusartOddParity

Odd parity.


Definition at line 207 of file platform/emlib/inc/em_eusart.h

EUSART_Stopbits_TypeDef#

EUSART_Stopbits_TypeDef

Stop bits selection.

Enumerator
eusartStopbits0p5

0.5 stop bits.

eusartStopbits1p5

1.5 stop bits.

eusartStopbits1

1 stop bits.

eusartStopbits2

2 stop bits.


Definition at line 214 of file platform/emlib/inc/em_eusart.h

EUSART_OVS_TypeDef#

EUSART_OVS_TypeDef

Oversampling selection, used for asynchronous operation.

Enumerator
eusartOVS16

16x oversampling (normal).

eusartOVS8

8x oversampling.

eusartOVS6

6x oversampling.

eusartOVS4

4x oversampling.

eusartOVS0

Oversampling disabled.


Definition at line 222 of file platform/emlib/inc/em_eusart.h

EUSART_HwFlowControl_TypeDef#

EUSART_HwFlowControl_TypeDef

HW flow control config.

Enumerator
eusartHwFlowControlNone

No HW Flow Control.

eusartHwFlowControlCts

CTS HW Flow Control.

eusartHwFlowControlRts

RTS HW Flow Control.

eusartHwFlowControlCtsAndRts

CTS and RTS HW Flow Control.


Definition at line 231 of file platform/emlib/inc/em_eusart.h

EUSART_LoopbackEnable_TypeDef#

EUSART_LoopbackEnable_TypeDef

Loopback enable.

Enumerator
eusartLoopbackEnable

Enable loopback.

eusartLoopbackDisable

Disable loopback.


Definition at line 239 of file platform/emlib/inc/em_eusart.h

EUSART_MajorityVote_TypeDef#

EUSART_MajorityVote_TypeDef

Majority vote enable.

Enumerator
eusartMajorityVoteEnable

Enable majority vote for 16x, 8x and 6x oversampling modes.

eusartMajorityVoteDisable

Disable majority vote for 16x, 8x and 6x oversampling modes.


Definition at line 245 of file platform/emlib/inc/em_eusart.h

EUSART_BlockRx_TypeDef#

EUSART_BlockRx_TypeDef

Block reception enable.

Enumerator
eusartBlockRxEnable

Block reception enable, resulting in all incoming frames being discarded.

eusartBlockRxDisable

Block reception disable, resulting in all incoming frames being loaded into the RX FIFO.


Definition at line 251 of file platform/emlib/inc/em_eusart.h

EUSART_TristateTx_TypeDef#

EUSART_TristateTx_TypeDef

TX output tristate enable.

Enumerator
eusartTristateTxEnable

Tristates the transmitter output.

eusartTristateTxDisable

Disables tristating of the transmitter output.


Definition at line 257 of file platform/emlib/inc/em_eusart.h

EUSART_IrDARxFilterEnable_TypeDef#

EUSART_IrDARxFilterEnable_TypeDef

IrDA filter enable.

Enumerator
eusartIrDARxFilterEnable

Enable filter on demodulator.

eusartIrDARxFilterDisable

Disable filter on demodulator.


Definition at line 263 of file platform/emlib/inc/em_eusart.h

EUSART_IrDAPulseWidth_Typedef#

EUSART_IrDAPulseWidth_Typedef

Pulse width selection for IrDA mode.

Enumerator
eusartIrDAPulseWidthOne

IrDA pulse width is 1/16 for OVS=X16 and 1/8 for OVS=X8.

eusartIrDAPulseWidthTwo

IrDA pulse width is 2/16 for OVS=X16 and 2/8 for OVS=X8.

eusartIrDAPulseWidthThree

IrDA pulse width is 3/16 for OVS=X16 and 3/8 for OVS=X8.

eusartIrDAPulseWidthFour

IrDA pulse width is 4/16 for OVS=X16 and 4/8 for OVS=X8.


Definition at line 269 of file platform/emlib/inc/em_eusart.h

EUSART_PrsTriggerEnable_TypeDef#

EUSART_PrsTriggerEnable_TypeDef

PRS trigger enable.

Enumerator
eusartPrsTriggerDisable

Disable trigger on both receiver and transmitter.

eusartPrsTriggerEnableRx

Enable receive trigger only, transmit disabled.

eusartPrsTriggerEnableTx

Enable transmit trigger only, receive disabled.

eusartPrsTriggerEnableRxTx

Enable trigger on both receive and transmit.


Definition at line 284 of file platform/emlib/inc/em_eusart.h

EUSART_InvertIO_TypeDef#

EUSART_InvertIO_TypeDef

IO polarity selection.

Enumerator
eusartInvertIODisable

Disable inversion on both RX and TX signals.

eusartInvertRxEnable

Invert RX signal, before receiver.

eusartInvertTxEnable

Invert TX signal, after transmitter.

eusartInvertIOEnable

Enable trigger on both receive and transmit.


Definition at line 302 of file platform/emlib/inc/em_eusart.h

EUSART_AutoTxDelay_TypeDef#

EUSART_AutoTxDelay_TypeDef

Auto TX delay transmission.

Enumerator
eusartAutoTxDelayNone

Frames are transmitted immediately.

eusartAutoTxDelaySingle

Transmission of new frames is delayed by a single bit period.

eusartAutoTxDelayDouble

Transmission of new frames is delayed by a two bit periods.

eusartAutoTxDelayTripple

Transmission of new frames is delayed by a three bit periods.


Definition at line 317 of file platform/emlib/inc/em_eusart.h

EUSART_RxFifoWatermark_TypeDef#

EUSART_RxFifoWatermark_TypeDef

RX FIFO Interrupt ans Status Watermark.

Enumerator
eusartRxFiFoWatermark1Frame
eusartRxFiFoWatermark2Frame
eusartRxFiFoWatermark3Frame
eusartRxFiFoWatermark4Frame

Definition at line 332 of file platform/emlib/inc/em_eusart.h

EUSART_TxFifoWatermark_TypeDef#

EUSART_TxFifoWatermark_TypeDef

TX FIFO Interrupt and Status Watermark.

Enumerator
eusartTxFiFoWatermark1Frame
eusartTxFiFoWatermark2Frame
eusartTxFiFoWatermark3Frame
eusartTxFiFoWatermark4Frame

Definition at line 354 of file platform/emlib/inc/em_eusart.h

Typedef Documentation#

EUSART_PrsChannel_TypeDef#

typedef uint8_t EUSART_PrsChannel_TypeDef

PRS Channel type.


Definition at line 299 of file platform/emlib/inc/em_eusart.h

Function Documentation#

EUSART_UartInitHf#

void EUSART_UartInitHf (EUSART_TypeDef * eusart, const EUSART_UartInit_TypeDef * init)

Initialize EUSART when used in UART mode with the high frequency clock.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Ainit

A pointer to the initialization structure.

Initialize EUSART when used in UART mode with the high frequency clock.


Definition at line 904 of file platform/emlib/inc/em_eusart.h

EUSART_UartInitLf#

void EUSART_UartInitLf (EUSART_TypeDef * eusart, const EUSART_UartInit_TypeDef * init)

Initialize EUSART when used in UART mode with the low frequency clock.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Ainit

A pointer to the initialization structure.

Initialize EUSART when used in UART mode with the low frequency clock.

Note

  • (1) When EUSART oversampling is set to eusartOVS0 (Disable), the peripheral clock frequency must be at least three times higher than the chosen baud rate. In LF, max input clock is 32768 (LFXO or LFRCO), thus 32768 / 3 ~ 9600 baudrate.


Definition at line 912 of file platform/emlib/inc/em_eusart.h

EUSART_IrDAInit#

void EUSART_IrDAInit (EUSART_TypeDef * eusart, const EUSART_IrDAInit_TypeDef * irdaInit)

Initialize EUSART when used in IrDA mode with the high or low frequency clock.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/AirdaInit

A pointer to the initialization structure.

Initialize EUSART when used in IrDA mode with the high or low frequency clock.


Definition at line 921 of file platform/emlib/inc/em_eusart.h

EUSART_Reset#

void EUSART_Reset (EUSART_TypeDef * eusart)

Configure EUSART to its reset state.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

Configure EUSART to its reset state.


Definition at line 952 of file platform/emlib/inc/em_eusart.h

EUSART_Enable#

void EUSART_Enable (EUSART_TypeDef * eusart, EUSART_Enable_TypeDef enable)

Enable/disable EUSART receiver and/or transmitter.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Aenable

Select the status for the receiver and transmitter.

Enable/disable EUSART receiver and/or transmitter.


Definition at line 960 of file platform/emlib/inc/em_eusart.h

EUSART_Rx#

uint8_t EUSART_Rx (EUSART_TypeDef * eusart)

Receive one 8 bit frame, (or part of 9 bit frame).

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

Note

  • This function is normally used to receive one frame when operating with frame length of 8 bits. See EUSART_RxExt() for reception of 9 bit frames. Notice that possible parity/stop bits are not considered a part of the specified frame bit length.

  • This function will stall if buffer is empty until data is received.

Returns

  • Data received.

Receive one 8 bit frame, (or part of 9 bit frame).

Note

  • (1) Handles the case where the RX Fifo Watermark has been set to N frames, and when N is greater than one. Attempt to read a frame from the RX Fifo. If the read is unsuccessful (i.e. no frames in the RX fifo), the RXFU interrupt flag is set. If the flag is set, wait to read again until the RXFL status flag is set, indicating there are N frames in the RX Fifo, where N is equal to the RX watermark level. Once there are N frames in the Fifo, read and return one frame. For consecutive N-1 reads there will be data available in the Fifo. Therefore, the RXUF interrupt will not be triggered eliminating delays between reads and sending N data frames in "bursts".


Definition at line 975 of file platform/emlib/inc/em_eusart.h

EUSART_RxExt#

uint16_t EUSART_RxExt (EUSART_TypeDef * eusart)

Receive one 8-16 bit frame with extended information.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

Note

  • This function is normally used to receive one frame and additional RX status information.

  • This function will stall if buffer is empty until data is received.

Returns

  • Data received and receive status.

Receive one 8-16 bit frame with extended information.


Definition at line 988 of file platform/emlib/inc/em_eusart.h

EUSART_Tx#

void EUSART_Tx (EUSART_TypeDef * eusart, uint8_t data)

Transmit one frame.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Adata

Data to transmit.

Note

  • Depending on the frame length configuration, 8 (least significant) bits from data are transmitted. If the frame length is 9, 8 bits are transmitted from data. See EUSART_TxExt() for transmitting 9 bit frame with full control of all 9 bits.

  • This function will stall if the 4 frame FIFO is full, until the buffer becomes available.

Transmit one frame.


Definition at line 1003 of file platform/emlib/inc/em_eusart.h

EUSART_TxExt#

void EUSART_TxExt (EUSART_TypeDef * eusart, uint16_t data)

Transmit one 8-9 bit frame with extended control.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Adata

Data to transmit.

Note

  • Possible parity/stop bits in asynchronous mode are not considered part of a specified frame bit length.

  • This function will stall if buffer is full until the buffer becomes available.

Transmit one 8-9 bit frame with extended control.


Definition at line 1016 of file platform/emlib/inc/em_eusart.h

EUSART_BaudrateSet#

void EUSART_BaudrateSet (EUSART_TypeDef * eusart, uint32_t refFreq, uint32_t baudrate)

Configure the baudrate (or as close as possible to a specified baudrate).

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/ArefFreq

The EUSART reference clock frequency in Hz that will be used. If set to 0, the currently configured peripheral clock is used.

N/Abaudrate

A baudrate to try to achieve.

Configure the baudrate (or as close as possible to a specified baudrate).

Note

  • (1) When the oversampling is disabled, the peripheral clock frequency must be at least three times higher than the chosen baud rate.


Definition at line 1072 of file platform/emlib/inc/em_eusart.h

EUSART_BaudrateGet#

uint32_t EUSART_BaudrateGet (EUSART_TypeDef * eusart)

Get the current baudrate.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

Returns

  • The current baudrate.

Get the current baudrate.


Definition at line 1083 of file platform/emlib/inc/em_eusart.h

EUSART_RxBlock#

void EUSART_RxBlock (EUSART_TypeDef * eusart, EUSART_BlockRx_TypeDef enable)

Enable/Disable reception operation until the configured start frame is received.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Aenable

Select the receiver blocking status.

Enable/Disable reception operation until the configured start frame is received.


Definition at line 1092 of file platform/emlib/inc/em_eusart.h

EUSART_TxTristateSet#

void EUSART_TxTristateSet (EUSART_TypeDef * eusart, EUSART_TristateTx_TypeDef enable)

Enable/Disable the tristating of the transmitter output.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Aenable

Select the transmitter tristate status.

Enable/Disable the tristating of the transmitter output.


Definition at line 1101 of file platform/emlib/inc/em_eusart.h

EUSART_PrsTriggerEnable#

void EUSART_PrsTriggerEnable (EUSART_TypeDef * eusart, const EUSART_PrsTriggerInit_TypeDef * init)

Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Ainit

Pointer to the initialization structure.

Note

Initialize the automatic enabling of transmissions and/or reception using the PRS as a trigger.


Definition at line 1114 of file platform/emlib/inc/em_eusart.h

EUSART_StatusGet#

uint32_t EUSART_StatusGet (EUSART_TypeDef * eusart)

Get EUSART STATUS register.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

Returns

  • STATUS register value.


Definition at line 1124 of file platform/emlib/inc/em_eusart.h

EUSART_IntClear#

void EUSART_IntClear (EUSART_TypeDef * eusart, uint32_t flags)

Clear one or more pending EUSART interrupts.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Aflags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


Definition at line 1138 of file platform/emlib/inc/em_eusart.h

EUSART_IntDisable#

void EUSART_IntDisable (EUSART_TypeDef * eusart, uint32_t flags)

Disable one or more EUSART interrupts.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Aflags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


Definition at line 1152 of file platform/emlib/inc/em_eusart.h

EUSART_IntEnable#

void EUSART_IntEnable (EUSART_TypeDef * eusart, uint32_t flags)

Enable one or more EUSART interrupts.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Aflags

Pending EUSART interrupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


Definition at line 1166 of file platform/emlib/inc/em_eusart.h

EUSART_IntGet#

uint32_t EUSART_IntGet (EUSART_TypeDef * eusart)

Get pending EUSART interrupt flags.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

Returns

  • Pending EUSART interrupt sources.


Definition at line 1178 of file platform/emlib/inc/em_eusart.h

EUSART_IntGetEnabled#

uint32_t EUSART_IntGetEnabled (EUSART_TypeDef * eusart)

Get enabled and pending EUSART interrupt flags.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

Useful for handling more interrupt sources in the same interrupt handler.

Returns

  • Pending and enabled EUSART interrupt sources.


Definition at line 1191 of file platform/emlib/inc/em_eusart.h

EUSART_IntSet#

void EUSART_IntSet (EUSART_TypeDef * eusart, uint32_t flags)

Set one or more pending EUSART interrupts from SW.

Parameters
N/Aeusart

Pointer to the EUSART peripheral register block.

N/Aflags

Interrupt source(s) to set to pending. Use a bitwise logic OR combination of valid interrupt flags for EUSART module (EUSART_IF_nnn).


Definition at line 1212 of file platform/emlib/inc/em_eusart.h